> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Camera Calibration

## Overview

ZED cameras undergo an extensive and rigorous multi-step factory calibration process to ensure accurate camera parameter estimation. This calibration defines key characteristics such as focal length, field of view, and stereo alignment, which are essential for various computer vision and imaging applications.

This applies to both **stereo cameras** (ZED, ZED Mini, ZED 2, ZED 2i, ZED X, ZED X Mini, ZED X Nano) and **monocular cameras** (ZED X One), which are factory-calibrated for their intrinsic parameters.

> **Note**
>
> The ZED and ZED 2 cameras are out of production and may no longer be supported by newer versions of the ZED SDK.

The following parameters can be retrieved for each eye and resolution:

* Focal length: `fx`, `fy`.
* Principal point (optical center): `cx`, `cy`.
* Lens distortion, depending on the lens model: radial-tangential (Brown-Conrady) uses radial coefficients `k1`–`k6`, tangential coefficients `p1`, `p2`, and thin-prism coefficients `s1`–`s4`, while fisheye uses `k1`–`k4`.
* Field of view: horizontal (`h_fov`), vertical (`v_fov`), and diagonal (`d_fov`).
* Stereo transform between the left and right eye (stereo cameras only): baseline, translation (`TY`, `TZ`), and rotation: optical convergence (`CV`/`RY`), `RX`, and `RZ`.

## The Calibration File

Each ZED camera has a dedicated **calibration file** that is generated during the factory calibration process. It stores the **optical characteristics** of the camera's sensor(s) (and, for stereo cameras, the **geometry between the two sensors**) and is essential to accurate imaging and to the quality of the depth estimation process.

The file is named after the camera's **serial number** (e.g. `SNxxxxxxx.conf`) and is normally stored in the following location:

* **Windows**: `C:\ProgramData\StereoLabs\settings`
* **Linux**: `/usr/local/zed/settings/`

In addition, all cameras produced after May 2026, except the ZED Mini, store the factory calibration data directly on their internal **EEPROM**.

When an application opens a camera through the ZED SDK API, it looks for the calibration file in the `settings` folder. The SDK selects the calibration source in the following order of priority:

1. The calibration file found in the `settings` folder.
2. The calibration data stored on the camera's EEPROM, when no local file is available.
3. A fresh copy **automatically downloaded** from the StereoLabs servers, when neither a local file nor valid EEPROM data is available. **Note**: an internet connection is required in this case.

The calibration file can also be downloaded manually at any time from [`https://calib.stereolabs.com/?SN=<serial_number>`](https://calib.stereolabs.com/?SN=\<serial_number>), replacing `<serial_number>` with the value reported on the label on the back panel of the camera.

> **Note**
>
> The calibration data in the `settings` folder takes priority over the data stored on the EEPROM. This means that a **custom calibration file**, which overrides the factory calibration, always takes precedence over the EEPROM data.

> **Note**
>
> Reading the calibration data from the EEPROM requires ZED SDK v5.3 or newer.

### File Structure

The calibration file is a plain-text, INI-style file organized in named sections. Its exact content depends on the camera type:

* A **stereo camera** file (e.g. ZED 2i) describes the **left and right sensors** and the geometry between them.
* A **monocular camera** file (e.g. ZED X One) describes a **single sensor** and contains no stereo geometry.

In both cases, the sections are named after the **resolution** they apply to, the intrinsics follow the **pinhole camera model**, and a final `[MISC]` section carries metadata such as the sensor identifier (`Sensor_ID`).

The table below summarizes the sections found in each file type:

| Content                            | Stereo camera                           | Monocular camera |
| ---------------------------------- | --------------------------------------- | ---------------- |
| Sensor intrinsics (per resolution) | `[LEFT_CAM_<RES>]`, `[RIGHT_CAM_<RES>]` | `[CAM_<RES>]`    |
| Lens distortion                    | `[LEFT_DISTO]`, `[RIGHT_DISTO]`         | `[DISTO]`        |
| Stereo transform (extrinsics)      | `[STEREO]`                              | *(none)*         |
| Metadata                           | `[MISC]`                                | `[MISC]`         |

#### Sensor intrinsics

The intrinsic parameters describe a single sensor at a given resolution, following the pinhole camera model:

* `fx`, `fy`: focal length in pixels.
* `cx`, `cy`: optical center (principal point) coordinates in pixels.

For a **stereo camera**, each eye has its own section per resolution, `[LEFT_CAM_<RES>]` and `[RIGHT_CAM_<RES>]`, where `<RES>` depends on the camera model (e.g. `2K`, `FHD`, `HD`, `VGA` for a ZED 2i; `FHD1200`, `FHD`, `SVGA` for the ZED X family). These sections also embed a basic radial-tangential distortion model (`k1`, `k2`, `k3`, `p1`, `p2`):

```ini
[LEFT_CAM_HD]
fx=951.925
fy=952.475
cx=642.95
cy=366.023
k1=-0.0719661
k2=-0.0168656
p1=2.16146e-05
p2=-0.000677513
k3=-0.0496784

[RIGHT_CAM_HD]
fx=955.27
fy=955.99
cx=633.98
cy=362.8445
k1=-0.0692211
k2=-0.0253319
p1=-1.05111e-05
p2=0.000239657
k3=-0.0460711
```

For a **monocular camera**, there is a single `[CAM_<RES>]` section per resolution (the resolution names depend on the camera model, e.g. `FHD1200`, `FHD`, `SVGA`). These sections contain only the focal length and optical center; the distortion is stored separately in a dedicated section (see below):

```ini
[CAM_FHD]
fx=737.615
fy=737.295
cx=951.708
cy=474.671
```

#### Lens distortion

The distortion model depends on the camera's **lens type**:

* **Standard (rectilinear) lenses** use a **radial-tangential (Brown-Conrady)** model: radial coefficients `k1`–`k6` and tangential coefficients `p1`, `p2`.
* **Fisheye lenses** (e.g. a ZED X One fitted with such a lens) use a dedicated **fisheye** distortion model, which relies on only four radial coefficients (`k1`–`k4`), with no tangential or prism terms.

These coefficients are stored separately from the per-resolution intrinsics, in a resolution-independent section: one per eye for a **stereo camera** (`[LEFT_DISTO]`, `[RIGHT_DISTO]`) and a single `[DISTO]` for a **monocular camera**. The example below shows the radial-tangential coefficients of a standard lens:

```ini
[DISTO]
k1=0.121598
k2=0.0687899
k3=-0.0443668
k4=0.122025
k5=0.123382
k6=-0.0586831
p1=0.000355499
p2=-0.000283728
```

Through the ZED SDK, you can determine which model a given camera uses by reading the `lens_distortion_model` field (`sl::LENS_DISTORTION_MODEL`) of its parameters: `calibration_parameters.left_cam` (or `right_cam`) for a stereo camera, and `calibration_parameters` directly for a monocular one. Raw/unrectified parameters report `RAD_TAN` (Brown-Conrady) or `FISHEYE`, whereas rectified parameters always report `PINHOLE`, since the distortion is corrected during rectification. The raw coefficients themselves are exposed in the `disto` array. For the `RAD_TAN` model it is ordered as `[k1, k2, p1, p2, k3, k4, k5, k6, s1, s2, s3, s4]`: radial (`k1`–`k6`), tangential (`p1`, `p2`), and thin-prism (`s1`–`s4`); for the `FISHEYE` model, only the first four entries (`k1`–`k4`) are used.

#### Stereo transform

The `[STEREO]` section is present **only for stereo cameras**. It holds the **extrinsic parameters**: the position of the right sensor relative to the left sensor, with the right sensor itself as the center of rotation. Monocular files do not contain this section, as a single sensor has no stereo geometry.

```ini
[STEREO]
Baseline=120.27
TY=-0.319205
TZ=0.444416
CV_2K=0.000952819
CV_FHD=0.000952819
CV_HD=0.000952819
CV_VGA=0.000952819
RX_2K=0.00196122
RX_FHD=0.00196122
RX_HD=0.00196122
RX_VGA=0.00196122
RZ_2K=0.0019015
RZ_FHD=0.0019015
RZ_HD=0.0019015
RZ_VGA=0.0019015
```

* `Baseline`: distance between the two optics, in mm.
* `TY`, `TZ`: translation of the right sensor relative to the left one along the Y and Z axes, in mm.
* `CV_*` (also written `RY_*`): optical convergence, i.e. the rotation around the Y axis, given per resolution.
* `RX_*`, `RZ_*`: the remaining rotation axes describing the transformation between the two sensors, given per resolution.

Rotations are expressed using the **Rodrigues notation**.

## Raw and Rectified Calibration

The ZED SDK exposes **two sets** of calibration parameters, and they intentionally differ. Knowing which one you are looking at explains, for example, why the values shown in the [ZED Explorer](/docs/development/zed-tools/zed-explorer) **Calibration** tab do not match those returned by the SDK API.

**Raw (unrectified) calibration** describes the **real optics** of each physical sensor: each side keeps its own intrinsics, and the full lens distortion (`RAD_TAN` or `FISHEYE`) is present. These values correspond to the unrectified images (`VIEW::LEFT_UNRECTIFIED` / `VIEW::RIGHT_UNRECTIFIED`) and match (or are very close to) the values stored in the [calibration file](#the-calibration-file) and shown by ZED Explorer.

**Rectified calibration** describes the images **after rectification**, with the lens distortion already removed; the distortion coefficients are therefore zero and the model is `PINHOLE`. For a **stereo camera**, rectification also aligns the two views as if they came from an ideal, perfectly matched stereo pair, so that:

* the left and right sensors share the **same intrinsics**, because the epipolar lines are aligned on the same image rows;
* the stereo rotation is zero and the translation reduces to the **baseline** (`Tx`), with the other components being zero.

These are the parameters of the `VIEW::LEFT` / `VIEW::RIGHT` images that feed the depth-estimation pipeline, which is why the SDK returns them by default. ZED Explorer, in contrast, displays the **raw** stream, hence the difference.

Both sets are available from `getCameraInformation()`:

**`C++`**

```cpp C++
auto cam_config = zed.getCameraInformation().camera_configuration;
// Rectified parameters (default VIEW::LEFT / VIEW::RIGHT images)
sl::CalibrationParameters calib = cam_config.calibration_parameters;
// Raw parameters (VIEW::LEFT_UNRECTIFIED / VIEW::RIGHT_UNRECTIFIED images)
sl::CalibrationParameters calib_raw = cam_config.calibration_parameters_raw;
```

**`Python`**

```python Python
cam_config = zed.get_camera_information().camera_configuration
# Rectified parameters (default VIEW.LEFT / VIEW.RIGHT images)
calib = cam_config.calibration_parameters
# Raw parameters (VIEW.LEFT_UNRECTIFIED / VIEW.RIGHT_UNRECTIFIED images)
calib_raw = cam_config.calibration_parameters_raw
```

Monocular cameras (`sl::CameraOne`) expose the same two sets through `calibration_parameters` and `calibration_parameters_raw`, each as a single `CameraParameters`. The stereo-specific points above do not apply, but the principle is identical: the rectified set describes the **undistorted** image (`PINHOLE`, zero distortion), while the raw set describes the real lens.

## Stereo Cameras

Stereo cameras expose the intrinsic parameters of both the left and right eye, as well as the stereo transform (rotation and translation) between them, which is required for depth computation.

### Using the API

Camera parameters are available in `CalibrationParameters`. They can be retrieved using `getCameraInformation()`.

**`C++`**

```cpp C++
CalibrationParameters calibration_params = zed.getCameraInformation().camera_configuration.calibration_parameters;
// Focal length of the left eye in pixels
float focal_left_x = calibration_params.left_cam.fx;
// First radial distortion coefficient
float k1 = calibration_params.left_cam.disto[0];
// Translation between left and right eye on x-axis
float tx = calibration_params.stereo_transform.getTranslation()[0];
// Horizontal field of view of the left eye in degrees
float h_fov = calibration_params.left_cam.h_fov;
```

**`Python`**

```python Python
calibration_params = zed.get_camera_information().camera_configuration.calibration_parameters
# Focal length of the left eye in pixels
focal_left_x = calibration_params.left_cam.fx
# First radial distortion coefficient
k1 = calibration_params.left_cam.disto[0]
# Translation between left and right eye on x-axis
tx = calibration_params.stereo_transform.get_translation().get()[0]
# Horizontal field of view of the left eye in degrees
h_fov = calibration_params.left_cam.h_fov
```

**`C#`**

```csharp C#
sl.CalibrationParameters calibration_params = zed.GetCameraInformation().cameraConfiguration.calibrationParameters;
// Focal length of the left eye in pixels
float focal_left_x = calibration_params.leftCam.fx;
// First radial distortion coefficient
double k1 = calibration_params.leftCam.disto[0];
// Translation between left and right eye on x-axis
float tx = calibration_params.Trans.X;
// Horizontal field of view of the left eye in degrees
float h_fov = calibration_params.leftCam.hFOV;
```

> **Note**
>
> If self-calibration is enabled (the default), the ZED SDK re-estimates and refines the calibration at startup, so the returned values may differ slightly from the factory file. See [Self-Calibration](#self-calibration) and [Raw and Rectified Calibration](#raw-and-rectified-calibration) for details.

### Self-Calibration

By default, the ZED SDK runs a **self-calibration** process every time a stereo camera is opened. This step refines the factory calibration on the fly, correcting the small offsets that develop over time or with changing operating conditions (mechanical stress, vibrations, or thermal expansion of the camera body). The optimized parameters are then used by the SDK for rectification and depth estimation.

This behavior is controlled by the [`camera_disable_self_calib`](https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html#affeaa06cfc1d849e311e484ceb8edcc5) field of `InitParameters`:

* `false` *(default)*: self-calibration is enabled. Accuracy is improved, but the calibration parameters change slightly from one live run to another, which can be an issue when strict repeatability is required.
* `true`: self-calibration is skipped. The SDK uses the calibration parameters straight from the calibration file, guaranteeing identical values across runs at the cost of potentially reduced accuracy.

In most situations, self-calibration should remain enabled. You can also trigger it manually at any time after the camera is opened by calling `Camera::updateSelfCalibration()`.

> **Note**
>
> This is why the camera parameters reported by the ZED SDK API often differ from those shown by the **ZED Explorer** tool. ZED Explorer reads the **raw** values directly from the calibration file, whereas the API returns the **self-calibrated** parameters that have been optimized at startup. Because of this, even the **raw** parameters returned by the SDK (`calibration_parameters_raw`) can differ slightly from the factory file. To obtain the unmodified factory values, disable self-calibration by setting `camera_disable_self_calib` to `true` in `sl::InitParameters`. See [Raw and Rectified Calibration](#raw-and-rectified-calibration) for the distinction between raw and rectified parameters, and [this support article](https://support.stereolabs.com/hc/en-us/articles/27824782212119-Why-is-there-a-difference-in-camera-parameters-between-the-ZED-SDK-API-and-the-ZED-Explorer-tool) for more details.

A common practical use of self-calibration is **compensating for temperature drift**: as the camera heats up, its optical and mechanical characteristics shift, and re-running the self-calibration realigns the stereo pair. See [Using the sensor to compensate for temperature drift](/docs/development/zed-sdk/modules/sensors/temperature-sensors#use-the-sensor-to-compensate-for-temperature-drift) for a concrete example.

## Monocular Cameras

Monocular cameras, such as the [ZED X One](/docs/products/cameras/zedxone/monocular-vision/), have a single lens and are factory-calibrated for their **intrinsic parameters** only (focal length, principal point, lens distortion, and field of view). As they have a single optical sensor, no stereo transform is provided.

### Using the API

When using a monocular camera through the `sl::CameraOne` class, calibration parameters are available in a single `CameraParameters` object (instead of the `CalibrationParameters` used for stereo cameras). They can be retrieved using `getCameraInformation()`.

**`C++`**

```cpp C++
CameraParameters calibration_params = zed_one.getCameraInformation().camera_configuration.calibration_parameters;
// Focal length in pixels
float focal_x = calibration_params.fx;
// First radial distortion coefficient
float k1 = calibration_params.disto[0];
// Horizontal field of view in degrees
float h_fov = calibration_params.h_fov;
```

**`Python`**

```python Python
calibration_params = zed_one.get_camera_information().camera_configuration.calibration_parameters
# Focal length in pixels
focal_x = calibration_params.fx
# First radial distortion coefficient
k1 = calibration_params.disto[0]
# Horizontal field of view in degrees
h_fov = calibration_params.h_fov
```

> **Note**
>
> Two ZED X One cameras can be rigidly paired to build a [**Virtual Stereo Vision system**](/docs/products/cameras/zedxone/dual-camera-stereo-vision/). Because each monocular factory calibration file describes a single sensor and contains no stereo geometry (no `[STEREO]` section), an additional **extrinsic calibration** is mandatory to compute the relative position and orientation of the two cameras before depth can be estimated.

## Recalibrating your camera

While the **factory calibration is typically more accurate than user calibrations**, you may need to recalibrate your camera in specific situations, such as when placing glass in front of the lens, when operating underwater, or after a strong impact or exposure to extreme temperatures.

* **[ZED Calibration tool](/docs/development/zed-tools/zed-calibration/)**: a GUI tool shipped with the ZED SDK to fine-tune the intrinsic and extrinsic parameters of a stereo ZED camera. This tool **only works with stereo cameras** and cannot be used to calibrate a monocular ZED X One camera.
* **[ZED OpenCV Calibration tool](/docs/integrations/opencv/zed-open-cv-calibration#use-the-github-open-source-calibration-tool)**: an open-source, OpenCV-based tool to perform a guided checkerboard calibration of both **monocular and stereo cameras**: single ZED X One cameras, ZED stereo cameras, and custom stereo rigs (e.g. a dual ZED X One Virtual Stereo system). It generates calibration files compatible with the ZED SDK, and can also be used to **verify the quality** of an existing calibration.

> **Note**
>
> To manually calibrate a **monocular ZED X One camera** used in particular conditions (e.g. underwater, behind glass) or fitted with **custom lenses**, you must use the **ZED OpenCV Calibration** packages or a standard OpenCV calibration process, as the ZED Calibration tool does not support monocular cameras.