> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.stereolabs.com/docs/development/zed-sdk/modules/depth-sensing/using-the-api/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server. # Using the Depth Sensing API ## Depth Sensing Configuration To enable depth sensing, set options in `InitParameters` when initializing the camera. For runtime adjustments, such as enabling or disabling depth computation or changing the confidence thresholds, use `RuntimeParameters` while the camera is running. **`C++`** ```cpp C++ // Set configuration parameters InitParameters init_params; init_params.depth_mode = DEPTH_MODE::NEURAL; // Use NEURAL depth mode init_params.coordinate_units = UNIT::MILLIMETER; // Use millimeter units (for depth measurements) ``` **`Python`** ```python Python # Set configuration parameters init_params = sl.InitParameters() init_params.depth_mode = sl.DEPTH_MODE.NEURAL # Use NEURAL depth mode init_params.coordinate_units = sl.UNIT.MILLIMETER # Use millimeter units (for depth measurements) ``` **`C#`** ```csharp C# // Set depth mode in NEURAL InitParameters init_parameters = new InitParameters(); init_parameters.depthMode = DEPTH_MODE.NEURAL; // Use NEURAL depth mode init_parameters.coordinateUnits = UNIT.MILLIMETER; // Use millimeter units (for depth measurements) ``` For more information on depth configuration parameters, see [Depth Settings](/docs/development/zed-sdk/modules/depth-sensing/depth-settings/). ## Retrieving Depth Data To obtain the depth map of a scene, first call `grab()` to capture a new frame, then use `retrieveMeasure()` to access the depth data aligned with the left image. The `retrieveMeasure()` function allows you to retrieve various types of data, including the depth map, confidence map, normal map, or point cloud, depending on the specified measure type. **`C++`** ```cpp C++ sl::Mat image; sl::Mat depth_map; if (zed.grab() == ERROR_CODE::SUCCESS) { // A new image and depth is available if grab() returns SUCCESS zed.retrieveImage(image, VIEW::LEFT); // Retrieve left image zed.retrieveMeasure(depth_map, MEASURE::DEPTH); // Retrieve depth } ``` **`Python`** ```python Python image = sl.Mat() depth_map = sl.Mat() runtime_parameters = sl.RuntimeParameters() if zed.grab(runtime_parameters) == sl.ERROR_CODE.SUCCESS : # A new image and depth is available if grab() returns SUCCESS zed.retrieve_image(image, sl.VIEW.LEFT) # Retrieve left image zed.retrieve_measure(depth_map, sl.MEASURE.DEPTH) # Retrieve depth ``` **`C#`** ```csharp C# sl.Mat image = new sl.Mat(); sl.Mat depth_map = new sl.Mat(); uint mWidth = (uint)zed.ImageWidth; uint mHeight = (uint)zed.ImageHeight; image.Create(mWidth, mHeight, MAT_TYPE.MAT_8U_C4, MEM.CPU); // Mat needs to be created before use. depth_map.Create(mWidth, mHeight, MAT_TYPE.MAT_32F_C1, MEM.CPU); // Mat needs to be created before use. sl.RuntimeParameters runtimeParameters = new sl.RuntimeParameters(); if (zed.Grab(ref runtimeParameters) == sl.ERROR_CODE.SUCCESS) { // A new image and depth is available if Grab() returns SUCCESS zed.RetrieveImage(image, VIEW.LEFT); // Retrieve left image zed.RetrieveMeasure(depth_map, MEASURE.DEPTH); // Retrieve depth } ``` ### Accessing Depth Values The depth map is stored in a `sl::Mat` object, which acts as a 2D matrix where each element represents the distance from the camera to a specific point in the scene. Each pixel at coordinates (X, Y) contains a 32-bit floating-point value indicating the depth (Z) at that location, typically in millimeters unless otherwise configured. To access the depth value at a particular pixel, use the `getValue()` method provided by the SDK. This allows you to retrieve the distance from the camera to the object at the specified pixel coordinates. **`C++`** ```cpp C++ float depth_value=0; depth_map.getValue(x, y, &depth_value); ``` **`Python`** ```python Python depth_value = depth_map.get_value(x, y) ``` **`C#`** ```csharp C# depth_map.GetValue(x, y, out float depth_value); ``` By default, depth values are expressed in millimeters. Units can be changed using `InitParameters::coordinate_units`. Advanced users can retrieve images, depth and points clouds either in CPU memory (default) or in GPU memory using `retrieveMeasure(*, *, MEM::GPU)`. ## Displaying Depth Image The 32-bit depth map can be displayed as a grayscale 8-bit image. To display the depth map, the ZED SDK scales the real depth values to 8-bit values \[0, 255], where 255 (white) represents the closest possible depth value and 0 (black) represents the most distant possible depth value. We call this process depth normalization. To retrieve a depth image, you can use `retrieveImage(depth, VIEW::DEPTH)`. > **Note** > > Do not use the 8-bit depth image in your application for other purposes than displaying depth. **`C++`** ```cpp C++ sl::Mat depth_for_display; zed.retrieveImage(depth_for_display, VIEW::DEPTH); ``` **`Python`** ```python Python depth_for_display = sl.Mat() zed.retrieve_image(depth_for_display, sl.VIEW.DEPTH) ``` **`C#`** ```csharp C# sl.Mat depth_for_display = new sl.Mat(); uint mWidth = (uint)zed.ImageWidth; uint mHeight = (uint)zed.ImageHeight; depth_for_display.Create(mWidth, mHeight, MAT_TYPE.MAT_8U_C4, MEM.CPU); // Mat needs to be created before use. zed.RetrieveImage(depth_for_display, VIEW.DEPTH); ``` ## Getting Point Cloud Data The ZED camera can also provide a 3D point cloud, which is a collection of points in 3D space representing the scene. Each point in the point cloud corresponds to a pixel in the depth map and contains its (X, Y, Z) coordinates along with color information (RGBA). A 3D point cloud with (X,Y,Z) coordinates and RGBA color can be retrieved using `retrieveMeasure()`. **`C++`** ```cpp C++ sl::Mat point_cloud; zed.retrieveMeasure(point_cloud, MEASURE::XYZRGBA); ``` **`Python`** ```python Python point_cloud = sl.Mat() zed.retrieve_measure(point_cloud, sl.MEASURE.XYZRGBA) ``` **`C#`** ```csharp C# sl.Mat point_cloud = new sl.Mat(); uint mWidth = (uint)zed.ImageWidth; uint mHeight = (uint)zed.ImageHeight; point_cloud.Create(mWidth, mHeight, MAT_TYPE.MAT_32F_C4, MEM.CPU); // Mat needs to be created before use. zed.RetrieveMeasure(point_cloud, MEASURE.XYZRGBA); ``` To access a specific pixel value, use `getValue()`. **`C++`** ```cpp C++ float4 point3D; // Get the 3D point cloud values for pixel (i, j) point_cloud.getValue(i, j, &point3D); float x = point3D.x; float y = point3D.y; float z = point3D.z; float color = point3D.w; ``` **`Python`** ```python Python # Get the 3D point cloud values for pixel (i, j) point3D = point_cloud.get_value(i, j) x = point3D[0] y = point3D[1] z = point3D[2] color = point3D[3] ``` **`C#`** ```csharp C# float4 point3D = new float4(); // Get the 3D point cloud values for pixel (i, j) point_cloud.GetValue(i, j, out point3D); float x = point3D.x; float y = point3D.y; float z = point3D.z; float color = point3D.w; ``` The point cloud stores its data on 4 channels using a 32-bit float for each channel. The last float is used to store color information, where R, G, B, and alpha channels (4 x 8-bit) are concatenated into a single 32-bit float. You can choose between different color formats using `XYZ`. For example, BGRA color is available using `retrieveMeasure(point_cloud, MEASURE::XYZBGRA)`. ### Measuring distance in point cloud When measuring distances, use the 3D point cloud instead of the depth map. The Euclidean distance formula allows us to calculate the distance of an object relative to the left eye of the camera. **`C++`** ```cpp C++ float4 point3D; // Measure the distance of a point in the scene represented by pixel (i,j) point_cloud.getValue(i, j, &point3D); float distance = sqrt(point3D.x * point3D.x + point3D.y * point3D.y + point3D.z * point3D.z); ``` **`Python`** ```python Python # Measure the distance of a point in the scene represented by pixel (i,j) point3D = point_cloud.get_value(i, j) distance = math.sqrt(point3D[0] * point3D[0] + point3D[1] * point3D[1] + point3D[2] * point3D[2]) ``` **`C#`** ```csharp C# float4 point3D = new float4(); // Measure the distance of a point in the scene represented by pixel (i,j) point_cloud.GetValue(i, j, out point3D); float distance = (float)Math.Sqrt(point3D.x * point3D.x + point3D.y * point3D.y + point3D.z * point3D.z); ``` ## Getting Normal Map ### Retrieving Surface Normals You can obtain a normal map by calling `retrieveMeasure()` with the `NORMALS` measure type. Surface normals are useful for applications such as traversability analysis and real-time lighting, as they describe the orientation of surfaces in the scene. The normal map is stored as a 4-channel, 32-bit floating-point matrix, where the X, Y, and Z components represent the direction of the normal vector at each pixel. The fourth channel is unused. **`C++`** ```cpp C++ sl::Mat normal_map; zed.retrieveMeasure(normal_map, MEASURE::NORMALS); ``` **`Python`** ```python Python normal_map = sl.Mat() zed.retrieve_measure(normal_map, sl.MEASURE.NORMALS) ``` **`C#`** ```csharp C# sl.Mat normal_map = new sl.Mat(); uint mWidth = (uint)zed.ImageWidth; uint mHeight = (uint)zed.ImageHeight; normal_map.Create(mWidth, mHeight, MAT_TYPE.MAT_32F_C4, MEM.CPU); // Mat needs to be created before use. zed.RetrieveMeasure(normal_map, MEASURE.NORMALS); ``` To access the normal vector at a specific pixel, use the `getValue()` method, which returns the (X, Y, Z) components of the normal. ## Adjusting Depth Resolution To optimize performance and reduce data acquisition time, you can retrieve depth or point cloud data at a lower resolution by specifying the desired width and height in the `retrieveMeasure()` function. Additionally, you can choose whether the data is stored in CPU (RAM) or GPU memory by setting the appropriate memory type parameter. This flexibility allows you to balance processing speed and resource usage according to your application's needs. **`C++`** ```cpp C++ sl::Mat point_cloud; // Retrieve a resized point cloud // width and height specify the total number of columns and rows for the point cloud dataset sl::Resolution camera_resolution = zed.getCameraInformation().camera_configuration.resolution; sl::Resolution low_resolution(camera_resolution.width / 2, camera_resolution.height / 2); zed.retrieveMeasure(point_cloud, MEASURE::XYZRGBA, MEM::GPU, low_resolution); ``` **`Python`** ```python Python point_cloud = sl.Mat() # Retrieve a resized point cloud # width and height specify the total number of columns and rows for the point cloud dataset camera_resolution = zed.get_camera_information().camera_configuration.resolution low_resolution = sl.Resolution(camera_resolution.width // 2, camera_resolution.height // 2) zed.retrieve_measure(point_cloud, sl.MEASURE.XYZRGBA, sl.MEM.GPU, low_resolution) ``` **`C#`** ```csharp C# sl.Mat point_cloud = new sl.Mat(); // Retrieve a resized point cloud // width and height specify the total number of columns and rows for the point cloud dataset int width = zed.ImageWidth / 2; int height = zed.ImageHeight / 2; point_cloud.Create((uint)width, (uint)height, MAT_TYPE.MAT_32F_C4, MEM.GPU); // Mat needs to be created before use. zed.RetrieveMeasure(point_cloud, MEASURE.XYZRGBA, MEM.GPU, new Resolution(width, height)); ``` ## Code Example For code examples, check out the [Tutorial](https://github.com/stereolabs/zed-sdk/tree/master/tutorials/tutorial%203%20-%20depth%20sensing) and [Sample](https://github.com/stereolabs/zed-sdk/tree/master/depth%20sensing) on GitHub.