> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Setting up GNSS / RTK on Linux

This guide walks you through setting up a **GNSS receiver** on **Linux**, with optional **RTK** corrections, in order to use it with the ZED SDK's **Global Localization** module. If you are new to GNSS, start with the [GNSS Overview](/docs/development/zed-sdk/modules/global-localization/gnss) that explains the concepts used in this guide.

The instructions apply to most USB and serial GNSS receivers. If you use a **ZED Box Orin** with the GNSS option, `gpsd` is already installed and configured: follow the [ZED Box Orin GNSS guide](/docs/products/embedded/zed-box-orin/using-gnss) instead.

## Installation

Using [gpsd](https://gpsd.gitlab.io/gpsd/index.html) is the simplest way to retrieve GNSS data on Linux. `gpsd` is a service daemon that reads the data of the receiver, decodes NMEA and the most common binary protocols, and provides it to any number of applications through a single API. It can also act as an **NTRIP client** to forward RTK corrections to the receiver.

It is recommended to install `gpsd` from source, at the tested commit used below:

```bash
# Install the dependencies
sudo apt update && sudo apt install scons libgtk-3-dev

# Compile gpsd from source, at the tested commit
git clone https://gitlab.com/gpsd/gpsd.git
cd gpsd && git checkout 8910c2b60759490ed98970dcdab8323b957edf48
scons && scons check && sudo scons udev-install

# Add the Python path of the gpsd tools to .bashrc
echo 'export PYTHONPATH="$PYTHONPATH:/usr/local/lib/python3/dist-packages"' >> ~/.bashrc
```

In order to run without root privileges, it is recommended to add your user to the `dialout` and `tty` groups:

```bash
sudo adduser $USER dialout
sudo adduser $USER tty
```

Log out of the session or reboot the device for these changes to take effect.

### Checking the receiver

Connect the antenna and the receiver, then check that the receiver is detected:

```bash
ls /dev/tty*
```

You should see a device named `/dev/ttyACM0` (USB receivers) or `/dev/ttyUSB0` (USB-to-serial adapters). Receivers connected to a UART of the board use the corresponding serial port, for example one of the `/dev/ttyTHS*` devices on NVIDIA® Jetson™.

The device streams the raw [NMEA sentences](/docs/development/zed-sdk/modules/global-localization/gnss#gnss-data-formats) of the receiver. The data should look like this:

```bash
# Note: the cat command should be able to work without sudo
cat /dev/ttyACM0

$GNGSA,A,1,,,,,,,,,,,,,99.99,99.99,99.99,1*33
$GNGSA,A,1,,,,,,,,,,,,,99.99,99.99,99.99,2*30
$GPGSV,1,1,00,0*65
$GLGSV,1,1,00,0*79
$GAGSV,1,1,00,0*74
$GBGSV,2,1,05,10,,,29,11,,,28,12,,,28,13,,,29,3*72
$GBGSV,2,2,05,14,,,29,3*7F
$GNGLL,,,,,082018.00,V,N*57
$GNRMC,082019.00,V,,,,,,,230623,,,N,V*1D
$GNVTG,,,,,,,,,N*2E
$GNGGA,082019.00,,,,,0,00,99.99,,,,,,*7A
```

In this example the receiver has no fix yet: the position fields are empty. They are filled once enough satellites are tracked.

### Running gpsd

`gpsd` can be started by systemd, for example when it is installed from the Ubuntu `gpsd` package. However, the systemd service has reliability issues with USB GNSS receivers (for example, the device may need to be rebooted every time your application is restarted), so we recommend running the daemon manually and starting it at boot with a *cron job*. If a `gpsd` systemd service is present on your system, disable it first:

```bash
sudo systemctl disable --now gpsd.service gpsd.socket
```

To run the daemon, use the following command:

```bash
gpsd -nG -s 115200 /dev/ttyACM0
```

* `-n` starts reading the receiver immediately, without waiting for a client to connect.
* `-G` accepts connections from other machines on the network, in addition to `localhost`.
* `-s 115200` sets the baud rate. It is ignored by most USB receivers, but must match the configuration of the receiver on a UART.

To start `gpsd` at boot, add the following cron job with `crontab -e`:

```bash
@reboot sleep 10 && /usr/local/sbin/gpsd -nG -s 115200 /dev/ttyACM0
```

> **Note**
>
> Replace `ttyACM0` with the communication port of your GNSS receiver.

You can test that `gpsd` is working properly with the `xgps` tool installed with `gpsd`:

```bash
# GNSS and satellite data in graphical interface
xgps
```

![](/_fern-files/stereolabs.docs.buildwithfern.com/b5ff2e3425587e96b0bad2d0cc59514f2d3d3e9dfd8a9072f3c887fddaf02583/docs/products/embedded/zed-box-orin/images/xgps.webp)

On a headless device, use the terminal-based `cgps` tool instead.

## Enabling RTK on your GNSS receiver

[RTK](/docs/development/zed-sdk/modules/global-localization/gnss#rtk) uses the correction data streamed by a nearby base station to improve the accuracy of the position from a few meters to a few centimeters. The corrections are usually received through the internet from an [NTRIP caster](/docs/development/zed-sdk/modules/global-localization/gnss#ntrip).

### Using NTRIP

`gpsd` can act as an NTRIP client to retrieve RTK corrections from a base station and forward them to the receiver. Replace the placeholders of the command below with the [NTRIP connection information](/docs/development/zed-sdk/modules/global-localization/gnss#ntrip) of your correction provider: the caster `<url>` and `<port>`, the `<mountpoint>` of a base station less than 25 km away, and the `<username>` and `<password>` if the caster requires them.

Restart `gpsd` as an NTRIP client with:

```bash
sudo pkill gpsd # Kill gpsd if it is already running
gpsd -nG ntrip://<username>:<password>@<url>:<port>/<mountpoint> -s 115200 /dev/ttyACM0
```

> **Note**
>
> Replace `ttyACM0` with the communication port of your GNSS receiver.

You can now run `xgps` and wait for the GNSS to get an **RTK fix**. The *ECEF pAcc* value gives the estimated 3D position accuracy: with an RTK FIX status, this value should be a few centimeters.

### Set RTK configuration at boot

Update the cron job so that `gpsd` connects to the base station at every boot:

```bash
crontab -e
```

And replace the `gpsd` line already present with the following:

```bash
@reboot sleep 10 && /usr/local/sbin/gpsd -nG ntrip://<username>:<password>@<url>:<port>/<mountpoint> -s 115200 /dev/ttyACM0
```

## Next steps

* If your receiver provides a **PPS** output, you can use it to [synchronize the system clock](/docs/development/zed-sdk/modules/global-localization/gnss/pps-time-synchronization) with GNSS time.
* [Read the GNSS data from gpsd in your application](/docs/development/zed-sdk/modules/global-localization/gnss/using-gnss-data) and ingest it into the Fusion module.
* Try the [Global Localization samples on GitHub](https://github.com/stereolabs/zed-sdk/tree/master/global%20localization), which read GNSS data from `gpsd`.