> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Magnetometer Overview

The magnetometer measures the intensity of the magnetic field around the camera in microteslas (μT). The magnetometer determines the orientation of the Earth's magnetic field, which gives the absolute orientation of the camera relative to the magnetic North Pole.

> **Note**
>
> Only the **ZED 2** (out of production) and the **ZED 2i** cameras are equipped with a magnetometer.

## Output Data

The following information is accessible from the camera sensor stack:

| Output Data                   | Description                                                                                     | Units                                                                                                                                    |
| ----------------------------- | ----------------------------------------------------------------------------------------------- | ---------------------------------------------------------------------------------------------------------------------------------------- |
| **Magnetometer (50 Hz)**      |                                                                                                 |                                                                                                                                          |
| `magnetic_field_uncalibrated` | Ambient geomagnetic field for all three physical axes (x, y, z) in μT. Values are uncalibrated. | μT                                                                                                                                       |
| `magnetic_field_calibrated`   | Ambient geomagnetic field for all three physical axes (x, y, z) in μT. Values are calibrated.   | μT                                                                                                                                       |
| `magnetic_heading`            | Camera heading relative to the magnetic North Pole.                                             | °                                                                                                                                        |
| `magnetic_heading_state`      | State of the `magnetic_heading`. (If `magnetic_heading` is reliable or not.)                    | [HEADING\_STATE](https://www.stereolabs.com/docs/api/structsl_1_1SensorsData_1_1MagnetometerData.html#a147c457960e1dbf933486089d226979c) |
| `magnetic_heading_accuracy`   | Accuracy of the magnetic heading measure in the range \[0.0, 1.0].                              |                                                                                                                                          |
| `timestamp`                   | Timestamp of the data measurement recording.                                                    | ns                                                                                                                                       |
| `effective_rate`              | Realtime data acquisition rate                                                                  | Hz                                                                                                                                       |

## Using the API

The magnetometer measures the intensity of the magnetic fields around the camera. By measuring the Earth's magnetic field, the sensor can estimate the camera's absolute orientation relative to the magnetic North Pole.

Magnetometer values are stored in the `SensorsData::MagnetometerData` which can be accessed with:

**`C++`**

```cpp C++
SensorsData sensors_data;
SensorsData::MagnetometerData magnetometer_data;

// Grab new frames and retrieve sensors data
while (zed.grab() == ERROR_CODE::SUCCESS) {
  zed.getSensorsData(sensors_data, TIME_REFERENCE::IMAGE); // Retrieve only frame synchronized data

  // Extract magnetometer data
  magnetometer_data = sensors_data.magnetometer;

  // Retrieve uncalibrated magnetic field
  float3 magnetic_field_uncalibrated = magnetometer_data.magnetic_field_uncalibrated;

  // Retrieve calibrated magnetic field
  float3 magnetic_field_calibrated = magnetometer_data.magnetic_field_calibrated;
}
```

**`Python`**

```python Python
sensors_data = sl.SensorsData()
magnetometer_data = sl.SensorsData.MagnetometerData()

# Grab new frames and retrieve sensors data
while zed.grab() == sl.ERROR_CODE.SUCCESS :
  zed.get_sensors_data(sensors_data, sl.TIME_REFERENCE.IMAGE) # Retrieve only frame synchronized data

  # Extract magnetometer data
  magnetometer_data = sensors_data.get_magnetometer_data()

  # Retrieve uncalibrated magnetic field
  magnetic_field_uncalibrated = magnetometer_data.get_magnetic_field_uncalibrated()

  # Retrieve calibrated magnetic field
  magnetic_field_calibrated = magnetometer_data.get_magnetic_field_calibrated()
```

**`C#`**

```csharp C#
SensorsData sensors_data = new SensorsData();
MagnetometerData magnetometer_data = new MagnetometerData();

RuntimeParameters runtimeParameters = new RuntimeParameters();
// Grab new frames and retrieve sensors data
while (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
  zed.GetSensorsData(ref sensors_data, TIME_REFERENCE.IMAGE); // Retrieve only frame synchronized data

  // Extract magnetometer data
  magnetometer_data = sensors_data.magnetometer;

  // Retrieve uncalibrated magnetic field
  Vector3 magnetic_field_uncalibrated = magnetometer_data.magneticFieldUncalibrated;

  // Retrieve calibrated magnetic field
  Vector3 magnetic_field_calibrated = magnetometer_data.magneticField;
}
```

> **Note**
>
> The values in `magnetic_field_calibrated` are different from the values in `magnetic_field_uncalibrated` only if the magnetometer sensor has been calibrated following the [procedure illustrated below](#magnetometer-calibration).

## Code Example

For a code example, check out the [Getting Sensor Data](/docs/tutorials/sensor-data/) tutorial.

## Magnetometer Calibration

Unlike all the other sensors, the magnetometer cannot be factory calibrated. The Earth's magnetic field is very weak, about 35-65 µT, so the measures of the magnetometer sensor are highly affected by the environment where the camera is placed. Metal cases, power cables, robot motors, speakers, and all the ferromagnetic objects, are very strong sources of magnetic disturbance that strongly influence what the magnetometer measures.

For this reason, if you plan to use this useful sensor, you must calibrate it once the camera is fixed in the final location where it will be used.
An accurate calibration procedure requires the camera to be rotated in space to acquire magnetic field information from all possible directions.

Once the magnetometer sensor is calibrated it can be used as a (3D) compass to determine the direction of the magnetic North (heading or yaw).

There are two kinds of calibration to be performed:

* Hard iron calibration
* Soft iron calibration

The hard iron calibration procedure generates the offset parameters used to compensate for the effects of all the active magnetic materials placed near the sensors. The soft iron calibration procedure generates the rescaling factor parameters used to compensate for the effects of metal objects placed near the sensor, which do not necessarily generate a magnetic field themselves. It ensures that the magnetic field is measured with the same scale along the three main axes.

> **Note**
>
> Calibrating the sensor once does not guarantee a permanent good calibration. The procedure must be replicated in time to compensate for the variations of the local magnetic fields.

To perform a tri-axis magnetometer calibration you can use the `ZED Sensor Viewer` application. Select the `Magnetometer` sensor and click on `Calibrate Magnetometer`.

![image](/_fern-img/140f2062d1c4c30ac8dff7414c671d538eb9d67aeec2447795fa87b864c2261e.webp)

### Calibration process

Start the calibration by pressing the button `START CALIBRATION`.

> **Note**
>
> You can clear all the acquired data and restart the calibration process at any moment by pressing the `CLEAR DATA` button.

#### 1. Initialize the plane XY

Perform a series of **roll rotations**. The scope of this phase is to "draw" a complete red circumference fitting the red ellipsoid in the background:

#### 2. Initialize the plane YZ

Perform a series of **pitch rotations**. The scope of this phase is to "draw" a complete green circumference fitting the green ellipsoid in the background:

#### 3. Initialize the plane XZ

Perform a series of **yaw rotations**. The scope of this phase is to "draw" a complete blue circumference fitting the blue ellipsoid in the background:

#### 4. Perform a full calibration

Perform a series of **mixed rotations** trying to orient the camera in all the possible roll, pitch, and yaw combinations. The scope of this phase is to fill as much area inside the three ellipsoids as possible for the three planes XY, YZ and XZ:

#### 5. Stop the calibration and verify the result

When the three ellipsoids are filled, the calibration process can be stopped by pressing the button `STOP CALIBRATION`.

You can check the reliability of the calibration by verifying that the calibrated values for the three planes are perfectly overlapped in the `Calibrated data` chart, and that they fit (with some outliers) the unitary ellipsoid displayed in the background:

![image](/_fern-img/92158d9972cc29c2c8aa1df9c4f584395e0fc997facc2d242e9c53b6cfa4f71e.webp)

On the left side of the interface, you can find two compasses. The red compass shows the heading of the camera calculated using the uncalibrated magnetic field values, the blue compass shows the heading of the camera calculated using the calibrated magnetic field values. Place the camera horizontally and rotate it around the vertical axis. If the calibration is done well, the blue compass should display the correct camera orientation with respect to the North Magnetic Pole. You can use a "real" compass to compare the values.

> **Note**
>
> The North Magnetic Pole does not correspond to the geographic North Pole, and the angle between magnetic north and true north (magnetic declination) depends on where the camera is located. Do not use a digital compass to compare the results if its readings are corrected to true north using GPS coordinates (e.g. smartphone compass applications can apply this correction and show different values).

#### 6. Save the calibration parameters

Store the calibration parameters in the non-volatile memory of the camera by pressing the button `STORE CALIBRATION`.

You can reset the magnetometer calibration to the default values at any moment by pressing the `RESET CALIBRATION` button.

> **Warning**
>
> The reset process is not reversible and it will erase the current calibration.

#### 7. Close the dialog

You can now close the calibration dialog to go back to the main Sensor Viewer. Select again the `Magnetometer` sensor and verify that on top of the plot you can read `Magnetometer [Calibrated]`.