> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Depth Viewer

**ZED Depth Viewer** is the tool that lets you explore the depth processing capabilities of the ZED camera. It allows you to visualize the depth map, point cloud, and other depth-related data in real-time.

![image](/_fern-img/4917388d56d02ef9e1d3198983174d8a392d984879db62d3a30d58a9e832c5f8.webp)

**ZED Depth Viewer** can work with live camera feeds, Network streams, or recorded SVO files. It provides a user-friendly interface to visualize depth data and adjust various parameters to optimize the depth perception.

## Run ZED Depth Viewer

After connecting your camera and installing the ZED SDK, you can run **ZED Depth Viewer** to visualize the depth data.

**ZED Depth Viewer** is an application for ZED depth map and point cloud visualization. It lets you change video resolution, depth mode, and camera parameters, and capture high-resolution images, depth maps, and point clouds.

Under Windows, you can find **ZED Depth Viewer** in the Start menu under the ZED SDK folder. You can also run it from the command line by navigating to the ZED SDK installation directory: `C:\Program Files (x86)\ZED SDK\tools\ZED Depth Viewer.exe`

Under Ubuntu, you can run **ZED Depth Viewer** from the terminal by typing `ZED_Depth_Viewer` or by navigating to the ZED SDK installation directory: `/usr/local/zed/tools/ZED_Depth_Viewer`

## Select the camera

When you launch **ZED Depth Viewer**, it automatically detects all connected ZED cameras and opens the first available. You can select the camera you want to use from the dropdown menu at the top right of the window.

![image](/_fern-img/876cdaa4abd3cc71eaff98ce59d190046b82c14cd2cf934aea4939f93c3707e7.webp)

You can click on the arrows icon on the right side of the dropdown menu to refresh the dropdown content after unplugging and replugging one camera.

You can click on the gear icon on the right side of the serial number text field to open the [**Camera and Application Settings** dialog](/docs/development/zed-tools/zed-depth-viewer/#configure-the-application-and-camera).

## Select the video mode and source

You can select the resolution and framerate from the dropdown menus at the top left of the window. The available video modes depend on the camera model and its capabilities.

![image](/_fern-img/f84716db20992cd6ac110ed902fce140036dedb34753b3de19b34148bed9ab35.webp)

Between the StereoLabs logo and the video mode dropdown, you can see the current playback mode: `LIVE`, SVO `PLAYBACK`, or `STREAMING (NETWORK)`.

You can select the input source by clicking on the related icon:

* **Live Camera**: Use the live feed from the connected ZED camera.
* **SVO File**: Use a recorded SVO file for playback.
* **Network Stream**: Use a network stream from another device or application that supports ZED streaming.

You can also drag and drop a saved `sl::InputType` onto the window, making it easier to open a stream or a virtual stereo setup. Available since ZED SDK 5.1.

## Visualize the data

The interface of **ZED Depth Viewer** is divided into three main sections:

* **Color Video Feed**: Displays the color video feed, allowing you to select between the left, right, or synchronized stereo side-by-side data.

| Left                                                                       | Right                                                                       | Side by Side                                                                 |
| -------------------------------------------------------------------------- | --------------------------------------------------------------------------- | ---------------------------------------------------------------------------- |
| ![image](/_fern-img/be1fcca9dd307074795cc5cd3faca4adfa514a04d364e4f41d2c126fab0dfde7.webp) | ![image](/_fern-img/0bc6e62c3b323e54b2b0850fbde57afd107f5a315ceab8b9778f8f96016de4be.webp) | ![image](/_fern-img/8c82611912585a2dcbb1673a5e86d5dddcf956bf86b1a9fb3a9e1491cc6aaa19.webp) |

* **Depth Feed**: Displays the depth map or the confidence map, depending on the selected mode.

| Depth Map                                                                   | Confidence Map                                                                   |
| --------------------------------------------------------------------------- | -------------------------------------------------------------------------------- |
| ![image](/_fern-img/b31d392f225151c849fe57ac01e53fca975110c2b7670ece4eb0facfbf77942b.webp) | ![image](/_fern-img/79b223ffee00a43da10e107a4f473587c2ffada3cb633444a8e5c8ccfbdffc8d.webp) |

* **3D Data Feed**: Displays the point cloud generated from the stereo data.
  * You can rotate the camera view by clicking the left button and dragging the mouse in the 3D view.
  * You can zoom in and out by scrolling the mouse wheel.
  * You can pan the view by clicking the right button and dragging the mouse in the 3D view.

![image](/_fern-img/648ae867b2056351969f65e2fddb59766a760b39b6704b5171b2c033aeb539d2.webp)

By toggling the options at the top left of the interface, you can:

* **Enable/Disable the Depth Shading**: toggle the depth shading effect on the depth map.
  ![image](/_fern-img/b1ed4ddc959eca292001945e2ba071a2dd25581e66226f81f7429807d52791c7.webp)
* **Enable/Disable the Lidar View**: transform the point cloud into a Lidar-like view, where points are colored based on their depth value.
* **Enable/Disable the gravity alignment**: align the point cloud to the gravity vector using the IMU data from the camera. This is useful for applications that require a consistent orientation of the point cloud.
* **Quickly toggle between Confidence level 95 and 100**: Allows you to quickly remove noisy points by filtering measures with lower confidence values.

## Monitor the Depth Processing performance

![image](/_fern-img/8903c1548e149ed90663a38a4e17d71206234ed2a47cf7f45f3a617805f11e1c.webp)

Under the video feed, on the bottom left, you can see the processing status information, including:

* **Image grab frequency**: The frequency at which images are grabbed from the camera.
* **Depth processing frequency**: The frequency at which depth data is processed.

## Configure the Application and Camera

### Configure the application

![image](/_fern-img/073657a1605790e02446bcd9aa2ee73e83e92d01c84de9c6c5771890d5637f7d.webp)

In the **Application Settings** tab, you can configure the following options:

* **Depth Initialization**: Depth settings to be tuned before opening the camera. Every modification will require a camera restart by clicking the **APPLY** button.
  * **Depth Mode**: Select the [depth mode](/docs/development/zed-sdk/modules/depth-sensing/depth-modes/) (`NEURAL_LIGHT`, `NEURAL`, `NEURAL_PLUS`) to adjust the depth quality and processing speed.
  * **Depth Min.**: Set the minimum depth range for depth processing.
  * **Depth Max.**: Set the maximum depth range for depth processing.
  * **Depth Stabilization**: Set the strength of the depth stabilization filter. Lower values result in less smooth but more reactive depth maps; higher values result in smoother depth maps that may appear blurred in dynamic scenes.
  * **Depth Precision**: Select the `NEURAL` depth precision (`sl::InitParameters::depth_precision`). `INT8` trades a small amount of accuracy for a faster depth runtime and a lower memory footprint; `FP16` remains the default. Available since ZED SDK 5.5.
* **Depth Runtime**: Depth settings that can be modified while the camera is open.
  * **Remove Saturated Areas**: Enable or disable the removal of color image saturated areas in the depth map.
  * **Confidence Threshold**: Set the confidence threshold for depth data. Higher values result in more reliable depth data but may reduce the effective range.
  * **Texture Confidence**: Enable or disable texture confidence for depth processing.
* **Other settings**:
  * **Enable Light Mode**: Switch the application window to light mode for better visibility in bright environments.
  * **Grid Y Translation**: Adjust the Y translation of the reference grid in the point cloud view.
* **Region of Interest (ROI)**: Draw a Region of Interest on the image. The mask is saved and can be loaded later by the ZED SDK. Available since ZED SDK 5.0.
* **Data Saving**:
  * **Directory**: Set the directory where captured images, depth maps, and point clouds will be saved.
  * **Image**: Select the image to be saved (`PNG` format) between `LEFT`, `RIGHT`, `SIDE BY SIDE`, or `DEPTH IMAGE`. Click on **SAVE** to save the current image.
  * **Depth**: Select the format for saving depth maps (`PNG`, `PFM`, or `PGM`). Click on **SAVE** to save the current depth map.
  * **Point Cloud**: Select the format for saving point clouds (`PLY`, `XYZ`, `PCD`, or `VTK`). Click on **SAVE** to save the current point cloud.

### Configure the camera

![image](/_fern-img/f58121bc779cb681eef35461f3c020d465b73df112ded1b2776d012bd180b575.webp)

In the **Camera Settings** tab, you can control different camera parameters:

* **Contrast**: Adjust the contrast of the video feed.
* **Saturation**: Adjust the saturation of the video feed.
* **Hue**: Adjust the hue of the video feed.
* **Gain**: Adjust the gain of the video feed.
* **White Balance**: Adjust the white balance of the video feed.
* **Exposure**: Adjust the exposure of the video feed.
* **Sharpness**: Adjust the sharpness of the video feed.
* **Gamma**: Adjust the gamma of the video feed.
* **Auto Exposure**: Enable or disable automatic exposure adjustment.
* **Auto White Balance**: Enable or disable automatic white balance adjustment.
* **Exposure Range**: Adjust the exposure range of the video feed.
* **Analog Gain Range**: Adjust the analog gain range of the video feed.
* **Digital Gain Range**: Adjust the digital gain range of the video feed.
* **Denoising**: Adjust the denoising filter strength.
* **Exposure Compensation**: Adjust the exposure compensation for the video feed.

These settings allow you to fine-tune the camera parameters to achieve the desired video quality and performance. You can adjust these parameters in real-time while the camera is streaming live or network streams.

Some of these parameters may not be available for all camera models or video modes. The available parameters depend on the camera model and its capabilities.

Click on the **DEFAULT VALUES** button to reset the camera parameters to their default values.