> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED X Driver

The **ZED X Driver** is the NVIDIA® Jetson™ Linux (L4T) driver package that runs the ZED X family of cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One GS, ZED X One 4K and ZED X One Core). It configures the deserializer of the capture card, the cameras and their IMU, and installs the `zed_x_daemon` service. The ZED SDK relies on it to open any [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) or MIPI camera connected to the Jetson.

Each package is built for one platform (ZED Link capture card or ZED Box model) and one Jetson Linux version; recent Jetson Linux versions also have a package for the real-time (RT) kernel. Download the package matching your setup from the [ZED X Camera Drivers](https://www.stereolabs.com/developers/drivers) page of the StereoLabs website. The same page also lists compatibility drivers for third-party embedded computers certified by StereoLabs.

## Install and upgrade

* [ZED Link GMSL2 capture cards](/docs/products/embedded/zed-link-capture-card/gmsl2/install-and-upgrade-the-drivers): ZED Link Mono, Duo and Quad.
* [ZED Link MIPI Quad](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-orin-agx-devkit-setup#install-the-zed-link-mipi-driver) on a Jetson AGX Orin™ devkit.
* [ZED Box series](/docs/products/embedded/zed-box-series/): the driver comes preinstalled. See the GMSL page of your ZED Box to reinstall it after a system upgrade.

## Release notes

* [ZED X Driver Release Notes](/docs/development/zed-x-driver/release-notes): new features, improvements and bug fixes of every GMSL2 and MIPI driver release.
* [Holoscan Driver](/docs/development/zed-x-driver/release-notes/holoscan-driver): release notes of the driver for the ZED Link MIPI Quad on a Jetson AGX Thor™ with the NVIDIA® Holoscan Sensor Bridge.