> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Holoscan Driver

The **Holoscan Driver** runs the [ZED Link MIPI Quad](/docs/products/embedded/zed-link-capture-card/mipi/) on an NVIDIA® Jetson AGX Thor™ through the NVIDIA® Holoscan Sensor Bridge (Lattice), with up to two [ZED X One Core](/docs/products/cameras/zedxone-core/) cameras over Camera-over-Ethernet. It is released separately from the [ZED X Driver](/docs/development/zed-x-driver/release-notes) and has its own version numbers.

> **Note**
>
> Download links are available in the Holoscan section of the [ZED X Camera Drivers](https://www.stereolabs.com/developers/drivers) page. To set up the camera, see the [Jetson AGX Thor setup guide](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-agx-thor-devkit-setup), and the [Holoscan troubleshooting section](/docs/products/embedded/zed-link-capture-card/mipi/troubleshooting#holoscan-sensor-bridge-on-jetson-agx-thor) if no camera is detected.

| Release       | Release date | Jetson Linux             |
| ------------- | ------------ | ------------------------ |
| [1.0.0](#100) | Nov 16, 2026 | JetPack 7.2 (L4T 39.2.1) |

## 1.0.0

*Released: Nov 16, 2026*

### New Features & Improvements

* Initial support for the Holoscan Sensor Bridge (Lattice) on Jetson AGX Thor with JetPack 7.2. The ZED X One Core is opened from the ZED SDK with `sl::INPUT_TYPE::HOLOSCAN`, available from ZED SDK 5.5. See the [ZED SDK 5.5 release notes](/docs/development/zed-sdk/release-notes/5-x/5-5).