> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# How to Use Foxglove with ZED

## What is Foxglove?

[Foxglove](https://foxglove.dev/product) is a visualization and debugging tool designed for robotics development. It offers an intuitive interface to inspect sensor data such as camera images, point clouds, and transforms in real time.

With Foxglove, developers can monitor and interact with their robotics applications via ROS 2, making it a powerful tool for analyzing and tuning perception systems like those using **StereoLabs ZED cameras**.
In this tutorial, we will go through how to visualize live or recorded ZED data in Foxglove.

## Installing and Launching Foxglove

To get started with Foxglove:

1. Download the app for your operating system from the [Foxglove Downloads page](https://foxglove.dev/download).
2. Once installed, launch Foxglove. You’ll be prompted to set up a data connection; it will be configured to connect to ROS 2 using the Foxglove Bridge.

## Running the ZED ROS 2 Wrapper

### Prerequisites

* [ZED ROS 2 Wrapper](/docs/integrations/ros-2/#installation) installed in your ROS 2 workspace
* A connected ZED camera or SVO file

### Launching the ZED node

```bash
source /opt/ros/humble/setup.bash
source ~/your_ros2_ws/install/local_setup.bash

ros2 launch zed_wrapper zed_camera.launch.py camera_model:=<camera model>
```

This will start the ZED ROS 2 Wrapper and begin publishing all the ZED topics.

## Installing and Running the Foxglove ROS 2 Bridge

To connect ROS 2 to Foxglove, you need to run the [ROS Foxglove Bridge](https://docs.foxglove.dev/docs/connecting-to-data/ros-foxglove-bridge), which converts ROS and ROS 2 topics into a WebSocket stream that Foxglove can read.

### Installation

Please take a look at [Foxglove's documentation](https://docs.foxglove.dev/docs/connecting-to-data/ros-foxglove-bridge#installation) to make sure the bridge is available in your ROS/ROS 2 distribution.

```bash
sudo apt install ros-$ROS_DISTRO-foxglove-bridge
```

### Running the bridge

```bash
source /opt/ros/humble/setup.bash
source ~/your_ros2_ws/install/local_setup.bash

ros2 launch foxglove_bridge foxglove_bridge_launch.xml
```

By default, the bridge starts a WebSocket server on port 8765.

### Connecting Foxglove to ROS 2

1. In Foxglove, click "Open Connection".

   ![](/_fern-img/b8cdaf2831f0467d2d5c693ca2cb2bf4699cac4138765cc7fe26c2884c8bce74.webp)

2. Enter the URL: ws\://localhost:8765 and click "Connect"

   ![](/_fern-img/50e1796a9feeadeb229deaa91d51f5f9575b90762bda2aa87c681140fd16f985.webp)

3. If you have not already, download [StereoLabs' Foxglove layout](https://github.com/stereolabs/zed-ros2-examples/blob/master/zed_display_foxglove/layouts/layout_foxglove_zed.json), and import it by clicking on "Import from file..." in the top right corner

   ![](/_fern-img/6e9d1a88683e8524216d1a63e09ff1890fd7552c673af0a12e27dde1b3edf9e6.webp)

4. You should now see your ZED topics available for visualization!

   ![](/_fern-img/63f5fe7c8e6d1e77789c90648c3cd5f2a24f36e090b53a4721b1e484b77cb951.webp)

You can add panels like Image, 3D, or Raw Messages to inspect your sensor data in real time.