> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Isaac™ ROS 3 Integration Overview (Legacy)

> **Warning**
>
> This is the legacy documentation for **[NVIDIA® Isaac™ ROS 3.2](https://nvidia-isaac-ros.github.io/v/release-3.2/)** (ROS 2 Humble, Ubuntu 22.04, JetPack 6). It is kept for existing projects and is no longer updated.
>
> For new projects, use **NVIDIA® Isaac™ ROS 5** and follow the [current Isaac™ ROS documentation](/docs/integrations/isaac-ros/).

NVIDIA® Isaac™ ROS (Robot Operating System) is a collection of [NVIDIA® CUDA®-accelerated computing packages](https://nvidia-isaac-ros.github.io/v/release-3.2/repositories_and_packages/index.html) and AI models designed to streamline and expedite the development of advanced AI robotics applications.

![image](/_fern-files/stereolabs.docs.buildwithfern.com/731f0d4938578ea4dd891078030ca2e8a3cd1206cd2d12577075b275bbe79201/docs/software-integration/isaac-ros/images/how-isaac-ros-works.svg)

## ZED ROS 2 Integration

The [ZED ROS 2 Wrapper](/docs/integrations/ros-2/) automatically integrates the ZED stereo cameras with the NVIDIA® Isaac™ ROS framework, enabling developers to leverage the power of NVIDIA GPUs for real-time perception tasks.

### NITROS Support

When building the ZED ROS 2 Wrapper packages, the build system automatically checks for the presence of the NVIDIA® Isaac™ ROS packages, in particular the [`isaac_ros_nitros` package](https://nvidia-isaac-ros.github.io/v/release-3.2/repositories_and_packages/isaac_ros_nitros/isaac_ros_nitros/index.html). If detected, the ZED Camera ROS 2 components are built with [NITROS](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/index.html) support enabled. NITROS (NVIDIA® Isaac™ Transport for ROS) is a technology that accelerates ROS data streaming by leveraging GPU memory, allowing high-performance data transfer without routing through the CPU.

You can find more information about NITROS and how it works with ROS 2 in the [official NITROS documentation](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/index.html).

> **Note**
>
> If the [`isaac_ros_nitros` package](https://nvidia-isaac-ros.github.io/v/release-3.2/repositories_and_packages/isaac_ros_nitros/isaac_ros_nitros/index.html) is not detected during the build, the ZED ROS 2 Wrapper will still compile and function normally, but NITROS acceleration will not be enabled. You can continue to use your ZED cameras in a standard ROS 2 environment, though you will not benefit from the enhanced data transfer and performance optimizations provided by NVIDIA NITROS.

![image](/_fern-files/stereolabs.docs.buildwithfern.com/09705e0a829969a2174b5cbce17c8ea30905e3ab30a3d9dfd8a2f8ade2c1a5c8/docs/software-integration/isaac-ros/images/nitros-pipeline.gif)

The ZED ROS 2 Wrapper can leverage NITROS thanks to its strong integration with CUDA processing using the [`isaac_ros_managed_nitros` package](https://nvidia-isaac-ros.github.io/v/release-3.2/repositories_and_packages/isaac_ros_nitros/isaac_ros_managed_nitros/index.html).

In particular, the ZED ROS 2 Wrapper uses [Managed NITROS publishers](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/cuda_with_nitros.html#managed-nitros-publisher) to publish images and depth maps directly from the GPU memory, avoiding unnecessary data copies and CPU overhead. This results in significantly improved performance for applications that require high throughput and low latency, such as real-time object detection, mapping, and navigation.

The [Managed NITROS publisher](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/cuda_with_nitros.html#managed-nitros-publisher) and its counterpart, the [Managed NITROS subscriber](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/cuda_with_nitros.html#managed-nitros-subscriber), enable efficient, GPU-accelerated data transfer between the ZED camera node and other Isaac™ ROS nodes. Thanks to [ROS 2 Type Adaptation](https://ros.org/reps/rep-2007.html), these components maintain compatibility with standard (non-Isaac™) ROS 2 nodes by automatically converting data to standard ROS 2 message types when needed, for example to visualize images in RViz2. This seamless integration ensures high performance while preserving interoperability within the ROS 2 ecosystem.

![image](/_fern-files/_img/cbd2f64f12201452c98c1c696b228977eb45c85c15057865787a06b51f9aef5e.webp)

You can find more information about CUDA with NITROS and how it works in the ["CUDA with NITROS" documentation](https://nvidia-isaac-ros.github.io/v/release-3.2/concepts/nitros/cuda_with_nitros.html).

## Get Started

To use the ZED ROS 2 Wrapper with NVIDIA® Isaac™ ROS, you need to install the NVIDIA® Isaac™ ROS packages and configure the environment to support the ZED cameras through the ZED SDK.

### Install NVIDIA® Isaac™ ROS with ZED support and NITROS

[Follow the instructions](/docs/integrations/isaac-ros/legacy/setup-and-installation/) to install the NVIDIA® Isaac™ ROS packages and enable the ZED ROS 2 Wrapper with NITROS support.

## Tutorials and examples

You can find a variety of tutorials and examples to help you get started with the ZED ROS 2 Wrapper and NVIDIA® Isaac™ ROS integration:

* [NITROS Subscriber](/docs/integrations/isaac-ros/legacy/subscribe-to-zed-topics/): Learn how to create a ROS 2 component that subscribes to the ZED camera's image and depth streams using NITROS in an Isaac™ ROS node.
* [AprilTag Detection](/docs/integrations/isaac-ros/legacy/april-tag-detection/): Learn how to use the ZED camera with the AprilTag detection package in an NVIDIA® Isaac™ ROS environment.