> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Setting up Isaac™ ROS 3 to work with ZED Cameras in ROS 2 (Legacy)

> **Warning**
>
> This page belongs to the legacy documentation for **NVIDIA® Isaac™ ROS 3.2** (ROS 2 Humble). It relies on NITROS, which was removed in Isaac™ ROS 5. For new projects, follow the [current Isaac™ ROS documentation](/docs/integrations/isaac-ros/).

This guide will help you set up the NVIDIA® Isaac™ ROS packages to work with the ZED ROS 2 Wrapper.

> **Note**
>
> A solid connection to the internet is required to download the NVIDIA® Isaac™ ROS packages and the StereoLabs software. If you are using a Jetson device, we recommend using a wired connection for better stability and speed.

## NVIDIA® Jetson™ Setup

> **Note**
>
> You can ignore this section if you are not using an NVIDIA® Jetson™ device.

Before installing Isaac™ ROS on an NVIDIA® Jetson™ device, ensure that it is set up correctly and has the necessary software installed.

### Install the prerequisites

Open a terminal \[`Ctrl+Alt+T`] and enter the following commands to install the prerequisites:

```bash
sudo apt-get update
sudo apt-get install python3 python3-pip # Install python3
sudo apt-get install nvidia-jetpack # Install the Jetson developer tools
sudo pip3 install jetson-stats # Optional but recommended to monitor the status of the Jetson™ module
```

### Install the VPI library

[Configure the VPI library](https://nvidia-isaac-ros.github.io/v/release-3.2/getting_started/hardware_setup/compute/jetson_vpi.html) for running compute on Jetson™ device’s PVA accelerator.

1. Generate CDI Spec for GPU/PVA:

   ```bash
   sudo nvidia-ctk cdi generate --mode=csv --output=/etc/cdi/nvidia.yaml
   ```

2. Install `pva-allow-2` package:

   ```bash
   # Add Jetson public APT repository
   sudo apt-get update
   sudo apt-get install software-properties-common
   sudo apt-key adv --fetch-key https://repo.download.nvidia.com/jetson/jetson-ota-public.asc
   sudo add-apt-repository 'deb https://repo.download.nvidia.com/jetson/common r36.4 main'
   sudo apt-get update
   sudo apt-get install -y pva-allow-2
   ```

### Install an additional SSD memory if you are using an NVIDIA® Jetson™ development kit

**Using Isaac™ ROS with Docker requires a fast and large storage solution**, such as an SSD, to ensure optimal performance.

The Docker images can be quite large, and running them on slower storage devices may lead to performance issues.

If you are using an NVIDIA® Jetson™ development kit device, we recommend you follow the official [NVIDIA® documentation for best practices on setting up an NVMe SSD card in the Jetson developer kit’s carrier board](https://nvidia-isaac-ros.github.io/v/release-3.2/getting_started/hardware_setup/compute/jetson_storage.html).

If you are using instead a StereoLabs [ZED Box](https://www.stereolabs.com/store/products/zed-box-orin), [ZED Box Mini](https://www.stereolabs.com/store/products/zed-box-mini), or a [Mini Carrier board](https://www.stereolabs.com/store/products/zed-carrier-mini), the preinstalled NVMe SSD is already configured for optimal performance and no further configuration is required.

## Configure NVIDIA® Isaac™ ROS using Docker

> **Note**
>
> You can skip this section if you are not using Docker to run your Isaac™ ROS applications and prefer to use the [official Apt Repository](/docs/integrations/isaac-ros/legacy/setup-and-installation/#configure-nvidia-isaac-ros-from-the-official-apt-repository).
>
> This setup is recommended when using an NVIDIA® Jetson™ device.

NVIDIA® provides ready-to-use Docker images for using Isaac™ ROS. The Docker configuration allows you to easily set up your development environment with all the necessary dependencies and tools pre-installed on Jetson devices and x86_64 systems.

Please refer to the [official NVIDIA® Isaac™ ROS documentation](https://nvidia-isaac-ros.github.io/v/release-3.2/index.html) for advanced configurations and usage.

1. Install the prerequisite:

   ```bash
   sudo apt-get install python3-pip # Install pip for Python 3
   ```

2. Restart Docker:

   ```bash
   sudo systemctl daemon-reload && sudo systemctl restart docker
   ```

3. Install [Git LFS](https://git-lfs.com/) to pull down all large files:

   ```bash
   sudo apt-get install git-lfs
   git lfs install  --skip-repo
   ```

4. Create a workspace and add it to the environment:

   ```bash
   mkdir -p ~/ros2/isaac_ros_ws/src
   echo "export ISAAC_ROS_WS=${HOME}/ros2/isaac_ros_ws/" >> ~/.bashrc
   source ~/.bashrc
   ```

5. Enter the workspace and clone packages:

   ```bash
   cd ${ISAAC_ROS_WS}/src
   git clone https://github.com/NVIDIA-ISAAC-ROS/isaac_ros_common.git --branch release-3.2 --recurse-submodules
   ```

6. Pull the official Isaac Common Docker image and start the first instance of development environment:

   ```bash
   cd ${ISAAC_ROS_WS}/src/isaac_ros_common && \
   ./scripts/run_dev.sh
   ```

7. Wait for the build to complete. This may take some time :coffee:

8. When the build is complete, the Docker container will start automatically. You can verify that you are inside the Docker container by checking the command prompt, which should look like `admin@ubuntu:/workspaces/isaac_ros-dev$`.

   Enter the command `exit` to leave the Docker container.

For any problems with the installation please refer to the [NVIDIA® Isaac™ ROS Troubleshooting](https://nvidia-isaac-ros.github.io/v/release-3.2/troubleshooting/index.html) documentation.

### Configure NVIDIA® Isaac™ ROS using Docker with ZED cameras

To use Isaac™ ROS with ZED cameras, you must create a Docker layer that installs the ZED SDK in the Isaac™ ROS Docker image. This layer will allow you to use ZED cameras in your Isaac™ ROS applications.

1. Create a new entrypoint script to change the permissions of the ZED SDK folder when the container starts to allow access to non-root users:

   ```bash
   cd ${ISAAC_ROS_WS}/src/isaac_ros_common/docker/scripts
   touch zed-entrypoint.sh
   chmod +x zed-entrypoint.sh
   ```

2. Open the `zed-entrypoint.sh` file in a text editor and add the following content:

   ```bash
   #!/bin/bash

   # Enable ZED if installed
   echo "Checking ZED SDK..."

   ZED_FOLDER=/usr/local/zed/

   if [ -d "${ZED_FOLDER}" ]; then
      echo " * ${ZED_FOLDER} exists. Changing permissions"
      chown -R ${USERNAME}:${USERNAME} ${ZED_FOLDER}
      echo " * ZED SDK available:"
      ${ZED_FOLDER}tools/ZED_Explorer -v
   else
      echo " * $ZED_FOLDER does not exist. ZED SDK not installed"
      exit 1
   fi
   ```

3. Create a new `Dockerfile.zed` file in the `isaac_ros_common/docker` directory:

   ```bash
   cd ${ISAAC_ROS_WS}/src/isaac_ros_common/docker
   touch Dockerfile.zed
   ```

4. Open the `Dockerfile.zed` file in a text editor and add the following content:

   ```dockerfile
   ARG BASE_IMAGE=NONE
   FROM ${BASE_IMAGE} AS catscanners

   # disable terminal interaction for apt
   ENV DEBIAN_FRONTEND=noninteractive
   ENV SHELL=/bin/bash
   SHELL ["/bin/bash", "-c"]

   ARG ARCH=aarch64
   #ARG ARCH=x86_64

   # Copy the SDK install script
   COPY scripts/install-zed-${ARCH}.sh /opt/zed/install-zed.sh

   # Copy the entrypoint script to change the permissions of the ZED SDK folder
   # when the container starts to the correct location
   COPY scripts/zed-entrypoint.sh /usr/local/bin/scripts/entrypoint_additions/zed-entrypoint.sh

   # Install the ZED SDK
   RUN chmod +x /opt/zed/install-zed.sh && \
      /opt/zed/install-zed.sh
   ```

   > **Note**
   >
   > Uncomment the `ARG ARCH=x86_64` line if you are using an x86_64 system instead of a Jetson™ device.

   > **Note**
   >
   > The Dockerfile copies the `zed-entrypoint.sh` script to the `/usr/local/bin/scripts/entrypoint_additions/` directory. This will ensure that the script is executed when the Docker container starts, as the default entrypoint script in the Isaac™ ROS Docker image is designed to run any scripts found in this directory at startup.

5. Modify the `install-zed-<arch>.sh` file to install the latest ZED SDK.

   A. Open the `isaac_ros_common/docker/scripts/install-zed-<arch>.sh` file in a text editor. *Replace `<arch>` with `aarch64` if you are using a Jetson device or `x86_64` if you are using an x86_64 system*.

   B. Replace the content of the file with the following script:

   **Jetson**:

   *click the arrow to expand the full script content*

   <details>
     <summary>
       **scripts/install-zed-aarch64.sh**
     </summary>

     ```bash
     #!/bin/bash

     # Download dependencies for zed SDK installation RUN file
     sudo apt-get update -y || true
     sudo apt-get install --no-install-recommends lsb-release wget less zstd udev sudo apt-transport-https -y

     # Download zed SDK installation RUN file to /tmp directory
     cd /tmp

     URL=https://download.stereolabs.com/zedsdk/5.5/l4t36.4/jetsons
     wget -q --no-check-certificate -O ZED_SDK_Linux.run ${URL}
     SIZE=$(du -sb './ZED_SDK_Linux.run' | awk '{ print $1 }')
     if ((SIZE<1024)) ; then
        echo "ERROR: ZED_SDK_Linux.run size is not valid: ${SIZE}B!!!";
        echo " * Verify the ZED SDK download link validity: " ${URL} ;
        exit 1
     fi

     sudo chmod 777 ./ZED_SDK_Linux.run
     sudo ./ZED_SDK_Linux.run silent skip_od_module skip_python skip_drivers
     # Symlink required to use the streaming features on Jetson inside a container, based on
     # https://github.com/stereolabs/zed-docker/blob/fd514606174d8bb09f21a229f1099205b284ecb6/4.X/l4t/devel/Dockerfile#L27C5-L27C95
     sudo ln -sf /usr/lib/aarch64-linux-gnu/tegra/libv4l2.so.0 /usr/lib/aarch64-linux-gnu/libv4l2.so

     # Install zed-ros2-wrapper dependencies
     sudo apt-get update && sudo apt-get install -y \
        ros-humble-zed-msgs \
        ros-humble-nmea-msgs \
        ros-humble-geographic-msgs \
        ros-humble-robot-localization \
        #ros-humble-point-cloud-transport \
        #ros-humble-point-cloud-transport-plugins \
        #ros-humble-draco-point-cloud-transport \
        #ros-humble-zlib-point-cloud-transport \
        #ros-humble-zstd-point-cloud-transport \

     # Uncomment the point cloud transport packages above if you want to use point cloud compression.

     # Install base Isaac ROS Nitros packages
     sudo apt-get update && sudo apt-get install -y \
        ros-humble-isaac-ros-common \
        ros-humble-isaac-ros-nitros \
        ros-humble-isaac-ros-managed-nitros \
        ros-humble-isaac-ros-nitros-image-type

     # Cleanup
     sudo rm -rf /usr/local/zed/resources/*
     rm -rf ZED_SDK_Linux.run
     sudo rm -rf /var/lib/apt/lists/*
     ```
   </details>

   * If you are using a different version of the JetPack SDK, you must adjust the URL accordingly. For example, if you are using JetPack 6.2.2 (L4T 36.5), you must change `l4t36.4` to `l4t36.5`.

   * If you are using a different version of the ZED SDK, you must adjust the URL accordingly. For example, if you want to install ZED SDK 5.4, you must change `5.5` to `5.4`. Make sure the ZED SDK version matches the one required by the ZED ROS 2 Wrapper version you build.

   **x86_64**:

   *click the arrow to expand the full script content*

   <details>
     <summary>
       **scripts/install-zed-x86_64.sh**
     </summary>

     ```bash
     #!/bin/bash

     # Download dependencies for zed SDK installation RUN file
     sudo apt-get update -y || true
     sudo apt-get install --no-install-recommends lsb-release wget less udev sudo zstd build-essential cmake libpng-dev libgomp1 -y

     # Download zed SDK installation RUN file to /tmp directory
     cd /tmp
     URL=https://download.stereolabs.com/zedsdk/5.5/cu12/ubuntu22
     wget -q --no-check-certificate -O ZED_SDK_Linux.run ${URL}
     SIZE=$(du -sb './ZED_SDK_Linux.run' | awk '{ print $1 }')
     if ((SIZE<1024)) ; then
        echo "ERROR: ZED_SDK_Linux.run size is not valid: ${SIZE}B!!!";
        echo " * Verify the ZED SDK download link validity: " ${URL} ;
        exit 1
     fi

     sudo chmod 777 ./ZED_SDK_Linux.run
     sudo ./ZED_SDK_Linux.run silent skip_od_module skip_python skip_drivers


     # Install zed-ros2-wrapper dependencies
     sudo apt-get update && sudo apt-get install -y \
        ros-humble-zed-msgs \
        ros-humble-nmea-msgs \
        ros-humble-geographic-msgs \
        ros-humble-robot-localization \
        #ros-humble-point-cloud-transport \
        #ros-humble-point-cloud-transport-plugins \
        #ros-humble-draco-point-cloud-transport \
        #ros-humble-zlib-point-cloud-transport \
        #ros-humble-zstd-point-cloud-transport \

     # Uncomment the point cloud transport packages above if you want to use point cloud compression.

     # Install base Isaac ROS Nitros packages
     sudo apt-get update && sudo apt-get install -y \
        ros-humble-isaac-ros-common \
        ros-humble-isaac-ros-nitros \
        ros-humble-isaac-ros-managed-nitros \
        ros-humble-isaac-ros-nitros-image-type

     # Cleanup
     sudo rm -rf /usr/local/zed/resources/*
     rm -rf ZED_SDK_Linux.run
     sudo rm -rf /var/lib/apt/lists/*
     ```
   </details>

   * If you are using a different version of the ZED SDK, you must adjust the URL accordingly. For example, if you want to install ZED SDK 5.4, you must change `5.5` to `5.4`. Make sure the ZED SDK version matches the one required by the ZED ROS 2 Wrapper version you build.

   * If you are using a different version of CUDA, you must adjust the URL accordingly. For example, if you want to install the ZED SDK for CUDA 13, you must change `cu12` to `cu13`.

   * Keep `ubuntu22` in the URL: the Isaac™ ROS 3.2 `ros2_humble` Docker image is based on Ubuntu 22.04.

6. Build the Docker image with the ZED SDK installed:

   ```bash
   cd ${ISAAC_ROS_WS}/src/isaac_ros_common && \
   ./scripts/run_dev.sh -i ros2_humble.zed \
   -a "-v /usr/local/zed/settings:/usr/local/zed/settings \
       -v /usr/local/zed/resources:/usr/local/zed/resources"
   ```

   Wait for the build to complete. This may take some time :coffee:

7. When the build is complete, the Docker container will start automatically. You can check that the ZED SDK is installed by running the following commands inside the Docker container:

   Check the ZED SDK version:

   ```bash
   /usr/local/zed/tools/ZED_Explorer --version
   ```

   Check camera opening and Depth extraction capabilities:

   ```bash
   /usr/local/zed/tools/ZED_Depth_Viewer
   ```

### Install the ZED ROS 2 Wrapper packages

Start a new terminal and enter the Docker container with the ZED SDK installed:

```bash
cd ${ISAAC_ROS_WS}/src/isaac_ros_common && \
./scripts/run_dev.sh -i ros2_humble.zed \
-a "-v /usr/local/zed/settings:/usr/local/zed/settings \
    -v /usr/local/zed/resources:/usr/local/zed/resources"
```

You can now install the ZED ROS 2 Wrapper packages with NITROS support to be used in your Isaac™ ROS applications:

```bash
# Move to the `src` folder of the ROS 2 Workspace
cd ${ISAAC_ROS_WS}/src
git clone https://github.com/stereolabs/zed-ros2-wrapper.git
cd ..
sudo apt-get update
# Install the required dependencies
rosdep install --from-paths src --ignore-src -r -y
# Build the wrapper
colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=Release --packages-up-to zed_wrapper
# Setup the environment variables
echo source $(pwd)/install/local_setup.bash >> ~/.bashrc
source ~/.bashrc
```

If you are new to the ZED ROS 2 Wrapper, we recommend starting with the [Getting Started with ROS 2 and ZED](/docs/integrations/ros-2/) guide. This guide will help you set up your environment and run your first ZED camera application using ROS 2.

You can also explore the [ZED ROS 2 Examples repository](https://github.com/stereolabs/zed-ros2-examples) for tutorials and advanced examples.

> **Note**
>
> If the ZED ROS 2 Wrapper was already installed in your workspace, just clean and rebuild your workspace to ensure that the ZED ROS 2 Wrapper is built with the NVIDIA® Isaac™ ROS support.

```bash
cd ${ISAAC_ROS_WS}
rm -rf build/ install/ log/
colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=Release --packages-up-to zed_wrapper
source install/local_setup.bash
```

You can verify that the ZED ROS 2 Wrapper is built with NVIDIA® Isaac™ ROS support by checking the output of the `colcon build` command. You should see messages indicating that the `isaac_ros_nitros` package is being used:

```cmake
--- stderr: zed_components
 * ISAAC ROS Nitros transport is available
---
```

## Configure NVIDIA® Isaac™ ROS from the official Apt Repository

> **Note**
>
> You can skip this section if you are [using Docker to run your Isaac™ ROS applications](/docs/integrations/isaac-ros/legacy/setup-and-installation/#configure-nvidia-isaac-ros-using-docker).

On Desktop machines, you can easily install the NVIDIA® Isaac™ ROS packages using the official Apt Repository. This repository provides pre-built packages for all supported platforms, making it easy to get started with Isaac™ ROS without using Docker.

> **Note**
>
> We do not recommend this procedure when working with Jetson devices because it's not straightforward to satisfy all dependencies.

NVIDIA® Isaac™ Apt Repository built on NVIDIA's CDN (Content Distribution Network) hosts the following categories of packages for all users.

* All Isaac™ ROS packages pre-built for the currently supported platforms.
* Auxiliary packages to improve developer experience or to support a legacy OS.

### Set up the Isaac™ Apt Repository

Open a terminal and follow these steps to set up the NVIDIA® Isaac™ ROS Apt Repository on your system. This guide assumes you are using Ubuntu 22.04.

1. **Set Locale** - Ensure your system locale is set to UTF-8:

   ```bash
   locale  # check for UTF-8

   sudo apt-get update && sudo apt-get install locales
   sudo locale-gen en_US en_US.UTF-8
   sudo update-locale LC_ALL=en_US.UTF-8 LANG=en_US.UTF-8
   export LANG=en_US.UTF-8

   locale  # verify settings
   ```

2. **Install Dependencies** - Install the required dependencies for the Isaac™ Apt Repository:

   ```bash
   sudo apt-get update && sudo apt-get install gnupg wget
   sudo apt-get install software-properties-common
   sudo add-apt-repository universe
   ```

3. **Setup Source** - Register the GPG key with apt. Two options are listed below, one for .com (US CDN) and one for .cn (China CDN) - choose whichever you prefer.

   #### US CDN

   ```bash
   wget -qO - https://isaac.download.nvidia.com/isaac-ros/repos.key | sudo apt-key add -
   grep -qxF "deb https://isaac.download.nvidia.com/isaac-ros/release-3 $(lsb_release -cs) release-3.0" /etc/apt/sources.list || \
   echo "deb https://isaac.download.nvidia.com/isaac-ros/release-3 $(lsb_release -cs) release-3.0" | sudo tee -a /etc/apt/sources.list
   sudo apt-get update
   ```

   #### China CDN

   ```bash
   wget -qO - https://isaac.download.nvidia.cn/isaac-ros/repos.key | sudo apt-key add -
   grep -qxF "deb https://isaac.download.nvidia.cn/isaac-ros/release-3 $(lsb_release -cs) release-3.0" /etc/apt/sources.list || \
   echo "deb https://isaac.download.nvidia.cn/isaac-ros/release-3 $(lsb_release -cs) release-3.0" | sudo tee -a /etc/apt/sources.list
   sudo apt-get update
   ```

4. **Add the ROS 2 apt repository** - Register the ROS 2 GPG key and package repository with apt:

   ```bash
   sudo apt-get update && sudo apt-get install curl -y
   sudo curl -sSL https://raw.githubusercontent.com/ros/rosdistro/master/ros.key -o /usr/share/keyrings/ros-archive-keyring.gpg
   echo "deb [arch=$(dpkg --print-architecture) signed-by=/usr/share/keyrings/ros-archive-keyring.gpg] http://packages.ros.org/ros2/ubuntu $(. /etc/os-release && echo $UBUNTU_CODENAME) main" | sudo tee /etc/apt/sources.list.d/ros2.list > /dev/null
   ```

You are now ready to install the NVIDIA® Isaac™ ROS packages.

### Install the required NVIDIA® Isaac™ ROS packages

Open a terminal and run the following command to install the required NVIDIA® Isaac™ ROS packages:

```bash
sudo apt-get update
sudo apt-get install ros-humble-isaac-ros-managed-nitros ros-humble-isaac-ros-nitros-image-type
```

### Install the ZED SDK and ZED X Driver

If you haven't already, install the [ZED SDK](/docs/development/zed-sdk/) on your system. On NVIDIA® Jetson™ devices only, also install the [ZED X Driver](/docs/products/embedded/zed-link-capture-card/gmsl2/#setting-up-your-system-for-using-a-gmsl2-camera): it is required to use ZED X, ZED X Mini, ZED X Nano, and ZED X One (GMSL2) cameras with Isaac™ ROS.

### Install the ZED ROS 2 Wrapper

You can now install the ZED ROS 2 Wrapper packages with NITROS support to be used in your Isaac™ ROS applications by following the instructions in the [ZED ROS 2 Wrapper Installation Guide](/docs/integrations/ros-2/#installation).
The ZED ROS 2 Wrapper will automatically detect the available NVIDIA® Isaac™ ROS packages and enable NITROS support during the build process.

If you are new to the ZED ROS 2 Wrapper, we recommend starting with the [Getting Started with ROS 2 and ZED](/docs/integrations/ros-2/) guide. This guide will help you set up your environment and run your first ZED camera application using ROS 2.

You can also explore the [ZED ROS 2 Examples repository](https://github.com/stereolabs/zed-ros2-examples) for tutorials and advanced examples.

> **Note**
>
> If the ZED ROS 2 Wrapper was already installed in your workspace, just clean and rebuild your workspace to ensure that the ZED ROS 2 Wrapper is built with the NVIDIA® Isaac™ ROS support.

```bash
cd ~/your_workspace # e.g. cd ~/devel/ros_ws
rm -rf build/ install/ log/
colcon build --symlink-install --cmake-args -DCMAKE_BUILD_TYPE=Release --packages-up-to zed_wrapper
source install/local_setup.bash
```

You can verify that the ZED ROS 2 Wrapper is built with NVIDIA® Isaac™ ROS support by checking the output of the `colcon build` command. You should see messages indicating that the `isaac_ros_nitros` package is being used:

```cmake
--- stderr: zed_components
 * ISAAC ROS Nitros transport is available
---
```

## Validate the installation

To validate that the installation was successful and that the ZED ROS 2 Wrapper is properly configured with NVIDIA® Isaac™ ROS support, you can run the following command:

```bash
ros2 launch zed_wrapper zed_camera.launch.py camera_model:=<your_camera_model> enable_ipc:=false
```

If the node starts successfully without errors, your installation is likely correct. You can also check the ROS 2 topic list to see if the ZED camera topics are being published:

```bash
ros2 topic list | grep zed
```

You should see topics related to the ZED camera, such as `/zed/zed_node/rgb/color/rect/image/nitros` and `/zed/zed_node/depth/depth_registered/nitros`, indicating that the ZED ROS 2 Wrapper is running with NITROS support as expected.

> **Note**
>
> When using the ZED ROS 2 Wrapper with NVIDIA® Isaac™ ROS, make sure to set the `enable_ipc` parameter to `false` in the launch file to avoid potential conflicts with the NITROS transport. Read more in the [ZED Isaac™ ROS Troubleshooting Guide](/docs/integrations/isaac-ros/legacy/troubleshooting/#i-cannot-start-the-zed-ros-2-node) and the [NVIDIA® Isaac™ ROS Troubleshooting Documentation](https://nvidia-isaac-ros.github.io/v/release-3.2/troubleshooting/dev_env.html#failed-to-load-a-nitros-enabled-nodes-with-intraprocess-communication-enabled).

## Good practices

When starting the Isaac™ ROS Docker container, it's a good practice to enable a few shared volumes to persist your data and configurations across sessions.

Here are some recommended volume mounts:

* `/usr/local/zed/settings:/usr/local/zed/settings` if you plan to use the robot in an area without internet access, and you previously downloaded the camera calibration files by following [this guide](https://support.stereolabs.com/hc/en-us/articles/21614848880791-How-can-I-use-the-ZED-with-Docker-on-a-robot-with-no-internet-connection).
* `/usr/local/zed/resources:/usr/local/zed/resources` if you plan to use the AI module of the ZED SDK (Object Detection, Body Tracking, NEURAL depth), we suggest bind-mounting a folder to avoid downloading and optimizing the AI models each time the Docker image is restarted. The first time you use an AI model inside the Docker image, it will be downloaded and optimized in the local bound-mounted folder, and stored there for the next runs.

To use these volume mounts, use the following command when starting the Docker container:

```bash
cd ${ISAAC_ROS_WS}/src/isaac_ros_common && \
./scripts/run_dev.sh -i ros2_humble.zed \
-a "-v /usr/local/zed/settings:/usr/local/zed/settings \
    -v /usr/local/zed/resources:/usr/local/zed/resources"
```

> **Note**
>
> With [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One) on NVIDIA® Jetson™, also add the volumes required by the ZED X driver to the `-a` argument (`run_dev.sh` already shares `/tmp` on Jetson): `-v /var/nvidia/nvcam/settings/:/var/nvidia/nvcam/settings/` and `-v /etc/systemd/system/zed_x_daemon.service:/etc/systemd/system/zed_x_daemon.service`. See the [Docker volumes reference](/docs/integrations/docker/create-docker-images#volumes) for details.