> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Isaac™ ROS 3 Troubleshooting (Legacy)

> **Warning**
>
> This page belongs to the legacy documentation for **NVIDIA® Isaac™ ROS 3.2** (ROS 2 Humble). It relies on NITROS, which was removed in Isaac™ ROS 5. For new projects, follow the [current Isaac™ ROS documentation](/docs/integrations/isaac-ros/).

Please refer to the following troubleshooting tips if you encounter issues while using the ZED nodes with the NVIDIA® Isaac™ ROS packages.

## I cannot start the ZED ROS 2 node

If you try to start the ZED ROS 2 node and it fails with an error message like this:

```bash
[component_container_isolated-3] terminate called after throwing an instance of 'std::invalid_argument'
[component_container_isolated-3]   what():  intraprocess communication allowed only with volatile durability
[ERROR] [component_container_isolated-3]: process has died [pid 1339364, exit code -6, cmd '/opt/ros/humble/lib/rclcpp_components/component_container_isolated --use_multi_threaded_executor --ros-args --log-level info --ros-args -r __node:=zed_container -r __ns:=/zed'].
```

then you have not disabled the IPC (Intra Process Communication) in the ZED ROS 2 node configuration:

```bash
ros2 launch zed_wrapper zed_camera.launch.py camera_model:=<your_camera_model> enable_ipc:=false
```