> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.stereolabs.com/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server. # ZED Isaac Sim Extension Overview > **Warning** > > This is documentation for previous versions of the **Isaac Sim ZED Extension \< 4.0.0**. > > For the most recent version, please refer to [this page](/docs/integrations/isaac-sim/) The ZED Camera extension for NVIDIA® Isaac Sim enables developers to connect the ZED SDK to their virtual ZED Cameras in Isaac Sim, allowing them to seamlessly simulate ZED-based robotics applications. Some examples of applications: * Smart navigation, where mobile robots autonomously navigate in a virtual environment using the ZED SDK, the ZED ROS 2 wrapper, and any virtual robot rigged with the ZED X camera. * Repeatable testing environment that makes it easier to debug and optimize applications. ![image](/_fern-img/3f0749c55b4ef89d9fcd8bd22eaa16aa7c4001d66382cc4778eb74c272a6cde9.webp) ## ZED Camera extension The extension is available through the community (or third-party) tab in the NVIDIA® Isaac Sim extension manager. It includes the Omnigraph node needed to stream data and the USD model of the ZED X camera. The extension can also be found on the official [StereoLabs GitHub repository](https://github.com/stereolabs/zed-isaac-sim). ## Get started To connect your virtual ZED camera to the ZED SDK, you have to complete the following steps: ### Step 1: Install NVIDIA® Isaac Sim The recommended way to install Isaac Sim is to use the [Omniverse launcher](https://www.nvidia.com/en-us/omniverse/). You can find the [installation instructions here](/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/get-started-with-isaac-sim). ### Step 2: Install the ZED SDK The ZED SDK must be installed on the machine running Isaac Sim. You can find the [installation instructions here](/docs/development/zed-sdk). ### Step 3: Add the virtual camera to your simulation If you haven't already, we recommend familiarizing yourself with Isaac Sim by reading the [Isaac Sim Main Concepts](https://docs.isaacsim.omniverse.nvidia.com/latest/reference_material/reference_glossary.html) section of the official NVIDIA® documentation. Then, get started with the [ZED camera in Isaac Sim](/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/setting-up-the-zed-in-isaac-sim)! ### ROS 2 integration Isaac Sim can be used to simulate robots and generate ZED data for use with ROS 2 and the ZED ROS 2 Wrapper. Follow this [guide](/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/using-the-zed-with-ros-2-in-isaac-sim) to learn how to configure the [*Isaac Sim ROS 2 Bridge*](https://docs.isaacsim.omniverse.nvidia.com/latest/installation/install_ros.html#enabling-the-ros-bridge-extension) to send simulated information to a [*ZED ROS 2 Wrapper*](https://github.com/stereolabs/zed-ros2-wrapper) node. ## Docs - [Getting started with Isaac Sim](https://docs.stereolabs.com/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/get-started-with-isaac-sim.md) - [Setting up ZED Camera in Isaac Sim](https://docs.stereolabs.com/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/setting-up-the-zed-in-isaac-sim.md) - [Using ZED with ROS 2 and Isaac Sim](https://docs.stereolabs.com/docs/integrations/isaac-sim/old-version-of-the-zed-extension-for-isaac-sim/using-the-zed-with-ros-2-in-isaac-sim.md)