> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# How to Use Matlab with ZED

## Introduction

This tutorial is intended for those who want to use the ZED with Matlab. It is divided into two sections:

* The [first part](#capturing-video) shows how to capture video with the camera in Matlab.

* The [second part](#using-the-zed-sdk) explains how to get depth, point cloud and positional tracking data.

![image](https://cdn.sanity.io/images/s18ewfw4/production/1900f7433d543a5d7977d6619d24388e896d5d19-3221x889.webp)

## Capturing Video

This section shows how to open the camera in Matlab and display the raw (unrectified) video feed. To get the rectified video and depth, see the [second part](#using-the-zed-sdk) of this tutorial.

### Prerequisites

You must have a MathWorks account (free) and Matlab installed on your system. Even if you're new to Matlab, this tutorial should be easy to follow.

### Getting started

Open Matlab and in the **Command Window**, enter this command:

```
>> webcamlist
```

You should encounter this error if you've never used Matlab with a webcam before:

```
Error using webcamlist (line 20)
MATLAB Support Package for Webcams has not been installed. Open Support Package Installer to install the Webcam Support Package.
```

If you encounter the error, **click** on the link in the error log. A dialog window should appear that prompts you to install a package to support video acquisition with USB cameras:

![image](/_fern-files/stereolabs.docs.buildwithfern.com/d4dd2744f839a6e2a1d120ae5878799283ea03eee2ed5cceec3ca8cfdfb77e31/docs/software-integration/matlab/images/webcamInstall.png)

Click **Next** and **Log In**. Matlab will ask for your MathWorks account credentials. Go through the MathWorks auxiliary software license agreement. Click **Next** and **Install**. Package installation can take around 10-15 seconds.

When the setup process is finished, uncheck the *“Show support package examples”* check box and click on **Finish**.
Now, in the Matlab Command Window, enter:

```matlab
>> webcamlist
```

You should get this return:

```matlab
ans ='ZED'
```

Perfect! The ZED camera is now properly detected. Open the ZED camera with the following command line:

```matlab
>> cam = webcam
```

and the cam variable will return the current parameters of the camera:

```matlab
cam =

webcam with properties:

Name: 'ZED'
Resolution: '2560x720'
AvailableResolutions: {1x4 cell}
WhiteBalanceMode: 'auto'
Sharpness: 4
Saturation: 5
Hue: 0
Gain: 4
WhiteBalance: 4600
Contrast: 4
Brightness: 4
Exposure: 2
ExposureMode: 'auto'
```

You can also check if the ZED camera is running properly with this command:

```matlab
>> preview(cam)
```

Now start grabbing images with this command:

```matlab
>> img = snapshot(cam);
```

You've just grabbed your first ZED frame in Matlab. If you need real-time video capture, set a loop. The ZED camera will stay active as long as you keep the cam variable in Matlab's environment. To turn off the camera, use this command:

```matlab
>> clear cam
```

Here is a code snippet that demonstrates how to open the ZED, grab side-by-side images and split them into left and right images:

```matlab
clear all;close all;clc;

% Open the ZED
zed = webcam('ZED')
% Set video resolution
zed.Resolution = zed.AvailableResolutions{1};
% Get image size
[height width channels] = size(snapshot(zed))

% Create Figure and wait for keyboard interrupt to quit
f = figure('name','ZED camera','keypressfcn','close','windowstyle','modal');
ok = 1;

% Start loop
while ok
      % Capture the current image
      img = snapshot(zed);

      % Split the side-by-side image into two images
      image_left = img(:, 1 : width/2, :);
      image_right = img(:, width/2 +1: width, :);

      % Display the left and right images
      subplot(1,2,1);
      imshow(image_left);
      title('Image Left');
      subplot(1,2,2);
      imshow(image_right);
      title('Image Right');
      drawnow;

      % Check for interrupts
      ok = ishandle(f);
end

% close the camera instance
clear zed
```

As a result, you should see the left and right images in the same window.

![image](/_fern-img/fbca6b9875bd0f0d8eb5db24a69b4aeda83dd3fb8b1ac7def2028b743638e35e.webp)

## Using the ZED SDK

The purpose of this section is to explain how to use the ZED and its SDK to capture depth and motion tracking in Matlab. Here we use the ability of Matlab to execute C++ code through an intermediate file called MEX file.

### Prerequisites

* Matlab (tested with R2016b version).
* ZED SDK
* ZED Matlab interface available on [GitHub](https://github.com/stereolabs/zed-matlab)

### Package

The Matlab interface contains the following directories:

* **matlab**: Contains Matlab example scripts, such as *ZED\_Camera.m*, *ZED\_DepthSensing.m*, *ZED\_Tracking.m* and *ZED\_PointCloud.m*, that demonstrate the use of the ZED SDK features in Matlab.
* **src**: Contains all the files needed to build the Mex file wrapping the SDK functions.
  In this directory, you will find a **mex** subfolder with a *'mexZED.cpp'* file which contains the ZED SDK functions and the interface with Matlab. This file is referred to as a MEX file; it re-implements the majority of the ZED SDK functions in Matlab. It is provided as a basic container and can be complemented with your own functions.
  * Since Matlab does not handle image representations the same way the ZED SDK does, additional conversion functions are required. They are located in the different *'.hpp'* files in the **include** directory.

In the *'ZED\_Camera.m'* file, the ZED SDK functions can be called using mexZED('..'). Check the *'mexZED.cpp'* to see the list of available functions.

### Build procedure

We need to compile the `mexZED.cpp` file into a MEX file which can be used by Matlab. Usually, MEX files can be directly compiled by Matlab but since several libraries need to be linked (ZED, OpenCV, CUDA), it is easier to use CMake.

**Windows**

In CMake GUI:

* Set *'where is the source code'* as *'zed-matlab\src'*
* Set *'Where to build the binaries'* as *'zed-matlab\build'*
* Make sure to specify an *x64* version of Visual Studio
* Click *'Configure'*
  * You may encounter an error saying 'MATLAB not found...nothing will be built.'
    It means that the 'MATLAB\_ROOT' variable doesn't contain a valid path to your Matlab installation. To solve it, you can create a MATLAB\_ROOT environment variable, reboot, and click on *'Configure'*, or edit the MATLAB\_ROOT variable if it is already displayed in the CMake GUI, e.g. 'MATLAB\_ROOT=C:/Program Files/MATLAB/R2016b'
    ![image](/_fern-img/859d01fb22e539bac4b2b8c5ae80433649b5e1b1930232746d1cd02f5a5c0ea0.webp)
* Click on *'Generate'*
* Click on *'Open Project'*
* Set the Solution Configuration to **Release**
* Build **mexZED**
* Build **INSTALL**
  ![image](/_fern-img/3d61f8cdd87a92877948207fe6072ed788ab9525044847f3891b3a8d31cd1a8b.webp)

**Linux**

Open a terminal in the 'zed-matlab' directory and execute the following command:

```
export MATLAB_ROOT=/usr/local/MATLAB/R2016b
mkdir build
cd build
cmake ../src
make
make install
```

The created Mex file will be copied into `zed-matlab/matlab`. Now you should be able to run the ZED examples!

### Run the Examples

Open Matlab, move to the `zed-matlab/matlab` directory and launch the samples.

![image](/_fern-img/7a919c6d3cce443f5216b9f4234fe33d54fa225ad80be0f3c1909920a0ce6353.webp)

[ZED\_Camera.m](https://github.com/stereolabs/zed-matlab/blob/master/matlab/ZED_Camera.m) shows how to open the ZED, capture video and depth and display a depth histogram.

[ZED\_Tracking.m](https://github.com/stereolabs/zed-matlab/blob/master/matlab/ZED_Tracking.m) shows how to open the ZED, capture images and positional tracking data and draw the 3D position of the camera over time.

[ZED\_PointCloud.m](https://github.com/stereolabs/zed-matlab/blob/master/matlab/ZED_PointCloud.m) shows how to open the ZED, capture images and 3D point cloud. The point cloud is displayed as a mesh.