> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.stereolabs.com/docs/integrations/ros-2/region-of-interest/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server. # Setting the Region of Interest in ROS 2 The ZED SDK provides a "Region of Interest" feature for robotics applications: an area to focus on for all SDK processing, discarding other parts. When mounting a ZED on a robot, parts of the robot itself are often statically visible in the camera's field of view. This fact affects the depth extraction and performance of the positional tracking algorithms because part of the image will be stable even if the camera is moving. The region of interest can be used to ignore these non-useful parts of the frame in the ZED SDK pipeline thus improving the overall performance of the ZED SDK algorithms run by the ZED ROS 2 Wrapper. ## How to use it To set the region of interest of the ZED SDK processing it is necessary to call the API function `sl::Camera::setRegionOfInterest` which requires as an input parameter an image mask of type `sl::Mat` which sets the valid pixel zones of the frames captured, all the pixels with 0 (zero) as value are ignored. ![image](/_fern-files/stereolabs.docs.buildwithfern.com/86da9ce272c24c479669a89987526576cec6e31787b8f7e81f554fb6ad8e396d/docs/software-integration/ros-2/images/roi.gif) The ZED ROS 2 Wrapper automatically creates the required `sl::Mat` starting from a parameter describing a polygon that contains the region of the image to be used during the data processing. The Region of Interest can be generated automatically by the ZED SDK, set when the node starts through a node parameter, or set at runtime by calling a ROS 2 service. All the related parameters live in the `region_of_interest` namespace of [`common_stereo.yaml`](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml). See the [Region of Interest parameters](/docs/integrations/ros-2/zed-stereo-node/#region-of-interest-parameters) reference for the full list. ### Automatic generation Set `region_of_interest.automatic_roi` to `true` to let the ZED SDK detect the parts of the robot in the field of view and remove them from the processing. Two parameters tune the detection: * `region_of_interest.depth_far_threshold_meters`: the maximum distance at which an object is still considered part of the robot. * `region_of_interest.image_height_ratio_cutoff`: the portion of the image to consider, starting from the bottom. The default `0.5` considers only the lower half, which filters out the sky. > **Note** > > When `automatic_roi` is enabled the value of `manual_polygon` is ignored. ### Node parameter The node parameter used to set the region of interest manually is `region_of_interest.manual_polygon`, a string containing the list of the normalized coordinates of the polygon. We use normalized coordinates so it is possible to change the resolution of the images without necessarily changing the definition of the parameter of the Region of Interest. For example, to define a rhomboid-shaped Region of Interest, with the vertices in the central quarter of the frame, set the parameter as follows: ```yaml manual_polygon: "[[0.5,0.25],[0.75,0.5],[0.5,0.75],[0.25,0.5]]" ``` To keep the Region of Interest equal to the full image the polygon must be empty: ```yaml manual_polygon: "" ``` or ```yaml manual_polygon: "[]" ``` ### Selecting the modules Each of the following parameters enables the Region of Interest for one module. They all default to `true`, so set to `false` the ones you want to leave unmasked: * `region_of_interest.apply_to_depth` * `region_of_interest.apply_to_positional_tracking` * `region_of_interest.apply_to_object_detection` * `region_of_interest.apply_to_body_tracking` * `region_of_interest.apply_to_spatial_mapping` ### Visualizing the mask Set `region_of_interest.publish_roi_mask` to `true` to advertise the `~/roi_mask/image` topic, which carries the mask actually applied to the ZED SDK processing. The topic is advertised only when a Region of Interest is active, either automatic or manual, and, as with every other topic of the node, the data is published only while a node is subscribed to it. ### ROS 2 service The custom service to set a new Region of Interest at runtime is defined in the `zed-ros2-interfaces` repository. The service name is `set_roi` and the type is `zed_msgs/srv/SetROI`. The service has a parameter of type string defining the shape of the polygon of the Region of Interest defined in the same way as the node parameter `region_of_interest.manual_polygon`. To reset the Region of Interest to the full image you can call the service `reset_roi` of type `std_srvs/srv/Trigger`.