> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ROS - Data display with RViz

> **Warning**
>
> **The ZED ROS Wrapper packages are no longer maintained** because ROS 1 reached [end-of-life (EOL) on 2025-05-31](https://www.ros.org/blog/noetic-eol/) with the final Noetic release.
>
> We recommend upgrading to [ROS 2](/docs/integrations/ros-2) to take advantage of the latest ZED SDK features for robotics applications.

[RViz](http://wiki.ros.org/rviz) is a ROS graphical interface that allows you to visualize a lot of information, using plugins for many kinds of available topics.

The [`zed_display_rviz`](https://github.com/stereolabs/zed-ros-examples/tree/master/zed_display_rviz) package provides six launch files (`display_zed.launch`, `display_zedm.launch`, `display_zed2.launch`, `display_zed2i.launch`, `display_zedx.launch` and `display_zedxm.launch`) that start preconfigured RViz sessions for the ZED, ZED Mini, ZED 2, ZED 2i, ZED X and ZED X Mini cameras respectively. These sessions load the default RViz plugins preconfigured to show the most commonly used data from the ZED ROS infrastructure.

To create your own RViz configuration, you can use the plugins described below.

## Global options

To be able to visualize the information published by the ZED camera, it is necessary to correctly configure the `Global Options`:

![Global](/_fern-img/d3138220b761db4020346dca45df222ddd7e323404143b02519788069f1fba7f.webp)

Key parameters:

* `Fixed frame`: Indicates the name of the frame used as the reference for all the other frames. You can select any frame available in the combo box. `map` or `odom` are the best choices.
* `Frame rate`: The maximum frequency used to update the 3D view. `30` or `60` FPS are good values. Available computational power should guide your decision.

## Grid

This plugin allows you to visualize a grid normally associated with the floor plane.

Key parameters:

* `Reference frame`: The frame used as reference for the grid coordinates (normally: `<fixed_frame>`)
* `Plane cell count`: The size of the grid in cells
* `Normal cell count`: The number of cells in the direction normal to the grid plane (normally: `0`)
* `Cell size`: Dimensions in meters of each grid cell
* `Plane`: The two axes that identify the grid plane

## Robot model

This plugin allows you to visualize the Robot Model according to its description from the URDF model.
The ZED wrapper generates the camera model from the `zed_descr.urdf.xacro` file, according to the `camera_model` launch argument (`zed`, `zedm`, `zed2`, `zed2i`, `zedx` or `zedxm`).

![Model](/_fern-img/25e6a106f0035bd4a27ffda9c918862058c1b5473c52e9c4a2ed6daa5448bf88.webp)

Key parameters:

* `Visual enabled`: Enable/disable the 3D visualization of the model
* `Robot description`: The parameter containing the robot description. The ZED launch files load it as `<camera_name>_description` (for example `zed_description` with `zed.launch`)

By expanding the `Links` item, you can see the whole model tree, with all the joints and the links available and the relative position and orientation in the space relative to the `fixed frame`.

## TF

This plugin allows you to visualize the position and orientation of all the frames that compose the TF hierarchy.

![TF](/_fern-img/c5ec3fa7b8cca5b61e87d9e1a17c48ccb61e554bb3adebae6076d765ee5b1e8c.webp)

Key parameters:

* `Show names`: Enable/disable the 3D visualization of the names of the links
* `Show axes`: Enable/disable the 3D visualization of the axes of the frames
* `Show arrows`: Enable/disable the 3D visualization of the arrows that connect the various frames
* `Update interval`: The update time in seconds. Leave at `0` to see each update

Critical to using this plugin is the ability to enable/disable visualizing individual frames. This allows you to concentrate only on the parts that are most important for your current task.

## Video

Learn how to configure RViz for visualizing video information by following the [Video with RViz tutorial](/docs/integrations/ros/video-capture/#video-with-rviz).

## Depth Sensing and Mapping

Learn how to configure RViz for visualizing depth information by following the [Depth with RViz tutorial](/docs/integrations/ros/depth-sensing/#depth-with-rviz).

## Positional Tracking

Learn how to configure RViz for visualizing position information by following the [Position with RViz tutorial](/docs/integrations/ros/positional-tracking/#position-with-rviz).

## Object Detection

Learn how to configure RViz for visualizing detected object information by following the [Object Detection with RViz tutorial](/docs/integrations/ros/object-detection-and-tracking/#object-detection-with-rviz).