> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# AR Video Passthrough with Unity

In this tutorial, you will learn how to turn the scene you built in the [Build your First AR/MR App](/docs/integrations/unity/build-your-first-ar-mr-application/) tutorial into a stereo pass-through AR experience.

## Requirements

* ZED Mini

* Supported VR headset:

  * Oculus Rift
  * HTC Vive
  * HTC Vive Pro\*
  * Windows Mixed Reality headset\* (via SteamVR only)

* VR-ready PC (GTX 1070 GPU or greater recommended)

\* StereoLabs' ZED Mini mounting bracket was designed for the Oculus Rift and original HTC Vive. It can fit on some WMR headsets like the Samsung Odyssey, but you will need to create a custom attachment for the Vive Pro or other WMR headsets.

## Set Up your ZED Mini

To set up the ZED Mini on your headset, follow our guides for [Oculus Rift](https://www.stereolabs.com/zed-mini/setup/rift/) and [HTC Vive](https://www.stereolabs.com/zed-mini/setup/vive/). Use the provided straps to attach the cable to the headset, and make sure to plug the USB Type-C cable into your ZED Mini with the arrows facing forward.

## Enable Virtual Reality

* Go to **Edit** -> **Project Settings** -> **XR Plug-in Management** -> Click on **Install XR Plugin Management**.
* Now you need to choose which Provider to use. The ZED Unity Plugin is compatible with **OpenVR**, **Oculus** and **OpenXR**.

## Add the Stereo Rig

* Follow the steps described in the [Build Your First AR/MR App](/docs/integrations/unity/build-your-first-ar-mr-application/) tutorial.

* In your Hierarchy, delete the **ZED\_Rig\_Mono** prefab you added in the last tutorial.

* In the Project window, go to the **Packages** -> **ZED SDK** -> **Prefabs** folder. Click and drag the **ZED\_Rig\_Stereo** prefab into the Hierarchy window.

  ![image](/_fern-img/2e1569c0d5de963eca0256e684fe02c5d153193f56d5166634a3b49eaa684b98.webp)

## Run the Scene

Run the scene and put on your headset. Take a look at the sphere and the shadow beneath it. Walk around it, put your hand over and under it. You can also move the sphere in the Scene window and watch it fly across your room. You've built your first ZED Mini AR app!

![image](https://cdn.sanity.io/images/s18ewfw4/production/6c04dfdea01a474826bc1341452f76337b695025-1259x706.webp)

## Tips

* To see a similar scene already put together, import the Planetarium sample from the Package Manager and open the Planetarium scene in **Assets** -> **Samples** -> **ZED SDK** -> *version* -> **Planetarium** -> **Scene**.
* If you want to disable inside-out positional tracking to use Oculus or Vive external tracking systems, go to **ZED Manager** and uncheck *Enable Positional Tracking*. This will disable our Video Async Timewarp effect for latency compensation but can improve tracking accuracy in some situations.