> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Build your first AR/MR App with Unity

In this tutorial, you will learn how to create a simple mixed reality application.

## Create a new Project

* Run Unity.
* Select **File** > **New Project**.
* Select 3D mode and click **Create project**.
* Make sure the ZED SDK is installed, and [install the ZED Unity plugin](/docs/integrations/unity/#step-3-import-the-plugin) through the Package Manager.
* After importing the package, set the aspect ratio of your Game Window to **16:9** with a scale of **1x**. If the aspect ratio and scale are anything else, the image will appear distorted or blurry in the main window.

  ![image](/_fern-img/05c0551c09cab928347aa3c3b368f4d3f521f9afab9aeb83d45f6e45b3d05988.webp)

## Add the AR camera

Here we will add the **ZED Rig** prefab to the scene to replace Unity's conventional camera. The ZED Rig appears at (0,0,0) with -Z representing the forward direction facing the camera.

* In the Hierarchy panel, delete the Main Camera.
* In the Project panel, navigate to *Packages > ZED SDK > Prefabs*.
* Drag the **ZED\_Rig\_Mono.prefab** into the Hierarchy.

  ![image](/_fern-img/3d8625315a8d0a971cf4a2c98773510d9515577147138aca57a6d51cbbb12d3b.webp)

## Enable Positional Tracking

* Click on **ZED\_Rig\_Mono** in the Hierarchy to display the attached **ZED Manager** script in the Inspector panel.

  ![image](/_fern-img/f3bbd66f0d17431d96bde253dcbc456ca0779c5d7ab9d56ace9fa6774c372f5b.webp)

* Enable **Positional Tracking** so that the pose of the virtual camera follows the movement of the device in the real world.

* Enable **Spatial Memory**. This allows the ZED to detect and correct positional tracking drift while moving and maintains the real world position of virtual objects.

  ![image](/_fern-img/6fa6e788f7d8d42031ed5dafb71fa810144def53763b08f8665fc35b5f8666c7.webp)

## Adding AR Passthrough to HMD

This assumes you have a VR headset (Oculus Rift, HTC Vive, HTC Vive Pro or Windows Mixed Reality headset) with a ZED Mini mounted on the front.

* If you used **ZED\_Rig\_Mono** in the last steps, replace it with **ZED\_Rig\_Stereo**.
* Go to **Edit** -> **Project Settings** -> **XR Plug-in Management** -> Click on **Install XR Plugin Management**.
* Now you need to choose which Provider to use. The ZED Unity Plugin is compatible with **OpenVR**, **Oculus** and **OpenXR**.
* If you select **OpenXR**, make sure the corresponding **Interaction Profile** is selected in the OpenXR option panel.
* Run the scene and put on the headset.

## Add a Virtual Object

Let's add a virtual sphere to the scene. When you add virtual content, make sure to move it into the field of view of the camera and leave the camera rig at its origin (0,0,0). The field of view of the rig is automatically determined by the camera calibration parameters, and rig position is updated by positional tracking.

* To add a sphere to the scene, right-click in the Hierarchy and select **3D Object > Sphere**.
* The sphere should appear at the camera's origin. Move the sphere 2 meters away from the camera by setting the sphere's position to X = 0, Y = 0 and Z = 2.

![image](/_fern-img/a61eceea34772b0bc5402e22acbcd3e920bc1ddc20011a14d8a090215b98dfc5.webp)

* Now you can click on **Play** to see the virtual sphere in the real world and move around it.

To properly align the vertical axis of Unity with the real world, the plugin automatically uses the gravity provided by the inertial sensor of the camera (all models except the original ZED). If using the original ZED, the plugin makes no assumptions about the 3D world. Axis alignment is not guaranteed unless you maintain the device parallel to the floor before playing a scene.

> **Note**
>
> Unity's default scale is in **meters**, which affects physics, terrain, gravity, etc. To make sure your 3D objects integrate and behave realistically with respect to the real world, always use meters and keep your units consistent, especially when creating and importing artwork from third-party software such as Maya or Blender.