> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# AR Lighting and Shadows with Unity

In this tutorial, you will learn how to illuminate the real world with virtual lights, and cast shadows on it from virtual objects.

We will use the project created in the previous tutorial, [Build your first AR/MR App](/docs/integrations/unity/build-your-first-ar-mr-application/).

## Adding Lights

* In the Hierarchy, click on **Camera\_Left**.

  ![Hierarchy camera](/_fern-img/8f85a707d967ce3570c07146df79fde82ac5fc6f852e1b04c4d6660fc9fdd961.webp)

* Right-click the ZED\_Rig prefab object in the Hierarchy panel, and select **Light** > **Spotlight**. You should see the spotlight pointing in the same direction as the camera in the Scene window. (If not, adjust the position and rotation so that it is).

* With the spotlight selected, click on the white box beside **Color** in the Inspector window. Select a bright and distinct color, like red.

* Make sure the sphere you added in the last tutorial still has its position set to X = 0, Y = 0 and Z = 2. If you click on the Spotlight again, its "cone" of light should be touching the sphere.

  ![image](/_fern-img/e3bf6209c43f2f244c7ee32cbe8197e736def1f70021c401e3eeadce2801eef7.webp)

* In the Inspector panel, select your [Rendering Path](https://docs.unity3d.com/Manual/RenderingPaths.html) (**Deferred** or **Forward**). We recommend using Forward Rendering for better performance. See below for details on how each will affect your scene.

If you choose Deferred Rendering, your scene is ready to go. If you choose Forward, you must follow one more step.

### Forward Rendering

[Forward rendering](https://docs.unity3d.com/Manual/RenderTech-ForwardRendering.html) is the default rendering path in Unity. This rendering mode is very fast and allows the use of anti-aliasing (MSAA) which greatly improves the integration of virtual objects in real images. However, you are limited to 8 lights at a time that will affect the real world, and must attach a script to each of them.

To enable illumination of the real world with virtual lights, attach a script called **ZEDLight.cs** located in *SDK/Helpers/Scripts/Lighting* to each light you want to use. A light without a script will only illuminate virtual objects.

![Lights](/_fern-img/7b2ba76ee6a5560e8607f159b6cb08f32f6ebd835f21d4a0dbdd075ab85111c4.webp)

### Deferred Rendering

In deferred rendering, you do not need to add any scripts to your lights. The ZED plugin has its own custom deferred lighting pass that handles mixed-reality lighting. However, this path is less performant and will not allow you to use the [Garbage Matte](/docs/integrations/unity/green-screen-vr-capture/#garbage-matte) feature of the plugin's green screen component.

## Casting Shadows

To allow virtual objects to cast shadows on the real world, you need to add a **Directional Light** to the scene. In Forward rendering, attach the **ZEDLight** component to it, as described above: this makes the light cast shadows on the real world, and also illuminate it.

* To enable shadows, add a Directional Light to your scene from the *GameObject->Light* menu.

  ![Lights](/_fern-img/a2aecbdd7a7b21e9177959ab53f0245c929de4dd85a1109537ca5cc1abf89438.webp)

* Set Shadow Type to **Soft Shadows** and adjust the Strength value. A value of 0.2 or lower usually works well for most scenes.

* Adjust the directional light angle to **90 degrees** in the Transform panel. This will project shadows directly under the virtual objects.

  ![Lights](/_fern-img/2cb9b1460d9594a24c347894222fb0248279d1be5bf1da2ed422aad0a0e0c958.webp)

## Play the scene

You can now run your scene. You'll see colored light on both the sphere and the real world behind it, and the sphere will cast shadows on the floor if you added a Directional Light to the scene. You can play with the **Range** and **Intensity** values on the spotlight to make it stronger.