> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# How to Use YOLO with ZED

## Introduction

This package lets you use [YOLO models](https://docs.ultralytics.com/), a family of deep learning models for object detection, with the ZED stereo camera in Python or C++.

It enables the use of ZED 3D cameras with YOLO object detection, adding 3D localization and tracking to the most recent YOLO models.

![image](/_fern-img/af6751d6577100997dd55ca0de8a1d5de0867f33cf3d0abf477f008dff22fc61.webp)

These samples are designed to run state-of-the-art object detection models using the highly optimized TensorRT framework. Images are captured with the ZED SDK, and the 2D box detections are then used by the ZED SDK to extract 3D information (localization, 3D bounding boxes) and perform tracking.

The samples use a TensorRT-optimized ONNX model. They are currently compatible with YOLOv5, YOLOv6, YOLOv7, YOLOv8, YOLOv10, YOLOv11, YOLOv12, and YOLO26. If another architecture or future model uses the same output format as one of the supported models, it should also be compatible. The default model trained on the COCO dataset (80 classes) provided by the framework maintainers can be used.

A custom detector can also be trained using the same architecture. The following tutorials walk you through the process of training a custom detector:

* YOLOv6: [https://github.com/meituan/YOLOv6/blob/main/docs/Train\_custom\_data.md](https://github.com/meituan/YOLOv6/blob/main/docs/Train_custom_data.md)
* YOLOv5: [https://github.com/ultralytics/yolov5/wiki/Train-Custom-Data](https://github.com/ultralytics/yolov5/wiki/Train-Custom-Data)

## Installation

[ZED YOLO](https://github.com/stereolabs/zed-yolo) depends on the following libraries:

* ZED SDK and [Python API](/docs/development/api-languages/python)
* TensorRT (installed by the ZED SDK with the AI module)
* OpenCV
* CUDA

## Workflow

There are two main ways of running a YOLO ONNX model with the ZED and TensorRT:

1. **\[Recommended]** Use the `OBJECT_DETECTION_MODEL::CUSTOM_YOLOLIKE_BOX_OBJECTS` mode in the ZED SDK API to natively load a YOLO ONNX model. The inference code is fully optimized and internally uses TensorRT. The output is directly available as 2D and 3D tracked objects. This is the easiest and most optimized solution for supported models. ONNX to TensorRT engine generation (optimized model) is automatically handled by the ZED SDK.

   The model format is inferred from the output tensor size. If a future model uses a similar output format to the supported models, it should work.

2. **\[Advanced – for unsupported models]** Use external code for TensorRT model inference, then ingest the detected boxes into the ZED SDK. This approach is for advanced users, as it requires maintaining the inference code. It is suitable for models not supported by the previously mentioned method.

### Supported output formats

The ZED SDK detects the model type from the shape of the ONNX output tensor. The supported YOLO versions produce one of the following formats (shown for an 80-class COCO model; `N` is the number of candidate boxes and scales with the input resolution):

| Output shape  | Layout                                                            | YOLO versions                                           |
| ------------- | ----------------------------------------------------------------- | ------------------------------------------------------- |
| `[1, N, 85]`  | `N` boxes × (4 bbox + 1 objectness + 80 classes)                  | YOLOv5 (original repository), YOLOv7                    |
| `[1, N, 85]`  | `N` boxes × (4 bbox + 1 objectness + 80 classes), anchor-free     | YOLOv6                                                  |
| `[1, 84, N]`  | (4 bbox + 80 classes) × `N` boxes, no objectness                  | YOLOv8, YOLOv11, YOLOv12, YOLOv5u (Ultralytics package) |
| `[1, 300, 6]` | up to 300 boxes × (4 bbox + score + class), end-to-end (NMS-free) | YOLOv10, YOLO26                                         |

For a custom model with `nc` classes, the class dimension changes accordingly (`nc + 5`, `nc + 4`); the end-to-end format stays `[1, 300, 6]`. Any model whose ONNX output matches one of these shapes should work, including future versions.

> **Note**
>
> The first time the SDK loads a given ONNX model, it generates an optimized TensorRT engine for your GPU. This is a one-time step that can take from a few seconds to a few minutes depending on the model and hardware; the resulting engine is cached and reused on subsequent runs.

## Exporting the model to ONNX (mandatory step)

Refer to the [YOLO ONNX Export](/docs/integrations/yolo/exporting-yolo-onnx-models) page to export your YOLO model to ONNX for compatibility. Depending on the version, there may be multiple export methods, and not all are compatible or optimized.

You can use the default model trained on the COCO dataset (80 classes) provided by the framework maintainers, or a custom-trained model.

## Using the ONNX model

* Use the dedicated GitHub repository samples available at [ZED YOLO GitHub](https://github.com/stereolabs/zed-yolo) to run the ONNX model with the ZED SDK.

* More samples are also available at the [ZED SDK GitHub](https://github.com/stereolabs/zed-sdk/tree/master/object%20detection).