> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED - USB 3

Congratulations on being the owner of a brand-new ZED USB 3 camera!

You can use it for a wide range of applications, from robotics and drones to virtual reality and augmented reality. The ZED camera provides high-definition stereo video and depth perception, enabling you to create immersive experiences and advanced computer vision applications.

This guide will help you get started with your ZED camera, from unpacking it to running your first application.

> **Note**
>
> If you are the owner of a ZED X stereo camera, please refer to the [**ZED X Getting Started Guide**](/docs/products/cameras/zedx/) for specific instructions related to that model.

> **Note**
>
> If you are the owner of a ZED X One monocular camera, please refer to the [**ZED X One Getting Started Guide**](/docs/products/cameras/zedxone/) for specific instructions related to that model.

## What's in the Box?

Let's review the items you have received:

| **ZED 2i**                       | **ZED Mini**                           |
| -------------------------------- | -------------------------------------- |
| A brand new ZED 2i Stereo camera | A brand new ZED Mini camera            |
|                                  | A 1.5m and a 4m external USB 3.0 cable |

![image](/_fern-img/7253febed8748fd7608d11c35a70176a2d2c4eea4bbde69b2d6e625a89c76bc5.webp)

## Connect your camera

Unpack your camera, plug it into a USB 3.0 port, and go to the next step. ZED cameras are all UVC compliant, so they should be automatically recognized by your computer.

Some frequently asked questions:

* How to use [multiple cameras](https://support.stereolabs.com/hc/en-us/articles/207678815-How-do-I-use-multiple-ZED-cameras-on-one-computer) on a single platform.
* How to extend the USB [working distance](https://support.stereolabs.com/hc/en-us/articles/212542089-Can-I-use-the-ZED-camera-with-an-extension-cable) of your camera.
* How to fix USB 3.0 [connection issues](https://support.stereolabs.com/hc/en-us/articles/207635225-How-to-fix-USB-3-0-bandwidth-and-connection-issues) or drop frames.
* To turn your ZED into an IP camera and transmit video over IP, see the [Local Streaming](/docs/development/zed-sdk/modules/camera/local-network-streaming/) section.

## Download and install the ZED SDK

The [ZED SDK](https://www.stereolabs.com/developers/release/) is available for Windows, Linux and NVIDIA® Jetson™ platforms.
It contains all the libraries that power your camera along with tools that let you test its features and settings.

Select your platform and follow the installation guide: [Windows](/docs/development/zed-sdk/windows/), [Linux](/docs/development/zed-sdk/linux/), [Jetson](/docs/development/zed-sdk/linux/work-with-nvidia-jetson/).

## Test the camera with the ZED Tools

Test the capabilities of your brand new ZED camera with the [**ZED Tools**](/docs/development/zed-tools/), a set of applications that provide a user-friendly interface to visualize and interact with the data captured by your new device.

## Play with the code samples

The ZED SDK includes several [tutorials](/docs/tutorials/) and [samples](/docs/samples) to learn how to use video, depth, positional tracking, mapping and other information, along with many third-party [integrations](/docs/integrations).

You can also check our [GitHub](https://github.com/stereolabs) page for the latest updates. Read the [API documentation](/docs/development/api-languages/api-reference) and start experimenting with the samples!

## Using ZED with a Virtual Display

For remote access to your ZED system, running on an NVIDIA® Jetson™ device, a virtual display lets you run GUI applications and development tools without a physical monitor or HDMI dongle. This is ideal for headless robotic setups where you need to use the ZED SDK remotely through VNC, NoMachine, or X11 forwarding.

Follow the ["Virtual Display on NVIDIA® Jetson™"](/docs/development/zed-sdk/linux/work-with-nvidia-jetson/virtual-display-headless-mode/) guide to configure a software-based virtual display for your environment.

## Using Docker

For deployment in production environments, we recommend packaging and running your applications and the ZED SDK in [Docker](/docs/integrations/docker/) containers.

## Hardware reference

* [Specifications](/docs/products/cameras/zed/specifications) - image sensors, depth sensing, optics, mechanical drawings, part numbers, and compliance.
* [Datasheets](https://www.stereolabs.com/datasheets) - the official datasheets.
* [CAD Files](https://www.stereolabs.com/3dmodels) - the most up-to-date CAD files of all our products.