> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Remote access via Serial Console

The ZED Box Mini and Mini Carrier Board provide a Serial Console interface for low-level access to the system, via the Micro USB2.0 Type-B port. This is useful when no display is connected to the HDMI port.

> **Note**
>
> The Serial Console is available only when the device is:
>
> * Booting up
> * Booted into Normal Mode (not Recovery Mode)

## Connecting to the Serial Console

* Connect a Micro USB cable from your host computer to the [Micro USB2.0 - OTG](/docs/products/embedded/zed-box-mini/connectivity/#micro-usb-20---otg) port of the ZED Box Mini or Mini Carrier Board.

  ![image](/_fern-img/db6b816b985bf4cd754ac15373eb1adae75a493aa08a45fda51dc2a86ab1c31a.webp)

* Power on the ZED Box Mini or Mini Carrier Board.

* On the host computer, open a terminal (`Ctrl+Alt+T`) and install `gtkterm` if not already installed:

  ```bash
  sudo apt-get install gtkterm
  ```

* Launch `gtkterm` from the terminal with the appropriate device path (usually `/dev/ttyACM0`):

  ```bash
  sudo gtkterm -p /dev/ttyACM0
  ```

  > **Info**
  >
  > You can use other terminal emulators such as `minicom` or `screen` if you prefer.

* If the cable is connected before the device is powered on, the Serial Terminal will display all the boot messages as the device starts up. When the boot is complete, you will see a login prompt.

  > **Note**
  >
  > If the cable is connected when the boot procedure is completed, the terminal will not display any boot messages; you may need to press `Enter` a couple of times to see the login prompt.

  ![image](/_fern-img/f9bb7b4d49f005a6ac57f697dec63ad1cc34e78110d75ba0e741e2bf0548d0fa.webp)

* Log in with your credentials (default credentials: `user`/`admin`)

  ![image](/_fern-img/358f21e1b52b2ce6b0dfca7a6fe7779f3779350025e4daf3405d1786024c9e65.webp)

* You can now execute commands on the device via the Serial Console in the same way as you would via SSH.