> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.stereolabs.com/docs/products/embedded/zed-box-orin/power-modes/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server. # Power Modes The NVIDIA® Jetson™ module of the **ZED Box Orin** supports several **power modes**. Each power mode caps the number of online CPU cores, the number of active GPU TPCs, and the maximum frequencies of the CPU, GPU, DLA, and memory (EMC) to keep the module within a given power budget. Choosing the right power mode lets you trade performance against power consumption and heat. This is important on the ZED Box Orin, which uses a **passively cooled enclosure** with no fan. ## Power supply of the ZED Box Orin The ZED Box Orin can be powered in two ways: | Power source | Power input | | -------------------------------------------------- | ------------------------- | | **DC barrel jack**, with the provided power supply | 12V to 19V, up to **60W** | | **PoE+**, through a PoE+-enabled network switch | up to **25.5W** | With the DC barrel jack, you can use all the [supported power modes](#supported-power-modes) of your module. > **Note** > > With PoE+, the 25.5W budget is shared by the whole system: the Jetson module, the connected cameras, and the USB devices. Choose a power mode that keeps the total consumption of your setup below this limit, and use the DC barrel jack for the highest power modes with several cameras. ## Supported power modes The tables below list the power modes supported by the ZED Box Orin for each Jetson module, with their `nvpmodel` ID and main clock limits. #### Orin Nano 8GB | Mode | ID | Online CPU cores | CPU max (MHz) | GPU max (MHz) | Memory max (MHz) | | ---- | -- | ---------------- | ------------- | ------------- | ---------------- | | 15W | 0 | 6 | 1510.4 | 624.75 | 2133 | | 7W | 1 | 4 | 960 | 408 | 2133 | #### Orin NX 8GB | Mode | ID | Online CPU cores | CPU max (MHz) | GPU max (MHz) | Memory max (MHz) | | ---- | -- | ---------------- | ------------- | ------------- | ---------------- | | MAXN | 0 | 6 | 1984 | 765 | 3200 | | 10W | 1 | 4 | 1190.4 | 612 | 2133 | | 15W | 2 | 4 | 1420.8 | 612 | 3200 | | 20W | 3 | 6 | 1497.6 | 408 | 3200 | #### Orin NX 16GB | Mode | ID | Online CPU cores | CPU max (MHz) | GPU max (MHz) | Memory max (MHz) | | ---- | -- | ---------------- | ------------- | ------------- | ---------------- | | MAXN | 0 | 8 | 1984 | 918 | 3200 | | 10W | 1 | 4 | 1190.4 | 612 | 2133 | | 15W | 2 | 4 | 1420.8 | 612 | 3200 | | 25W | 3 | 8 | 1497.6 | 408 | 3200 | > **Warning** > > **MAXN** is an unconstrained mode, available on the Orin NX modules, that enables the maximum number of cores and the maximum clock frequencies. It has no fixed power budget: hardware throttling is engaged when the module power exceeds its limit, so MAXN does not always give the best performance, and NVIDIA does not recommend running heavy workloads in this mode for prolonged periods. > > The ZED Box Orin is passively cooled: if the system becomes unstable in MAXN mode, add active cooling, for example a fan blowing on the enclosure, or select a mode with a fixed power budget. With PoE+, use MAXN only if your whole setup stays within the 25.5W budget. > **Note** > > * Always check the modes defined on your device, as described in [Check the current power mode](#check-the-current-power-mode), before switching. > * A higher power budget does not always mean a faster GPU. For example, on the Orin NX, the 20W and 25W modes enable more CPU cores but cap the GPU at a lower frequency than the 15W mode. Benchmark your own application in each candidate mode to find the one that suits it best. The complete clock configuration of each mode, including DLA, PVA, and SoC engine frequencies, is available in the [NVIDIA Jetson Linux Developer Guide](https://docs.nvidia.com/jetson/archives/r39.2/DeveloperGuide/SD/PlatformPowerAndPerformance/JetsonOrinNanoSeriesJetsonOrinNxSeriesAndJetsonAgxOrinSeries.html#supported-modes-and-power-efficiency). ## Check the current power mode Display the active power mode: ```bash sudo nvpmodel -q ``` The command prints the name and the ID of the mode. For example, on an Orin NX 16GB in MAXN mode: ```console NV Power Mode: MAXN 0 ``` List all the power modes defined on your device, with their IDs and names, and the default mode applied after flashing: ```bash grep "^< POWER_MODEL\|^< PM_CONFIG" /etc/nvpmodel.conf ``` For example, on an Orin NX 16GB: ```console < POWER_MODEL ID=0 NAME=MAXN > < POWER_MODEL ID=1 NAME=10W > < POWER_MODEL ID=2 NAME=15W > < POWER_MODEL ID=3 NAME=25W > < PM_CONFIG DEFAULT=2 > ``` On the Ubuntu desktop, the current power mode is also displayed next to the NVIDIA icon in the top bar. ## Change the power mode ### From the command line Select a power mode by its ID: ```bash sudo nvpmodel -m ``` For example, to select the 25W mode of an Orin NX 16GB, which has ID `3`: ```bash sudo nvpmodel -m 3 ``` The selected power mode **persists across reboots** until you change it again. Some mode changes modify the number of active GPU TPCs, which can only be applied at boot. In this case, `nvpmodel` asks for a reboot: ```console NVPM WARN: Golden image context is already created NVPM WARN: Reboot required for changing to this power mode: 0 NVPM WARN: DO YOU WANT TO REBOOT NOW? enter YES/yes to confirm: ``` Type `yes` to reboot immediately. The new mode is applied after the reboot. ### From the Ubuntu desktop 1. Click the NVIDIA icon in the top bar. The current power mode is displayed next to it. 2. Open the **Power mode** submenu and click the mode you want to set. ![Power mode menu of the nvpmodel GUI](/_fern-files/stereolabs.docs.buildwithfern.com/65eb9664124089c65bf93a45dfdb95d7ca07a02cc06beaba6d85cb23e91eae65/docs/products/embedded/zed-box-orin/images/power-mode-menu.webp) *Power mode menu on a ZED Box Orin NX 16GB. The modes listed depend on your Jetson module.* 3. If the new mode requires a reboot, a dialog asks for confirmation. Click **OK** to reboot and apply the new mode. ![Reboot confirmation dialog](/_fern-files/stereolabs.docs.buildwithfern.com/3e58794dc35638ba31eeadfa02094afa9395a84a99f9036b6968a416f6887f71/docs/products/embedded/zed-box-orin/images/power-nvpmodel-gui-reboot.webp) ## Maximize the clocks with jetson\_clocks By default, the CPU, GPU, and memory frequencies scale dynamically with the load (DVFS), up to the limits of the active power mode. The `jetson_clocks` script locks these clocks at the **maximum frequencies of the current power mode**. This reduces latency and gives more stable performance, for example during benchmarks, at the cost of a higher idle power consumption. `jetson_clocks` never exceeds the limits of the power mode: select the power mode first, then run `jetson_clocks`. | Command | Description | | ------------------------------ | --------------------------------------------------------------------- | | `sudo jetson_clocks --show` | Display the current clock settings | | `sudo jetson_clocks --store` | Save the current clock settings to `~/.jetsonclocks_conf.txt` | | `sudo jetson_clocks` | Lock the clocks at their maximum frequency for the current power mode | | `sudo jetson_clocks --restore` | Restore the clock settings saved with `--store` | To return to dynamic frequency scaling later, store the settings before maximizing the clocks: ```bash sudo jetson_clocks --store sudo jetson_clocks # ... run your workload ... sudo jetson_clocks --restore ``` > **Note** > > * The effect of `jetson_clocks` does **not** persist across reboots. > * After running `jetson_clocks`, you cannot change the power mode with `nvpmodel` anymore. Reboot the device first. ## Create a custom power mode If none of the predefined modes suits your application, you can define a custom power mode, for example to keep more CPU cores online at a lower frequency, or to cap the GPU frequency. 1. Use the [NVIDIA Jetson Power Estimator](https://jetson-tools.nvidia.com/powerestimator/) to estimate the power consumption of your configuration and to generate the corresponding `nvpmodel` configuration. 2. Back up the current configuration file: ```bash sudo cp /etc/nvpmodel.conf /etc/nvpmodel.conf.bak ``` `/etc/nvpmodel.conf` is a link to the configuration file of your module, for example `/etc/nvpmodel/nvpmodel_p3767_0000.conf` for the Orin NX 16GB. 3. Edit `/etc/nvpmodel.conf` and add a new `< POWER_MODEL ID= NAME= >` block. The easiest way is to copy the block of the closest existing mode, then: * give it a **unique** `ID` and a descriptive `NAME`, * enable or disable CPU cores with the `CPU_ONLINE CORE_ 1|0` lines, * adjust the `MIN_FREQ` and `MAX_FREQ` values. CPU frequencies are expressed in **kHz**; GPU, memory (EMC), DLA, and PVA frequencies in **Hz**. A value of `-1` means no limit. For reference, this is the 15W mode of an Orin NX 16GB, with 4 CPU cores online, the CPU capped at 1420.8 MHz, and the GPU capped at 612 MHz: ```text < POWER_MODEL ID=2 NAME=15W > CPU_ONLINE CORE_0 1 CPU_ONLINE CORE_1 1 CPU_ONLINE CORE_2 1 CPU_ONLINE CORE_3 1 CPU_ONLINE CORE_4 0 CPU_ONLINE CORE_5 0 CPU_ONLINE CORE_6 0 CPU_ONLINE CORE_7 0 FBP_POWER_GATING FBP_PG_MASK 2 TPC_POWER_GATING TPC_PG_MASK 252 GPU_POWER_CONTROL_ENABLE GPU_PWR_CNTL_EN on CPU_A78_0 MIN_FREQ 729600 CPU_A78_0 MAX_FREQ 1420800 GPU MIN_FREQ 0 GPU MAX_FREQ 612000000 GPU_POWER_CONTROL_DISABLE GPU_PWR_CNTL_DIS auto EMC MAX_FREQ -1 DLA0_CORE MAX_FREQ 614400000 DLA1_CORE MAX_FREQ 115000000 DLA0_FALCON MAX_FREQ 294400000 DLA1_FALCON MAX_FREQ 115000000 PVA0_VPS MAX_FREQ 115000000 PVA0_AXI MAX_FREQ 115000000 ``` 4. Select the new mode: ```bash sudo nvpmodel -m ``` > **Warning** > > * Keep the total consumption within the limit of your [power supply](#power-supply-of-the-zed-box-orin). > * Capping the memory (EMC) frequency below the bandwidth required by your application can cause functional failures, for example dropped camera frames. ## Monitor power consumption and temperature Monitor the system while your application runs to validate your power mode choice. ### tegrastats `tegrastats` is installed with JetPack. It reports the CPU and GPU load and frequencies, the memory usage, the temperatures, and the power consumption of the module rails: ```bash sudo tegrastats --interval 1000 ``` ![tegrastats output](/_fern-files/stereolabs.docs.buildwithfern.com/e886e15d06c53ec04fa4027aabd9f50dea38943ae2cb81abf090d5b5a3349750/docs/products/embedded/zed-box-orin/images/power-tegrastats.webp) To log the statistics in the background, for example during a long test: ```bash sudo tegrastats --interval 1000 --logfile ~/tegrastats.log & ``` Stop the background logging with `sudo tegrastats --stop`. > **Tip** > > You can also start `tegrastats` from the Ubuntu desktop: click the NVIDIA icon in the top bar, then **Run tegrastats**. ### Jetson Power GUI The **Jetson Power GUI** is installed with JetPack. It displays the CPU, GPU, and memory frequencies and loads, the readings of the temperature sensors, and the instantaneous and average power of each monitored rail. To start it, click the NVIDIA icon in the top bar, then **Run Jetson Power GUI**. ![Jetson Power GUI main tab](/_fern-files/stereolabs.docs.buildwithfern.com/0e70ad8638239258a7cfdf5aaaa7a7c628fcc02151d25d7fa5298fd542849cda/docs/products/embedded/zed-box-orin/images/power-jetson-power-gui.webp) > **Note** > > The ZED Box Orin has no fan: ignore the fan values reported by the Jetson Power GUI and by `jtop`. The **Thermal / Power Monitor** tab shows the throttling and shutdown limits of each temperature sensor, and the voltage, current, and power of each monitored rail: ![Jetson Power GUI Thermal / Power Monitor tab](/_fern-files/stereolabs.docs.buildwithfern.com/33ab153dae7de6629d6d16e43aa859c9003c5061f79a67002457479ef785bc2d/docs/products/embedded/zed-box-orin/images/power-jetson-power-gui-thermal.webp) The **Record** section at the bottom of the **Main** tab captures a log over a given duration, and **plot graph...** plots the recorded or real-time data. This helps you compare the power consumption of your application in different power modes. ### jtop [jtop](https://github.com/rbonghi/jetson_stats), from the community `jetson-stats` package, is an interactive terminal monitor that also lets you change the power mode and toggle `jetson_clocks`: ```bash sudo apt update sudo apt install python3-pip sudo pip3 install -U jetson-stats sudo jtop --install-service ``` The last command installs and starts the `jtop` service, and adds your user to the `jtop` group. Log out and log in again, or reboot, then run: ```bash jtop ``` ![jtop main screen](/_fern-files/stereolabs.docs.buildwithfern.com/9f2937bcefb76db74271376849625637bd144760b610e880b83b5e82c33d9de6/docs/products/embedded/zed-box-orin/images/power-jtop.webp) ### Throttling The ZED Box Orin has no fan, so its temperature depends on the power mode, the workload, and the ambient temperature. Its operating temperature range is **0 °C to 50 °C** (32 °F to 122 °F). When a temperature sensor of the Jetson module reaches **99 °C**, the software starts throttling the clocks. At **103 °C**, hardware throttling is engaged, and the system shuts down at **104.5 °C** to protect itself. The clocks are also throttled when the input voltage drops or when the module power exceeds its electrical limits. On the Ubuntu desktop, the NVIDIA icon in the top bar displays a notification when the system is throttled because of an over-current event or a high temperature. If you observe throttling or unstable frame rates during long runs, select a lower power mode, improve the airflow around the ZED Box Orin, or reduce the workload of your application. With PoE+, also check that your setup stays within the 25.5W budget. ## Further reading * [NVIDIA Jetson Linux Developer Guide: Platform Power and Performance](https://docs.nvidia.com/jetson/archives/r39.2/DeveloperGuide/SD/PlatformPowerAndPerformance/JetsonOrinNanoSeriesJetsonOrinNxSeriesAndJetsonAgxOrinSeries.html) * [NVIDIA Technical Blog: Power Optimization with NVIDIA Jetson](https://developer.nvidia.com/blog/power-optimization-with-nvidia-jetson/) > Tune the power consumption and performance of your ZED Box Orin