> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Remote access via Serial Console

The ZED Box 2 Max provides a Serial Console interface for low-level access to the system, via its USB 2.0 Type-C debug port. This is useful when no display is connected to the HDMI ports.

> **Note**
>
> The Serial Console is available only when the device is:
>
> * Booting up
> * Booted into Normal Mode (not Recovery Mode)

## Connecting to the Serial Console

* Connect a USB Type-C cable from your host computer to the [USB 2.0 Type-C port](/docs/products/embedded/zed-box-series/zed-box-2-max/connectivity#usb-20-type-c---debug) labeled `Debug` on the rear panel of the ZED Box 2 Max.

* Power on the ZED Box 2 Max.

* On the host computer, open a terminal (`Ctrl+Alt+T`) and install `gtkterm` if not already installed:

  ```bash
  sudo apt-get install gtkterm
  ```

* Identify the serial device of the ZED Box 2 Max:

  ```bash
  ls /dev/ttyUSB*
  ```

  The debug port uses a USB-to-UART bridge, detected by the host as a `/dev/ttyUSB<n>` device.

* Launch `gtkterm` from the terminal with the appropriate device path (usually `/dev/ttyUSB0`) and a baud rate of 115200:

  ```bash
  sudo gtkterm -p /dev/ttyUSB0 -s 115200
  ```

  > **Info**
  >
  > You can use other terminal emulators such as `minicom` or `screen` if you prefer.

* If the cable is connected before the device is powered on, the terminal will display the boot messages as the device starts up. When the boot is complete, you will see a login prompt.

  > **Note**
  >
  > If the cable is connected after the boot procedure has completed, the terminal does not display any boot messages; you may need to press `Enter` a couple of times to see the login prompt.

  ![image](/_fern-files/_img/f9bb7b4d49f005a6ac57f697dec63ad1cc34e78110d75ba0e741e2bf0548d0fa.webp)

* Log in with your credentials (default credentials: `user`/`admin`)

  ![image](/_fern-files/_img/358f21e1b52b2ce6b0dfca7a6fe7779f3779350025e4daf3405d1786024c9e65.webp)

* You can now execute commands on the device via the Serial Console in the same way as you would via SSH.