> For clean Markdown of any page, append .md to the page URL. > For a complete documentation index, see https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/gmsl2/troubleshooting/llms.txt. > For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server. # GMSL2 Troubleshooting This is a comprehensive guide that addresses the **most common issues** you may face while setting up your **[GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2)** camera with the ZED Link capture cards on NVIDIA® Jetson devices. Follow the steps below to troubleshoot and resolve these issues effectively. ## The camera is not detected [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras have lower flexibility compared to USB cameras. Any modification in the **hardware configuration**, such as plugging or unplugging a camera, or changing the camera order, requires either **rebooting the Jetson**, or restarting the installed daemon with the following command: ```bash sudo systemctl restart zed_x_daemon ``` --- ## Upgrading a ZED Link driver If you want to upgrade the ZED Link driver, it is required to uninstall the previously installed version: ```bash sudo dpkg -r stereolabs- ``` To retrieve the correct name of the package to remove, you can use the command: ```bash sudo dpkg -l | grep stereolabs- ``` --- ## Troubleshooting commands The following commands will help troubleshoot your [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) connection: ```bash sudo dmesg | grep zedx ``` Use the ZED Diagnostic tool `dmesg` option for quick debugging: ```bash sudo /usr/local/zed/tools/ZED_Diagnostic --dmesg ``` --- ## Xavier NX / Orin NX MIPI Bandwidth The default configuration for the MIPI lanes may be too high depending on the quality and length of the flat cables used to connect the NX development kit carrier boards to the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card. In such cases, the `dmesg` diagnostic report does not indicate any problems, but the camera cannot be detected correctly by the ZED SDK. You can solve the problem by using shorter flat cables, or by changing the settings for the speed of the MIPI lanes. If you experience connection issues the recommended maximum length is 12 cm. ### Set the speed of the MIPI lanes Try first with 2 Gbps per lane: ```bash sudo i2cset -y -f 30 0x29 0x04 0x15 0x34 i sudo i2cset -y -f 30 0x29 0x04 0x18 0x34 i sudo i2cset -y -f 30 0x29 0x04 0x1B 0x34 i sudo i2cset -y -f 30 0x29 0x04 0x1E 0x34 i ``` then with 1.6 Gbps per lane if 2 Gbps is still too high: ```bash sudo i2cset -y -f 30 0x29 0x04 0x15 0x30 i sudo i2cset -y -f 30 0x29 0x04 0x18 0x30 i sudo i2cset -y -f 30 0x29 0x04 0x1B 0x30 i sudo i2cset -y -f 30 0x29 0x04 0x1E 0x30 i ``` > **Note** > > This set of commands must be entered after each reboot, and after calling the reset command `sudo systemctl restart zed_x_daemon`. --- ## Blurry images after system update After a system update, if you experience blurry images from the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) camera, it may be caused by the overwriting of a patched library used by the ZED Link driver. To fix this issue, please follow this procedure to manually restore the patched library: 1. Download the latest ZED Link driver package for your device from the [ZED X Drivers download page](https://www.stereolabs.com/developers/drivers). 2. Extract the downloaded `.deb` package and copy the patched library to the correct location: ```bash mkdir temp_zedx cd temp_zedx ar x ../stereolabs-zed_--_arm64.deb tar xvf data.tar.xz sudo cp ./tmp/R/libnvisppg.so /usr/lib/aarch64-linux-gnu/tegra/libnvisppg.so ``` Replace `stereolabs-zed_--_arm64.deb` with the actual filename of the downloaded package. Replace `` in the `cp` command with your current L4T version (for example, `36.4.3`). 3. Reboot the Jetson device: ```bash sudo reboot ``` After following these steps, the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) camera should function correctly with clear images. --- ## Contact Support If you are unable to resolve your issue, please visit our [community forum](https://community.stereolabs.com/) or contact [support@stereolabs.com](mailto:support@stereolabs.com) for further assistance.