> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Link Duo on Orin Nano

This tutorial will help you set up the **[ZED Link Duo](https://www.stereolabs.com/store/products/zed-link-capture-card)** [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card, and use the StereoLabs [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras with the NVIDIA® Jetson™ **Orin Nano** Developer Kit.

> **Note**
>
> NVIDIA® does not manufacture a development kit specifically for the Jetson™ **Orin NX** module. However, the carrier board of the Jetson™ **Orin Nano** Developer Kit is fully compatible with the **Orin NX** module. Therefore, you can use this setup to test the **Orin NX** module. Read more [here](https://docs.nvidia.com/jetson/archives/r35.3.1/DeveloperGuide/text/HR/JetsonModuleAdaptationAndBringUp/JetsonOrinNxNanoSeries.html).

## Prerequisites

Make sure that you have the following items before starting this guide:

* 1x NVIDIA® Jetson™ Orin Nano Developer Kit or NVIDIA® Jetson™ Orin Nano Developer Kit mounting an Orin NX module.
* 1x [ZED Link Duo](https://www.stereolabs.com/store/products/zed-link-capture-card) [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card
* 1x 1-to-4 [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Fakra Male to Female cable (included in the box)
* 1x NVIDIA® power supply to power the Development Kit (included with the devkit)
* 2x FPC Camera Cable 22-pin 0.5mm Pitch to 15-pin 1.0mm Pitch (not included)
* 9V-19V (min 2W) power input (Barrel Jack 5.5 mm outer diameter, 2.5 mm inner diameter) to power the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card (not included)

> **Note**
>
> FPC Camera Cables transmit video signals. If the cable length exceeds 12 cm, the video signal may become noisy or corrupted. We recommend keeping the cable length within this limit.

![Orin Devkit Material](/_fern-files/stereolabs.docs.buildwithfern.com/f4ea377da0479c0bcc739ad6e2a4f264bc3246057a97b0e2ecc601260442e4e1/docs/products/cameras/zedx/images/orin-devkit-material.webp)

If you encounter any issues during the installation process, please refer to the [troubleshooting page](/docs/products/embedded/zed-link-capture-card/gmsl2/troubleshooting) or contact [support@stereolabs.com](mailto:support@stereolabs.com).

## Install the GMSL2 Capture Card

Please make sure the DevKit and the capture card are not connected to a power source before beginning the installation process.

### Cabling the GMSL2 Capture Card

Connect both CSI cables to the MIPI 15-pin ports of the capture card. Make sure the correct side is plugged in for each port.

![Orin Devkit Capture Card Cabling](/_fern-files/stereolabs.docs.buildwithfern.com/63e7bf599d98c76235387473c2be47e852ce0dcaaa3b4665d0655838d8d4363d/docs/products/cameras/zedx/images/orin-devkit-capture-card-cabling.webp)

> **Warning**
>
> Inverting the side might damage the carrier board or the capture card.

Both MIPI cables must be connected to have access to 2x ZED X on the capture card.

### Cabling the Carrier Board

Connect the CSI cable to the carrier board 22-pin connector.

Make sure that `CAM1` is connected to the centered MIPI port of the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card.

`CAM0` must be connected to the MIPI port close to the edge.

Make sure to respect the side of the MIPI pins, according to the following picture:

![Orin Devkit Carrier Board Cabling](/_fern-files/stereolabs.docs.buildwithfern.com/194206b7cfae04495fe48927785cdf4d79e244bd03a48605d5a0be1091ae738d/docs/products/cameras/zedx/images/orin-devkit-carrier-board-cabling.webp)

Once connected, the setup should look like the following picture:

![Orin Devkit Cabled](/_fern-files/stereolabs.docs.buildwithfern.com/6ef02ee1aeee2132366b100c7e3048407f9543e9edbc5020ddb57d4d19e72062/docs/products/cameras/zedx/images/orin-devkit-cabled.webp)

### Connect the camera

Connect the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Fakra cable **female** end to your ZED X. When you hear a *click*, the cable is securely connected to the camera.

![ZED X with Fakra Cable](/_fern-files/stereolabs.docs.buildwithfern.com/95694c2856777b637c70f659e0d336d588116951a7df4c1afb0648869ef4bcb6/docs/products/embedded/zed-link-capture-card/images/zed-x-with-fakra-cable.webp)

With the capture card still **powered off**, connect the **male** end of the cable to the capture card's [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) input. Again, a *click* informs you that the cable is **secured**.

> **Note**
>
> Ideally, [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras should be plugged in before booting up. If this is not the case, you can restart the `zed_x_daemon` that will be installed by the driver in the next section.

![Orin Devkit Plug Camera](/_fern-files/stereolabs.docs.buildwithfern.com/337454958a7874044b78bf1e25c8b2c3a58fb1dc0cf50b11dc232994cff21726/docs/products/cameras/zedx/images/orin-devkit-plug-camera.webp)

Once the cables are connected, plug the power for the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card (9V-19V) so that cameras will be powered through the FAKRA cable (PoC).

Then connect optional HDMI/Keyboard/Mouse to USB and the power. Wait for boot up.

Now that the Developer Kit has been correctly set up, we can install the **associated software** and **drivers** for the ZED [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras.

## Setting up the software

### Install the ZED Link Driver

After setting up your ZED Link [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card, please follow this guide to [Install the ZED Link Driver](/docs/products/embedded/zed-link-capture-card/gmsl2/install-and-upgrade-the-drivers/).

### Install the ZED SDK

After installing the ZED Link driver, please follow this guide to [Install the ZED SDK on NVIDIA® Jetson](/docs/development/zed-sdk/linux/work-with-nvidia-jetson/).

## Multi-camera configurations

The ZED Link Duo provides 4 [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) ports organized in 2 Groups (**A**, **B**):

* Group **A**: port **#0** and port **#1**
* Group **B**: port **#2** and port **#3**

![ZED Link Duo Connections](/_fern-img/96d8c17b874582c443fc6d2099234b4a57fec3ef621b283765c739c467aec72b.webp)

Please refer to the table below to understand how different camera configurations provide different image capture behaviors, according to the number of cameras, their type, and the Group they are connected to:

| Camera Type | Camera Model                                           | Max number of cameras **per Group**  | Max Resolution/FPS **per Group**                     |
| ----------- | ------------------------------------------------------ | ------------------------------------ | ---------------------------------------------------- |
| Monocular   | ZED X One GS ZED X One S                               | Up to 2 cameras                      | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Monocular   | ZED X One 4K                                           | 1 camera *only to port #0, #2*       | 4K\@15fps QHDPLUS\@15fps HD1200\@60fps HD1080\@60fps |
| Stereo      | ZED X ZED X Mini ZED X Nano                            | 1 Camera                             | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Stereo      | ZED X ZED X Mini ZED X Nano                            | Up to 2 Cameras                      | HD1200\@30fps HD1080\@30fps SVGA\@60fps              |
| Mixed       | ZED X One GS/ZED X One S + ZED X/ZED X Mini/ZED X Nano | 1 ZED X One GS/S + 1 ZED X/Mini/Nano | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |

> **Note**
>
> Maximum resolution and framerate require no more than 2 cameras per 4-wire [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Fakra connector.

---

🎉 **Congratulations!** You have successfully set up your StereoLabs **[GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Capture Card** and started exploring its features. Now that you have the camera up and running, it is time to start experimenting and building your projects.

Whether you are using the camera for robotics, computer vision, or something else entirely, the ZED [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras are a powerful tool that can help you achieve your goals. **Happy coding!**