> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Link Mono on Orin Nano

This tutorial will help you set up the **[ZED Link Mono](https://www.stereolabs.com/store/products/zed-link-capture-card-mono)** [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card, and use the StereoLabs [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras with the NVIDIA® Jetson™ **Orin Nano** Developer Kit.

> **Note**
>
> NVIDIA® does not manufacture a development kit specifically for the Jetson™ **Orin NX** module. However, the carrier board of the Jetson™ **Orin Nano** Developer Kit is fully compatible with the **Orin NX** module. Therefore, you can use this setup to test the **Orin NX** module. Read more [about Jetson Orin NX/Nano series adaptation](https://docs.nvidia.com/jetson/archives/r35.3.1/DeveloperGuide/text/HR/JetsonModuleAdaptationAndBringUp/JetsonOrinNxNanoSeries.html).

## Prerequisites

Make sure that you have the following items before starting this guide:

* 1x NVIDIA® Jetson™ Orin Nano Developer Kit or NVIDIA® Jetson™ Orin Nano Developer Kit mounting an Orin NX module.
* 1x **[ZED Link Mono](https://www.stereolabs.com/store/products/zed-link-capture-card-mono)** [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card
* 1x NVIDIA® power supply to power the Development Kit (included with the devkit)
* 1x FPC Camera Cable 22-pin 0.5mm Pitch (included in the box)
* 9V-14V (min 2W) power input (Barrel Jack 5.5 mm outer diameter, 2.5 mm inner diameter) to power the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card (not included)

> **Note**
>
> MIPI cables transmit video signals. As the cable length increases, the video signal becomes noisier. The maximum recommended length is 12 cm.

![ZED Link Mono Orin Nano material](/_fern-img/fe7692d013974ff78a232eba372cb2b2ef0acac8dd95d9c759905e3913b35263.webp)

If you encounter any issues during the installation process, please refer to the [troubleshooting page](/docs/products/embedded/zed-link-capture-card/gmsl2/troubleshooting) or contact [support@stereolabs.com](mailto:support@stereolabs.com).

## Install the GMSL2 Capture Card

Please make sure the DevKit and the capture card are not connected to a power source before beginning the installation process.

### Cabling the GMSL2 Capture Card

Connect the power adapter cable to the white **PWR J3** connector.

![ZED Link Mono Orin Nano power](/_fern-img/7a598927c14274be13b99f8ffe025c15b573c58a456e0b21e7aaac151889ddc0.webp)

Connect the CSI cable to the MIPI 22-pin port of the capture card. Make sure the correct side is plugged in.

![ZED Link Mono Orin Nano MIPI](/_fern-img/188ef843bb95e365e40951cd8485951353724cb7fd86b0c868d2294e4a6518d5.webp)

> **Warning**
>
> Inverting the side might damage the carrier board or the capture card.

### Cabling the Carrier Board

Connect the CSI cable to the carrier board 22-pin connector.

Make sure to respect the side of the MIPI pins, according to the following picture:

![ZED Link Mono Orin Nano MIPI carrier board connection](/_fern-img/179dbac4572bf9a5ddc874f54bc6937e97752d123561c9841f89021017df72c5.webp)

### Connect the camera

Connect the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Fakra cable **female** end to your [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) camera. When you hear a *click*, the cable is securely connected to the camera.

![ZED X camera with Fakra cable connected](/_fern-files/stereolabs.docs.buildwithfern.com/95694c2856777b637c70f659e0d336d588116951a7df4c1afb0648869ef4bcb6/docs/products/embedded/zed-link-capture-card/images/zed-x-with-fakra-cable.webp)

With the capture card still **powered off**, connect the **male** end of the cable to the capture card's [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) input. Again, a *click* informs you that the cable is **secured**.

![ZED Link Mono Fakra cable connection](/_fern-img/cbb0303d4779571affebc506c3287bbb65c0a05c479be0ce3979f0e66e258911.webp)

> **Note**
>
> Ideally, [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras should be plugged in before booting up. If this is not the case, you can restart the `zed_x_daemon` that will be installed by the driver in the next section.

Once the cables are connected, plug the power for the [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card (9V-14V) so that cameras will be powered through the FAKRA cable (PoC).

![Power adapter connection to ZED Link Mono](/_fern-img/d4a08d04f4ec846445b73534a2924442fa109e158e4b084fefc3d8bcc9413b39.webp)

Then connect optional HDMI/Keyboard/Mouse to USB and the power. Wait for boot up.

Now that the Developer Kit has been correctly set up, we can install the **associated software** and **drivers** for the ZED [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras.

## Setting up the software

### Install the ZED Link Driver

After setting up your ZED Link [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) capture card, please follow this guide to [Install the ZED Link Driver](/docs/products/embedded/zed-link-capture-card/gmsl2/install-and-upgrade-the-drivers/).

### Install the ZED SDK

After installing the ZED Link driver, please follow this guide to [Install the ZED SDK on NVIDIA® Jetson](/docs/development/zed-sdk/linux/work-with-nvidia-jetson/).

## Camera configurations

The ZED Link Mono provides a single [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) port, so only one camera can be connected to the capture card.

The table below illustrates the different behaviors that can be expected according to the camera type:

| Camera Type | Camera Model | Max Resolution/FPS                                   |
| ----------- | ------------ | ---------------------------------------------------- |
| Monocular   | ZED X One GS | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Monocular   | ZED X One S  | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Monocular   | ZED X One 4K | 4K\@15fps QHDPLUS\@15fps HD1200\@60fps HD1080\@60fps |
| Stereo      | ZED X        | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Stereo      | ZED X Mini   | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |
| Stereo      | ZED X Nano   | HD1200\@60fps HD1080\@60fps SVGA\@120fps             |

---

🎉 **Congratulations!** You have successfully set up your StereoLabs **[GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) Capture Card** and started exploring its features. Now that you have the camera up and running, it is time to start experimenting and building your projects.

Whether you are using the camera for robotics, computer vision, or something else entirely, the ZED [GMSL2](/docs/products/embedded/zed-link-capture-card/gmsl2#what-is-gmsl2) cameras are a powerful tool that can help you achieve your goals. **Happy coding!**