> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# ZED Link MIPI Quad

The [ZED Link MIPI Quad](https://www.stereolabs.com/store/products/zed-link-mipi-quad) is a [MIPI CSI-2](/docs/products/embedded/zed-link-capture-card/mipi#what-is-mipi-csi-2) capture card that connects up to four [ZED X One Core](/docs/products/cameras/zedxone-core/) cameras to an NVIDIA® Jetson™ device. Each of the four channels supports a camera at up to 1920x1200 @60 fps, and an onboard FPGA hardware-synchronizes the four channels.

![ZED Link MIPI Quad](/_fern-files/_img/fceeea297b8607167048e5442561a0b4390c48c343b2fdc112610bcb73fb2dfd.webp)

## Supported devices

| Host platform                                            | MIPI Support | Max cameras | Guide                                                                                                             |
| -------------------------------------------------------- | ------------ | ----------- | ----------------------------------------------------------------------------------------------------------------- |
| NVIDIA® Jetson AGX Orin™ DevKit                          | ✔️           | 4           | [Setup Guide](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-orin-agx-devkit-setup) |
| NVIDIA® Jetson AGX Thor™ DevKit + Holoscan Sensor Bridge | ✔️ *beta*    | 2           | [Setup Guide](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-agx-thor-devkit-setup) |
| Other Jetson™ carrier boards                             | -            | -           | Please contact [support@stereolabs.com](mailto:support@stereolabs.com)                                            |

## ZED Link MIPI Quad guides

#### [ZED Link MIPI Quad on AGX Orin](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-orin-agx-devkit-setup)

Install the ZED Link MIPI Quad on an NVIDIA® Jetson AGX Orin™ developer kit and connect up to four ZED X One Core cameras.

#### [ZED Link MIPI Quad on AGX Thor with Holoscan Sensor Bridge](/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-agx-thor-devkit-setup)

Connect up to two ZED X One Core cameras to an NVIDIA® Jetson AGX Thor™ developer kit through the NVIDIA® Holoscan Sensor Bridge.

## Common MIPI guides

* [What is MIPI CSI-2?](/docs/products/embedded/zed-link-capture-card/mipi#what-is-mipi-csi-2)
* [Troubleshooting](/docs/products/embedded/zed-link-capture-card/mipi/troubleshooting)