> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Tutorial - Image Capture

This tutorial shows how to grab frames from the ZED camera and retrieve the left image, printing its timestamp and resolution in the terminal. The program loops until it has successfully captured 50 images. We assume that you have read the [Hello ZED](/docs/tutorials/hello-zed/) tutorial before.

## Getting Started

* First, download the latest version of the [ZED SDK](https://www.stereolabs.com/developers/).
* Download the [Image Capture](https://github.com/stereolabs/zed-sdk/tree/master/tutorials/tutorial%202%20-%20image%20capture) sample code in C, C++, Python or C#.

## Code Overview

### Open the camera

As in the previous tutorial, here we create, configure and open the ZED. We set the 3D camera to dual HD 1080 resolution at 30 fps.

**`C++`**

```cpp C++
// Create a ZED camera object
Camera zed;

// Set configuration parameters
InitParameters init_params;
init_params.camera_resolution = RESOLUTION::HD1080; // Use HD1080 video mode
init_params.camera_fps = 30; // Set fps at 30

// Open the camera
ERROR_CODE err = zed.open(init_params);
if (err != ERROR_CODE::SUCCESS)
    exit(-1);
```

**`Python`**

```python Python
# Create a ZED camera object
zed = sl.Camera()

# Set configuration parameters
init_params = sl.InitParameters()
init_params.camera_resolution = sl.RESOLUTION.HD1080  # Use HD1080 video mode
init_params.camera_fps = 30  # Set fps at 30

# Open the camera
err = zed.open(init_params)
if err != sl.ERROR_CODE.SUCCESS:
    exit(1)
```

**`C#`**

```csharp C#
// Create a ZED camera object
Camera zed = new Camera(0);

// Set configuration parameters
InitParameters init_params = new InitParameters();
init_params.resolution = RESOLUTION.HD1080; // Use HD1080 video mode
init_params.cameraFPS = 30; // Set fps at 30

// Open the camera
ERROR_CODE err = zed.Open(ref init_params);
if (err != ERROR_CODE.SUCCESS)
    Environment.Exit(-1);
```

### Capture Image Data

Now that the ZED is opened, we can capture the live stream coming from the camera. Let's create a loop that captures 50 images and exits.

To capture an image and process it, you need to call the `Camera::grab()` function. This function can take runtime parameters as well, but we leave them to default in this tutorial.

If `grab()` returns `SUCCESS`, a new image has been captured and is now available. You can also check the status of `grab()` which tells you if there is an issue during capture.

**`C++`**

```cpp C++
// Grab an image
if (zed.grab() == ERROR_CODE::SUCCESS) {
	// A new image is available if grab() returns ERROR_CODE::SUCCESS
}
```

**`Python`**

```python Python
# Grab an image
runtime_parameters = sl.RuntimeParameters()
if zed.grab(runtime_parameters) == sl.ERROR_CODE.SUCCESS:
    # A new image is available if grab() returns ERROR_CODE.SUCCESS
    pass
```

**`C#`**

```csharp C#
// Grab an image
RuntimeParameters runtimeParameters = new RuntimeParameters();
if (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
    // A new image is available if Grab() returns ERROR_CODE.SUCCESS
}
```

Once the `grab()` method has been executed, you can retrieve the new image and its metadata. In this tutorial, we will retrieve the left image and its timestamp using `retrieveImage()` and `getTimestamp()`.

`retrieveImage()` takes an `sl::Mat` as well as a `VIEW` mode as parameters. When creating the `Mat`, you don't need to allocate memory. The first time `retrieveImage()` is called, the Mat is filled with image data and memory is allocated automatically.

**`C++`**

```cpp C++
// Capture 50 frames and stop
int i = 0;
sl::Mat image;
while (i < 50) {
    // Grab an image
    if (zed.grab() == ERROR_CODE::SUCCESS) {
        // A new image is available if grab() returns ERROR_CODE::SUCCESS
        zed.retrieveImage(image, VIEW::LEFT); // Get the left image
        auto timestamp = zed.getTimestamp(sl::TIME_REFERENCE::IMAGE); // Get image timestamp
        printf("Image resolution: %d x %d  || Image timestamp: %llu\n", (int)image.getWidth(), (int)image.getHeight(), (unsigned long long)timestamp.getNanoseconds());
        i++;
    }
}
```

**`Python`**

```python Python
# Capture 50 frames and stop
i = 0
image = sl.Mat()
runtime_parameters = sl.RuntimeParameters()
while i < 50:
    # Grab an image, a RuntimeParameters object must be given to grab()
    if zed.grab(runtime_parameters) == sl.ERROR_CODE.SUCCESS:
        # A new image is available if grab() returns ERROR_CODE.SUCCESS
        zed.retrieve_image(image, sl.VIEW.LEFT) # Get the left image
        timestamp = zed.get_timestamp(sl.TIME_REFERENCE.IMAGE)  # Get the image timestamp
        print("Image resolution: {0} x {1} || Image timestamp: {2}\n".format(image.get_width(), image.get_height(), timestamp.get_nanoseconds()))
        i = i + 1
```

**`C#`**

```csharp C#
uint mWidth = (uint)zed.ImageWidth;
uint mHeight = (uint)zed.ImageHeight;
// Initialize the Mat that will contain the left image
Mat image = new Mat();
image.Create(mWidth, mHeight, MAT_TYPE.MAT_8U_C4, MEM.CPU); // Mat needs to be created before use.

// Capture 50 frames and stop
int i = 0;
RuntimeParameters runtimeParameters = new RuntimeParameters();
while (i < 50) {
    // Grab an image
    if (zed.Grab(ref runtimeParameters) == ERROR_CODE.SUCCESS) {
        // A new image is available if Grab() returns ERROR_CODE.SUCCESS
        zed.RetrieveImage(image, VIEW.LEFT); // Get the left image
        ulong timestamp = zed.GetCameraTimeStamp(); // Get image timestamp
        Console.WriteLine("Image resolution: " + image.GetWidth() + "x" + image.GetHeight() + " || Image timestamp: " + timestamp);
        i++;
    }
}
```

> **Note**
>
> Image timestamp is given in nanoseconds and Epoch format. You can compare the timestamps between two `grab()`: it should be close to the framerate time, if you don't have any dropped frames.

For more information on Camera and Video parameters, read [Using the Video API](/docs/development/zed-sdk/modules/camera/camera-controls/).

### Close the Camera

Now that we have captured 50 images, let's close the camera and exit the program.

**`C++`**

```cpp C++
// Close the camera
zed.close();
```

**`Python`**

```python Python
# Close the camera
zed.close()
```

**`C#`**

```csharp C#
// Close the camera
zed.Close();
```

#### Additional Example

To learn how to adjust camera settings like Exposure, Gain, Contrast, Sharpness, etc. and display the resulting image, check the [Camera Control](https://github.com/stereolabs/zed-sdk/tree/master/camera%20control) sample code.