Skip to navigation

Create Docker images for ZED and OpenCV

Open in ClaudeOpen in ChatGPT

We have already seen how to create a Docker image. In this section, we follow the same recommended workflow with a few changes, so we strongly recommend going through that tutorial first to refresh your memory before continuing here.

The Dockerfile and build script below come from a community example and were written for older ZED SDK, Ubuntu, and CUDA versions (the compatibility check only allows Ubuntu 18.04 / 20.04 and CUDA 10 / 11). Use them to understand the workflow, then adapt the versions to your needs. The latest ZED SDK is v5.5.0, with Docker images for CUDA 12.8, 13.0, and 13.3 on Ubuntu 22.04 to 26.04 (check the available tags for the exact combinations). At the time of writing, the gl-devel variant used below is published up to ZED SDK 5.4. For officially maintained Dockerfiles and ready-to-use images, see the zed-docker GitHub repository and the StereoLabs DockerHub repository.

A generic Dockerfile skeleton (saved as Dockerfile.opencv) is provided to assemble an image, along with a build script, build-opencv-desktop-image.sh, that specifies the build arguments. build-opencv-desktop-image.sh lets you configure the build arguments and then build the Docker image, allowing you to customize your container.

Dockerfile Overview

The full Dockerfile contains many instructions, explained in detail below. You can adapt this file to your requirements.

# Build arguments
ARG UBUNTU_RELEASE_YEAR
ARG ZED_SDK_MAJOR
ARG ZED_SDK_MINOR
ARG CUDA_MAJOR
ARG CUDA_MINOR
# Specify the parent image from which we build
FROM stereolabs/zed:${ZED_SDK_MAJOR}.${ZED_SDK_MINOR}-gl-devel-cuda${CUDA_MAJOR}.${CUDA_MINOR}-ubuntu${UBUNTU_RELEASE_YEAR}.04
# OpenCV version
ARG OPENCV_VERSION
# Install dependencies
RUN apt-get update || true && apt-get upgrade -y &&\
# Install build tools, build dependencies and python
apt-get install --no-install-recommends -y \
build-essential gcc g++ \
cmake git libgtk2.0-dev pkg-config libavcodec-dev libavformat-dev libswscale-dev \
libtbb2 libtbb-dev libjpeg-dev libpng-dev libtiff-dev \
yasm libatlas-base-dev gfortran libpq-dev \
libxine2-dev libglew-dev libtiff5-dev zlib1g-dev libavutil-dev libpostproc-dev \
libeigen3-dev python3-dev python3-pip python3-numpy libx11-dev tzdata \
&& rm -rf /var/lib/apt/lists/*
# Set the working directory
WORKDIR /opt
# Install OpenCV from source
RUN git clone --depth 1 --branch ${OPENCV_VERSION} https://github.com/opencv/opencv.git && \
git clone --depth 1 --branch ${OPENCV_VERSION} https://github.com/opencv/opencv_contrib.git && \
cd opencv && \
mkdir build && \
cd build && \
cmake \
-D CMAKE_BUILD_TYPE=RELEASE \
-D CMAKE_INSTALL_PREFIX=/usr/ \
-D PYTHON3_PACKAGES_PATH=/usr/lib/python3/dist-packages \
-D WITH_V4L=ON \
-D WITH_QT=OFF \
-D WITH_OPENGL=ON \
-D WITH_GSTREAMER=ON \
-D OPENCV_GENERATE_PKGCONFIG=ON \
-D OPENCV_ENABLE_NONFREE=ON \
-D OPENCV_EXTRA_MODULES_PATH=/opt/opencv_contrib/modules \
-D INSTALL_PYTHON_EXAMPLES=OFF \
-D INSTALL_C_EXAMPLES=OFF \
-D BUILD_EXAMPLES=OFF .. && \
make -j"$(nproc)" && \
make install
# Alternatively, install from the Ubuntu repository
###
#RUN apt-get update -y || true && \
# DEBIAN_FRONTEND=noninteractive apt-get install -y && \
# apt-get install -y --no-install-recommends libopencv-dev && \
# rm -rf /var/lib/apt/lists/* && apt autoremove && apt clean
###
WORKDIR /
CMD ["bash"]

Below is an analysis of the main parts that make up the Dockerfile.

Specify the parent image

First, specify the base ZED SDK Docker image you want to build from. These images come with the ZED SDK pre-installed and let you use the ZED camera with SDK applications.

There are many Docker images available with different Ubuntu release years and SDK and CUDA versions. We therefore choose a specific ZED SDK Docker image as the parent image by configuring the build arguments.

The Ubuntu release year and the SDK and CUDA versions are passed as arguments during the build stage, which keeps the Dockerfile modular. Setting these arguments to the version of your choice is covered in a later section.

# Build arguments
ARG UBUNTU_RELEASE_YEAR
ARG ZED_SDK_MAJOR
ARG ZED_SDK_MINOR
ARG CUDA_MAJOR
ARG CUDA_MINOR
# Specify the parent image from which we build
FROM stereolabs/zed:${ZED_SDK_MAJOR}.${ZED_SDK_MINOR}-gl-devel-cuda${CUDA_MAJOR}.${CUDA_MINOR}-ubuntu${UBUNTU_RELEASE_YEAR}.04

Based on the arguments set in the build script, a specific base image is imported. For example, if the build arguments in build-opencv-desktop-image.sh are set to the values below:

UBUNTU_RELEASE_YEAR=20
ZED_SDK_MAJOR=3
ZED_SDK_MINOR=7
CUDA_MAJOR=11
CUDA_MINOR=4

then the base image will be stereolabs/zed:3.7-gl-devel-cuda11.4-ubuntu20.04.

Note that this base image already includes OpenGL support for display. If you do not need it, follow the section below to build an image without display support.

You can also browse the StereoLabs DockerHub repository, which lists all the official ZED SDK Docker images.

Install dependencies

Once you have specified the parent image, you can choose which OpenCV version to install. Be sure to check version availability and compatibility.

This part of the Dockerfile installs all the OpenCV dependencies.

# OpenCV version
ARG OPENCV_VERSION
# Install dependencies
RUN apt-get update || true && apt-get upgrade -y &&\
# Install build tools, build dependencies and python
apt-get install --no-install-recommends -y \
build-essential gcc g++ \
cmake git libgtk2.0-dev pkg-config libavcodec-dev libavformat-dev libswscale-dev \
libtbb2 libtbb-dev libjpeg-dev libpng-dev libtiff-dev \
yasm libatlas-base-dev gfortran libpq-dev \
libxine2-dev libglew-dev libtiff5-dev zlib1g-dev libavutil-dev libpostproc-dev \
libeigen3-dev python3-dev python3-pip python3-numpy libx11-dev tzdata \
&& rm -rf /var/lib/apt/lists/*

In the next stage, you install OpenCV. This can be done in two ways, both explained below.

Method 1: Install OpenCV from source

This step downloads the OpenCV source files for the chosen version and builds them.

# Install OpenCV from source
RUN git clone --depth 1 --branch ${OPENCV_VERSION} https://github.com/opencv/opencv.git && \
git clone --depth 1 --branch ${OPENCV_VERSION} https://github.com/opencv/opencv_contrib.git && \
cd opencv && \
mkdir build && \
cd build && \
cmake \
-D CMAKE_BUILD_TYPE=RELEASE \
-D CMAKE_INSTALL_PREFIX=/usr/ \
-D PYTHON3_PACKAGES_PATH=/usr/lib/python3/dist-packages \
-D WITH_V4L=ON \
-D WITH_QT=OFF \
-D WITH_OPENGL=ON \
-D WITH_GSTREAMER=ON \
-D OPENCV_GENERATE_PKGCONFIG=ON \
-D OPENCV_ENABLE_NONFREE=ON \
-D OPENCV_EXTRA_MODULES_PATH=/opt/opencv_contrib/modules \
-D INSTALL_PYTHON_EXAMPLES=OFF \
-D INSTALL_C_EXAMPLES=OFF \
-D BUILD_EXAMPLES=OFF .. && \
make -j"$(nproc)" && \
make install

Make sure you remove this section if you choose the second method.

Method 2: Install OpenCV from the Ubuntu repository

Alternatively, you can simply install OpenCV from the Ubuntu repository.

RUN apt-get update -y || true && \
DEBIAN_FRONTEND=noninteractive apt-get install -y tzdata libx11-dev && \
apt-get install -y --no-install-recommends libopencv-dev && \
rm -rf /var/lib/apt/lists/* && apt autoremove && apt clean

This is a much simpler way to install OpenCV and produces a lighter image, but building OpenCV from source gives you the latest available version, more flexibility, and complete control over the build options.

Choose the method that best fits your needs.

Build Script Overview

As mentioned above, the Docker image can be built for various versions. The build-opencv-desktop-image.sh script lets you configure the versions passed during the build and then creates the image with the docker build command.

The script is detailed below.

Configure the arguments

Specify the Ubuntu release year and the ZED SDK, CUDA, and OpenCV versions. The default values set in the script are shown below; edit them to the versions you want. These arguments are later passed as --build-arg during the build.

UBUNTU_RELEASE_YEAR=20 # Ubuntu release year
ZED_SDK_MAJOR=3 # ZED SDK major version
ZED_SDK_MINOR=7 # ZED SDK minor version
CUDA_MAJOR=11 # CUDA major version
CUDA_MINOR=4 # CUDA minor version
OPENCV_VERSION=4.5.3 # OpenCV version

Check version compatibility

This part of the script validates the arguments you entered above and checks compatibility between the different versions. If an entry is invalid, the build is aborted.

# Check for version compatibility
if [ ${UBUNTU_RELEASE_YEAR} == "18" ] ; then
echo "Ubuntu 18.04"
# Not compatible with CUDA <= 9
if [ ${CUDA_MAJOR} -le "9" ] ; then
echo "Ubuntu 18.04 Not compatible with CUDA <= 9"
exit
fi
elif [ ${UBUNTU_RELEASE_YEAR} == "20" ] ; then
# Not compatible with CUDA <= 10
if [ ${CUDA_MAJOR} -le "10" ] ; then
echo "Ubuntu 20.04 is not compatible with CUDA <= 10 "
exit
fi
else
echo "UBUNTU_RELEASE_YEAR! Allowed values are 18 or 20 "
exit
fi
if [ ${CUDA_MAJOR} -ge "11" ] ; then
if [ ${ZED_SDK_MINOR} -lt "2" ] ; then # CUDA 11.0 was introduced with 3.2
echo "CUDA 11.0 was introduced with 3.2"
exit
fi
if [ ${CUDA_MINOR} -ge "1" ] ; then
if [ ${ZED_SDK_MINOR} -lt "3" ] ; then # CUDA 11.1 was introduced with 3.3
echo "CUDA 11.1 was introduced with 3.3"
exit
fi
fi
if [ ${CUDA_MINOR} == "2" ] || [ ${CUDA_MINOR} == "3" ] || [ ${CUDA_MINOR} -ge "6" ] ; then
#invalid CUDA versions
echo "Invalid CUDA_MINOR! Allowed values : 0,1,4,5"
exit
fi
elif [ ${CUDA_MAJOR} == "10" ] ; then
if [ ${CUDA_MINOR} != "0" ] && [ ${CUDA_MINOR} != "2" ] ; then
echo "Invalid CUDA_MINOR! Allowed values are 0 or 2"
exit
fi
else
echo "Invalid CUDA_MAJOR! Allowed values are 10 or 11"
exit
fi

Docker build

The part of the script below assigns a default tag to the image based on the chosen arguments and runs the build.

# Default tag based on the selected versions
TAG="${ZED_SDK_MAJOR}.${ZED_SDK_MINOR}-opencv-gl-devel-cuda${CUDA_MAJOR}.${CUDA_MINOR}-ubuntu${UBUNTU_RELEASE_YEAR}.04"
echo "Building '${TAG}'"
docker build --build-arg UBUNTU_RELEASE_YEAR=${UBUNTU_RELEASE_YEAR} \
--build-arg ZED_SDK_MAJOR=${ZED_SDK_MAJOR} \
--build-arg ZED_SDK_MINOR=${ZED_SDK_MINOR} \
--build-arg OPENCV_VERSION=${OPENCV_VERSION} \
--build-arg CUDA_MAJOR=${CUDA_MAJOR} \
--build-arg CUDA_MINOR=${CUDA_MINOR} \
-t "${TAG}" -f Dockerfile.opencv .

Create your Docker Image with OpenCV

Now that you are familiar with the Dockerfile and build-opencv-desktop-image.sh, it’s time to create your image. Download the files from this link, edit the arguments to your desired versions, and run the script to build the Docker image.

./build-opencv-desktop-image.sh

That’s it! You can now change versions and create your own Docker containers just by editing the arguments. Go ahead and test your images, then host them as described in this tutorial.

Docker Image without display support

A display window is an integral part of most OpenCV applications. However, Docker is mainly intended to run command-line applications, and a display window is only possible in containers with OpenGL support.

By leaving out OpenGL, you can make the Docker images much lighter and remove the need for all the dependencies required for display support. There are a few ways to achieve this.

Choose a parent Docker image without OpenGL support by changing the parent image tag (drop the gl- prefix), as follows:

FROM stereolabs/zed:${ZED_SDK_MAJOR}.${ZED_SDK_MINOR}-devel-cuda${CUDA_MAJOR}.${CUDA_MINOR}-ubuntu${UBUNTU_RELEASE_YEAR}.04

You can read more about the image-specific tags on the StereoLabs DockerHub page.

  • In your application, the output image window can be saved instead of displayed. Below is a snippet from the zed-opencv sample that uses the ENABLE_DISPLAY flag to either display the image or save it as a video.
C++
#define ENABLE_DISPLAY 1
#if ENABLE_DISPLAY
cv::imshow("Image", image_ocv);
#ifdef HAVE_CUDA
// download the OpenCV GPU data from device to host to be displayed
depth_image_ocv_gpu.download(depth_image_ocv);
#endif
cv::imshow("Depth", depth_image_ocv);
#else
// Save image and depth video if the display is disabled
cv::VideoWriter video_image("../Image.avi", cv::VideoWriter::fourcc('M','J','P','G'), 10, cv::Size(new_width,new_height));
video_image.write(image_ocv);
#ifdef HAVE_CUDA
// download the OpenCV GPU data from device to host to be displayed
depth_image_ocv_gpu.download(depth_image_ocv);
#endif
cv::VideoWriter video_depth("../Depth.avi", cv::VideoWriter::fourcc('M','J','P','G'), 10, cv::Size(new_width,new_height));
video_depth.write(depth_image_ocv); // Display image and depth using cv::Mat, which shares sl::Mat data
//std::cout<<"The key: "<<key<<std::endl;
#endif

Refer to the zed-opencv GitHub repository for the complete code.