Skip to navigation

ROS 2 Composition and ZED ROS 2 Wrapper

Open in ClaudeOpen in ChatGPT

ROS 2 expanded the concept of nodelet from ROS 1 replacing nodelets with components and introducing the new concept of “Composition”.

Each node can be written as a “Component” which is a shared library loaded at runtime.

This tutorial explains how to:

  • run multiple nodes in separate processes with the benefits of process/fault isolation as well as easier debugging of individual nodes
  • run multiple nodes in a single process with lower overhead and optionally more efficient communication (see Intra Process Communication).

The launch file of the zed_wrapper package is designed to take advantage of both.

Run one ZED camera component in a single process

You can run a ZED Node in a single process by using the default launch command zed_camera.launch.py as it is:

ros2 launch zed_wrapper zed_camera.launch.py camera_model:=<camera_model>

the launch file creates a ROS 2 Container process called zed_container (unless an existing container is passed with the container_name launch argument):

Python
# ROS 2 Component Container
if (container_name_val == ''):
container_name_val = 'zed_container'
distro = os.environ['ROS_DISTRO']
if distro == 'foxy':
# Foxy does not support the isolated mode
container_exec = 'component_container'
arguments_val = ['--ros-args', '--log-level', 'info']
elif distro >= 'lyrical':
# `component_container_isolated` is deprecated since Lyrical: the
# distributions are in alphabetical order
container_exec = 'component_container'
arguments_val = ['--executor-type', 'multi-threaded', '--isolated',
'--ros-args', '--log-level', 'info']
else:
container_exec = 'component_container_isolated'
arguments_val = ['--use_multi_threaded_executor',
'--ros-args', '--log-level', 'info']
zed_container = ComposableNodeContainer(
name=container_name_val,
namespace=namespace_val,
package='rclcpp_components',
executable=container_exec,
arguments=arguments_val,
output=node_log_effective,
composable_node_descriptions=[]
)
return_array.append(zed_container)

then it loads a stereolabs::ZedCamera (stereo models) or a stereolabs::ZedCameraOne (monocular models) component into it. Intra-process communication is enabled according to the enable_ipc launch argument (default true):

Python
# ZED Wrapper component
if is_stereo_model:
zed_wrapper_component = ComposableNode(
package='zed_components',
namespace=namespace_val,
plugin='stereolabs::ZedCamera',
name=node_name_val,
parameters=node_parameters,
extra_arguments=[{'use_intra_process_comms': enable_ipc_effective}]
)
else: # monocular models
zed_wrapper_component = ComposableNode(
package='zed_components',
namespace=namespace_val,
plugin='stereolabs::ZedCameraOne',
name=node_name_val,
parameters=node_parameters,
extra_arguments=[{'use_intra_process_comms': enable_ipc_effective}]
)
full_container_name = '/' + namespace_val + '/' + container_name_val
info = 'Loading ZED node `' + node_name_val +\
'` in container `' + full_container_name + '`'
return_array.append(LogInfo(msg=TextSubstitution(text=info)))
load_composable_node = LoadComposableNodes(
target_container=full_container_name,
composable_node_descriptions=[zed_wrapper_component]
)

When the NVIDIA® Isaac™ ROS NITROS package is installed and debug.disable_nitros is false, the launch file forces enable_ipc:=false to avoid a conflict with NITROS. See NVIDIA® Isaac ROS Nitros.

Compose multiple node components in a single process to leverage IPC

Intra Process Communication (IPC) is an advanced concept of ROS 2 that allows you to optimize the performance of nodes running on the same machine.

The ZED IPC tutorial

The ZED IPC tutorial demonstrates how to leverage ROS 2 Composition and Intra-Process Communication to create a new node component that subscribes to point cloud topics published by all ZED Camera node components running within the same process.

The tutorial guides you through the creation of a new launch file. This launch file utilizes the launch file of the ZED Multi-Camera tutorial to:

  1. Start multiple ZED nodes within a single process.
  2. Load a new node component that subscribes to the point cloud topics.
  3. Achieve zero-copy data transfer for efficient data exchange.

This approach enhances performance and reduces resource consumption by minimizing data copying between nodes within the same process.

The zed_ipc.launch.py launch File

The zed_ipc.launch.py launch file is designed to facilitate the setup of multiple ZED Camera nodes within a single process, along with a custom node component that subscribes to their point cloud topics. This launch file ensures efficient intra-process communication by leveraging zero-copy data transfer.

Key Features
  • Multiple ZED Nodes: Initializes and manages multiple ZED Camera nodes within the same process to capture point cloud data.
  • Custom Subscriber Node: Loads a custom node component that subscribes to the point cloud topics published by the ZED Camera nodes.
  • Zero-Copy Data Transfer: Utilizes ROS 2’s intra-process communication capabilities to achieve zero-copy data transfer, enhancing performance and reducing resource usage.
Usage

To use the zed_ipc.launch.py launch file, execute the following command:

ros2 launch zed_ipc zed_ipc.launch.py cam_names:=[<camera_name_array>] cam_models:=[<camera_model_array>] cam_serials:=[<camera_serial_array>]

This command will start the launch file, initializing the ZED Camera nodes and the custom subscriber node within the same process.

The code explained

First step: create a ROS 2 Container and load the two ZED camera components nodes inside it. Here we use the multi-camera launch file described in the multi-camera tutorial.

Python
# Call the multi-camera launch file
multi_camera_launch_file = os.path.join(
get_package_share_directory('zed_multi_camera'),
'launch',
'zed_multi_camera.launch.py'
)
zed_multi_camera = IncludeLaunchDescription(
launch_description_source=PythonLaunchDescriptionSource(multi_camera_launch_file),
launch_arguments={
'cam_names': names,
'cam_models': models,
'cam_serials': serials,
'disable_tf': disable_tf
}.items()
)
actions.append(zed_multi_camera)

Second step: remap the topic names. The demo node that receives the Point Cloud messages subscribes to generic pointcloud_X topic names. The launch file must create a correct remapping between pointcloud_X and each ZED node Point Cloud topic name /zed_multi/<camera_name>/point_cloud/cloud_registered.

Python
# Create topic remappings for the point cloud node
remappings = []
name_array = parse_array_param(names.perform(context))
for i in range(cam_count):
base_topic = 'pointcloud_' + str(i)
remap = '/zed_multi/' + name_array[i] + '/point_cloud/cloud_registered'
remapping = (base_topic, remap)
remappings.append(remapping)

Third step: create the demo component node that subscribes to the Point Cloud topics and processes the relative messages.

Python
pc_node = ComposableNode(
package='zed_ipc',
plugin='stereolabs::PointCloudComponent',
name='ipc_point_cloud',
namespace='zed_multi',
parameters=[{
'cam_count': cam_count
}],
remappings=remappings,
extra_arguments=[{'use_intra_process_comms': True}]
)

Final step: load the Point Cloud component node in the existing ZED Container process to leverage Intra Process Communication.

Python
load_pc_node = LoadComposableNodes(
composable_node_descriptions=[pc_node],
target_container='/zed_multi/zed_multi_container'
)
actions.append(load_pc_node)

You can verify that all the nodes are now running into the same container process by using the command ros2 component list.

Example

Here’s an example for two ZED X cameras named zedx_front and zedx_rear:

  • Launch command:
ros2 launch zed_ipc zed_ipc.launch.py cam_names:=[zedx_front,zedx_rear] cam_models:=[zedx,zedx] cam_serials:=[xxxxxxxxx,yyyyyyyy]
  • Running check:
ros2 component list
/zed_multi/zed_multi_container
1 /zed_multi/zedx_front
2 /zed_multi/zedx_rear
3 /zed_multi/ipc_point_cloud