Skip to navigation

ROS - ZED Node

Open in ClaudeOpen in ChatGPT

The ZED ROS Wrapper packages are no longer maintained because ROS 1 reached end-of-life (EOL) on 2025-05-31 with the final Noetic release.

We recommend upgrading to ROS 2 to take advantage of the latest ZED SDK features for robotics applications.

To start a ZED ROS node you can use the following commands in a shell console:

  • ZED:
roslaunch zed_wrapper zed.launch
  • ZED Mini:
roslaunch zed_wrapper zedm.launch
  • ZED 2:
roslaunch zed_wrapper zed2.launch
  • ZED 2i:
roslaunch zed_wrapper zed2i.launch
  • ZED X:
roslaunch zed_wrapper zedx.launch
  • ZED X Mini:
roslaunch zed_wrapper zedxm.launch

Each launch file starts the node zed_node in a namespace named after the camera model, so the topics are published as /<camera_name>/zed_node/<topic>, for example /zed/zed_node/odom with zed.launch or /zed2i/zed_node/odom with zed2i.launch.

Published Topics

The ZED node publishes data on the following topics:

  • Left camera

    • rgb/image_rect_color: Color rectified image (left RGB image by default)
    • rgb/image_rect_gray: Grayscale rectified image (left RGB image by default)
    • rgb_raw/image_raw_color: Color unrectified image (left RGB image by default)
    • rgb_raw/image_raw_gray: Grayscale unrectified image (left RGB image by default)
    • rgb/camera_info: Color camera calibration data
    • rgb_raw/camera_info: Color unrectified camera calibration data
    • left/image_rect_color: Left camera color rectified image
    • left/image_rect_gray: Left camera grayscale rectified image
    • left_raw/image_raw_color: Left camera color unrectified image
    • left_raw/image_raw_gray: Left camera grayscale unrectified image
    • left/camera_info: Left camera calibration data
    • left_raw/camera_info: Left unrectified camera calibration data
  • Right camera

    • right/image_rect_color: Color rectified right image
    • right_raw/image_raw_color: Color unrectified right image
    • right/image_rect_gray: Grayscale rectified right image
    • right_raw/image_raw_gray: Grayscale unrectified right image
    • right/camera_info: Right camera calibration data
    • right_raw/camera_info: Right unrectified camera calibration data
  • Stereo pair

    • stereo/image_rect_color: Stereo rectified pair images side-by-side
    • stereo_raw/image_raw_color: Stereo unrectified pair images side-by-side

    To retrieve the camera parameters, you can subscribe to the topics left/camera_info, right/camera_info, left_raw/camera_info and right_raw/camera_info.

  • Depth and point cloud

    • depth/depth_registered: Depth map image registered on the left image (32-bit float in meters by default)
    • depth/camera_info: Depth camera calibration data
    • point_cloud/cloud_registered: Registered color point cloud
    • confidence/confidence_map: Confidence image (floating point values to be used in your own algorithms)
    • disparity/disparity_image: Disparity image
  • Tracking

    • odom: Absolute 3D position and orientation relative to the Odometry frame (visual odometry for the ZED, visual-inertial odometry for the other camera models when pos_tracking/imu_fusion is true)
    • pose: Absolute 3D position and orientation relative to the Map frame (Sensor Fusion algorithm + SLAM + Loop closure)
    • pose_with_covariance: Camera pose referred to Map frame with covariance
    • odom/status: Status of the odometry tracking
    • pose/status: Status of the pose tracking
    • path_odom: Sequence of camera odometry poses in Map frame
    • path_map: Sequence of camera poses in Map frame
  • Mapping

    • mapping/fused_cloud: Fused color point cloud

    Published only if mapping is enabled, see the mapping/mapping_enabled parameter.

  • Plane detection

    • plane: Detected plane (see Plane Detection)
    • plane_marker: Markers of the detected plane to be rendered in RViz
  • Sensor Data (not available for the ZED)

    • imu/data: Accelerometer, gyroscope, and orientation data in Earth frame
    • imu/data_raw: Accelerometer and gyroscope data in IMU frame
    • temperature/imu: Temperature of the IMU sensor [not available for the ZED Mini]
    • imu/mag: Calibrated magnetometer data [only ZED 2 and ZED 2i]
    • atm_press: Atmospheric pressure data [only ZED 2 and ZED 2i]
    • temperature/left: Temperature of the left camera sensor [only ZED 2 and ZED 2i]
    • temperature/right: Temperature of the right camera sensor [only ZED 2 and ZED 2i]
    • left_cam_imu_transform: Transform from the left camera sensor to IMU sensor position
  • Object Detection (not available for the ZED)

    • obj_det/objects: Array of the detected/tracked objects for each camera frame
  • Diagnostic

    • /diagnostics: ROS diagnostic message for ZED cameras

ZED parameters

You can specify the parameters to be used by the ZED node by modifying the values in the files:

  • params/common.yaml: common parameters to all camera models
  • params/zed.yaml: parameters for the ZED camera
  • params/zedm.yaml: parameters for the ZED Mini camera
  • params/zed2.yaml: parameters for the ZED 2 camera
  • params/zed2i.yaml: parameters for the ZED 2i camera
  • params/zedx.yaml: parameters for the ZED X camera
  • params/zedxm.yaml: parameters for the ZED X Mini camera

General parameters

Parameters with prefix general

ParameterDescriptionValue
camera_nameA custom name for the ZED camera. Used as namespace and prefix for camera TF framesstring, default=zed
camera_modelType of StereoLabs camera (set in the camera model file)zed: ZED, zedm: ZED Mini, zed2: ZED 2, zed2i: ZED 2i, zedx: ZED X, zedxm: ZED X Mini
grab_resolutionCamera resolution (set in the camera model file)HD2K, HD1080, HD720, VGA, AUTO (USB cameras); HD1080, HD1200, SVGA, AUTO (ZED X, ZED X Mini)
grab_frame_rateCamera grabbing framerate (set in the camera model file)int
camera_flipFlip the camera data if it is mounted upside downOFF, ON, AUTO
zed_idSelect a ZED camera by its ID. Useful when multiple cameras are connected. ID is ignored if an SVO path is specifiedint, default=0
serial_numberSelect a ZED camera by its serial numberint, default=0
pub_resolutionResolution of the published images. NATIVE uses the grab resolution, CUSTOM applies pub_downscale_factorNATIVE, CUSTOM
pub_downscale_factorDownscale factor applied to the published images when pub_resolution is CUSTOMdouble, default=2.0
pub_frame_ratePublishing frequency of video and depth datadouble, default=15.0
gpu_idSelect a GPU device for depth computationint, default=-1 (best device found)
base_frameFrame_id of the frame that indicates the reference base of the robotstring, default=base_link
sdk_verboseVerbosity level of the SDKint, default=1
svo_compressionSet SVO compression mode0: LOSSLESS, 1: H264 (AVCHD), 2: H265 (HEVC)
svo_realtimeIf true, an input SVO is played respecting its original framerate, eventually skipping framestrue, false
self_calibEnable/disable self calibration at startingtrue, false
region_of_interestPolygon defining the region of interest processed by the SDK, with coordinates normalized to 1.0string, default='[]'

Depth parameters

Parameters with prefix depth

ParameterDescriptionValue
depth_modeSelect depth map qualityNONE, PERFORMANCE, QUALITY, ULTRA, NEURAL, NEURAL_PLUS
depth_stabilizationDepth stabilization strength. Stabilizing the depth requires an additional computation load as it enables trackingint [0,100], 0: disabled
openni_depth_modeConvert 32-bit depth in meters to 16-bit in millimetersfalse: 32-bit float meters, true: 16-bit unsigned int millimeters
min_depthMinimum value allowed for depth measures (set in the camera model file)Min: 0.3 (ZED, ZED 2i), 0.2 (ZED 2, ZED X), 0.1 (ZED Mini, ZED X Mini), Max: 3.0 - Note: reducing this value will require more computational power and GPU memory. In cases of limited compute power, increasing this value can provide better performance
max_depthMaximum value allowed for depth measures (set in the camera model file)Max: 20.0 (ZED Mini), 40.0 (other models) - Values beyond this limit will be reported as TOO_FAR

Position parameters

Parameters with prefix pos_tracking

ParameterDescriptionValue
pos_tracking_enabledEnable/disable positional tracking from starttrue, false
pos_tracking_modePositional tracking mode of the ZED SDKGEN_1, GEN_2
set_gravity_as_originAlign the positional tracking world to the IMU gravity measurement, keeping the yaw from the initial posetrue, false
imu_fusionEnable/disable IMU fusion. When false, only the visual odometry is usedtrue, false
publish_tfEnable/disable publish TF framestrue, false
publish_map_tfEnable/disable publish map TF frametrue, false
map_frameFrame_id of the pose messagestring, default=map
odometry_frameFrame_id of the odom messagestring, default=odom
area_memory_db_pathPath of the database file for loop closure and relocalization that contains learnt visual information about the environmentstring, default=''
save_area_memory_db_on_exitSave the “known visual features” map when the node is correctly closed to the path indicated by area_memory_db_pathtrue, false
area_memoryEnable Loop Closingtrue, false
floor_alignmentIndicates if the floor must be used as origin for height measurestrue, false
initial_base_poseInitial reference posevector, default=[0.0,0.0,0.0, 0.0,0.0,0.0] -> [X, Y, Z, R, P, Y]
init_odom_with_first_valid_poseIndicates if the odometry must be initialized with the first valid pose received by the tracking algorithmtrue, false
path_pub_rateFrequency (Hz) of publishing of the trajectory messagesfloat, default=2.0
path_max_countMaximum number of poses kept in the pose arrays (-1 for infinite)int, default=-1
two_d_modeForce navigation on a plane. If true the Z value will be fixed to fixed_z_value, roll and pitch to zerotrue, false
fixed_z_valueValue to be used for Z coordinate if two_d_mode is truedouble, default=0.0
depth_min_rangeMinimum depth used by the visual odometry, to remove fixed parts of the robot in the camera field of viewdouble, default=0.0
set_as_staticIf true, the camera is considered static and does not move in the environmenttrue, false

Mapping parameters

Parameters with prefix mapping

ParameterDescriptionValue
mapping_enabledEnable/disable the mapping moduletrue, false
resolutionResolution of the fused point cloud in meters [0.01, 0.2]double, default=0.05
max_mapping_rangeMaximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]double, default=-1
fused_pointcloud_freqPublishing frequency (Hz) of the 3D map as fused point clouddouble, default=1.0
clicked_point_topicTopic published by RViz when a point is clicked. Used for plane detectionstring, default=/clicked_point

Sensors parameters (not available for the ZED)

Parameters with prefix sensors

ParameterDescriptionValue
sensors_timestamp_syncSynchronize Sensors message timestamp with latest received frametrue, false
max_pub_rateMaximum publishing frequency of the sensors datadouble, default=200.0, Max: 400.0
publish_imu_tfPublish IMU -> <camera_name>_left_camera_frame TFtrue, false

Object Detection parameters (not available for the ZED)

Parameters with prefix object_detection

ParameterDescriptionValue
od_enabledEnable/disable the Object Detection module when the node startstrue, false
modelObject Detection model to be usedstring, MULTI_CLASS_BOX_FAST, MULTI_CLASS_BOX_MEDIUM, MULTI_CLASS_BOX_ACCURATE, PERSON_HEAD_BOX_FAST, PERSON_HEAD_BOX_ACCURATE
confidence_thresholdMinimum value of the detection confidence of an objectint [0,100], default=50
max_rangeMaximum detection rangedouble, default=15.0
allow_reduced_precision_inferenceAllow inference to run at a lower precision to improve runtime and memory usagetrue, false
prediction_timeoutTime (seconds) during which a lost object keeps the OK state. 0 disables the SDK predictionsdouble, default=0.5
object_tracking_enabledEnable/disable the tracking of the detected objectstrue, false
mc_peopleEnable/disable the detection of persons for MULTI_CLASS_BOX_X modelstrue, false
mc_vehicleEnable/disable the detection of vehicles for MULTI_CLASS_BOX_X modelstrue, false
mc_bagEnable/disable the detection of bags for MULTI_CLASS_BOX_X modelstrue, false
mc_animalEnable/disable the detection of animals for MULTI_CLASS_BOX_X modelstrue, false
mc_electronicsEnable/disable the detection of electronic devices for MULTI_CLASS_BOX_X modelstrue, false
mc_fruit_vegetableEnable/disable the detection of fruits and vegetables for MULTI_CLASS_BOX_X modelstrue, false
mc_sportEnable/disable the detection of sport-related objects for MULTI_CLASS_BOX_X modelstrue, false

Dynamic parameters

The ZED node lets you reconfigure these parameters dynamically:

ParameterDescriptionValue
depth_confidenceThreshold to reject depth values based on their confidence. Each depth pixel has a corresponding confidence. A lower value means more confidence and precision (but less density). A higher value reduces filtering (more density, less certainty). A value of 100 disables the filtering.int [1,100], default=50
depth_texture_confThreshold to reject depth values based on their textureness confidence. A lower value means more confidence and precision (but less density). A higher value reduces filtering (more density, less certainty). A value of 100 disables the filtering.int [1,100], default=100
point_cloud_freqFrequency of the point cloud publishing (less than or equal to the general/pub_frame_rate value)double [0.1,60.0]
brightnessDefines the brightness controlint [0,8]
contrastDefines the contrast controlint [0,8]
hueDefines the hue controlint [0,11]
saturationDefines the saturation controlint [0,8]
sharpnessDefines the sharpness controlint [0,8]
gammaDefines the gamma controlint [1,9]
auto_exposure_gainDefines if the Gain and Exposure are in automatic mode or nottrue, false
gainDefines the gain control [only if auto_exposure_gain is false]int [0,100]
exposureDefines the exposure control [only if auto_exposure_gain is false]int [0,100]
auto_whitebalanceDefines if the White balance is in automatic mode or nottrue, false
whitebalance_temperatureDefines the color temperature value (x100)int [28,65]

To modify a dynamic parameter, you can use the GUI provided by the rqt stack:

rosrun rqt_reconfigure rqt_reconfigure
RQT Reconfigure

Transform frames

The ZED ROS wrapper broadcasts multiple coordinate frames that each provide information about the camera’s position and orientation. If needed, the reference frames can be changed in the launch file.

  • base_frame is the current position and orientation of the reference base of the robot
  • <camera_name>_camera_center is the current position and orientation of ZED, determined by visual odometry and the tracking module
  • <camera_name>_right_camera_frame is the position and orientation of the ZED’s right camera
  • <camera_name>_right_camera_optical_frame is the position and orientation of the ZED’s right camera optical frame
  • <camera_name>_left_camera_frame is the position and orientation of the ZED’s left camera
  • <camera_name>_left_camera_optical_frame is the position and orientation of the ZED’s left camera optical frame
  • <camera_name>_imu_link is the origin of the inertial data frame (not available for the ZED)
  • <camera_name>_mag_link is the origin of the magnetometer frame (ZED 2 and ZED 2i only)
  • <camera_name>_baro_link is the origin of the barometer frame (ZED 2 and ZED 2i only)
  • <camera_name>_temp_left_link is the origin of the left temperature frame (ZED 2 and ZED 2i only)
  • <camera_name>_temp_right_link is the origin of the right temperature frame (ZED 2 and ZED 2i only)

For RViz compatibility, the root frame map_frame is called map. The TF tree generated by the zed_wrapper reflects the standard described in REP105. The odometry frame is updated using the visual odometry information, fused with the inertial data when the camera has an IMU and pos_tracking/imu_fusion is true. The map frame is updated using the Tracking algorithm provided by the StereoLabs SDK, which also uses the spatial memory for loop closure and fuses the inertial information from the IMU sensor for the camera models that have one.

map_frame (`map`)
└─odometry_frame (`odom`)
└─base_frame (`base_link`)
└─camera_frame (`<camera_name>_camera_center`)
| └─left_camera_frame (`<camera_name>_left_camera_frame`)
| | └─left_camera_optical (`<camera_name>_left_camera_optical_frame`)
| | └─left_temperature_frame (`<camera_name>_temp_left_link`) (*only ZED 2 and ZED 2i*)
| | └─imu_frame (`<camera_name>_imu_link`) (*not available for the ZED*)
| └─right_camera_frame (`<camera_name>_right_camera_frame`)
| | └─right_camera_optical (`<camera_name>_right_camera_optical_frame`)
| | └─right_temperature_frame (`<camera_name>_temp_right_link`) (*only ZED 2 and ZED 2i*)
| └─magnetometer_frame (`<camera_name>_mag_link`) (*only ZED 2 and ZED 2i*)
| └─barometer_frame (`<camera_name>_baro_link`) (*only ZED 2 and ZED 2i*)

ZED Mini, ZED X and ZED X Mini

The ZED Mini, ZED X and ZED X Mini provide the same information as the ZED, plus the inertial data from the IMU sensor. The ZED X and ZED X Mini also provide the temperature of the IMU sensor. The IMU data are used internally to generate the pose in the Map frame with the Tracking sensor fusion algorithm.

The initial pose in Odometry frame can be set to the first pose received by the Tracking module by setting the parameter init_odom_with_first_valid_pose to true.

ZED 2 / ZED 2i

The ZED 2 and ZED 2i provide the same information as the ZED and the ZED Mini, plus the data from a new set of sensors. The ZED 2 and ZED 2i provide magnetometer data to get better and absolute information about the YAW angle, atmospheric pressure information to be used to estimate the height of the camera with respect to a reference point and temperature information to check the camera health in a complex robotic system.

Services

The ZED node provides the following services:

  • reset_tracking: Restarts the Tracking module setting the initial pose to the value available in the param server.
  • reset_odometry: Resets the odometry values eliminating the drift due to the Visual Odometry algorithm, setting the new odometry value to the latest camera pose received from the tracking module.
  • set_pose: Sets the current pose of the camera to the values passed as parameters -> X, Y, Z [m], R, P, Y [rad].
  • save_area_memory: Triggers the saving of the current area memory used for relocalization, if area memory is enabled.
  • set_led_status: Sets the status of the blue LED -> True: LED ON, False: LED OFF.
  • toggle_led: Toggles the status of the blue LED, returning the new status.
  • start_svo_recording: Starts recording an SVO file. If no filename is provided the default zed.svo is used. If no path is provided with the filename the default recording folder is ~/.ros/.
  • stop_svo_recording: Stops an active SVO recording.
  • start_remote_stream: Starts streaming over the network to allow processing of ZED data on a remote machine. See Remote streaming.
  • stop_remote_stream: Stops streaming over the network.
  • start_3d_mapping: Starts the Spatial Mapping processing. See Spatial Mapping.
  • stop_3d_mapping: Stops the Spatial Mapping processing (works even with an automatic start from the configuration file).
  • save_3d_map: Triggers the saving of the current 3D fused point cloud if the mapping module is enabled.
  • enable_object_detection: Starts (true) or stops (false) the Object Detection processing (std_srvs/SetBool). See Object Detection.
  • set_roi: Sets a region of interest, as a polygon with normalized coordinates, for the ZED SDK processing.
  • reset_roi: Resets the region of interest to the full image.

Currently the H26x SVO compression uses the resolution and the real FPS to calculate the bitrate. This feature can lead to some issues of quality when FPS is low. On NVIDIA® Jetson™ TX1 and NVIDIA® Jetson™ TX2, the FPS is quite low at the beginning of the grab loop, therefore it could be better to wait for some grab calls before calling start_svo_recording so that the camera FPS is stabilized at the requested value (15fps or more).

Remote streaming

SDK v2.8 introduced the capability to acquire ZED data and stream it on a remote machine over the network. This feature is useful when the ZED is connected to a machine with limited CUDA capabilities while a high-definition analysis is required. Starting the streaming without activating any other feature (i.e. depth processing, positional tracking, point cloud publishing, …) requires only the computing power needed for the H264 or H265 compression.

To start streaming the service start_remote_stream must be called with the following parameters:

  • codec (def. 0): Defines the codec used for streaming (0: AVCHD [H264], 1: HEVC [H265])

    If HEVC (H265) is used, make sure the receiving host is compatible with HEVC decoding (basically a Pascal NVIDIA® card). If not, prefer to use AVCHD (H264) since every compatible NVIDIA® card supports AVCHD decoding.

  • port (def. 30000): Defines the PORT the data will be streamed on.

    The port must be an even number. Any odd number will be rejected.

  • bitrate (def. 2000): Defines the streaming BITRATE in Kbits/s
  • gop_size (def. -1): Defines the GOP SIZE in frame unit.

    If the value is set to -1, the gop size will match 2 seconds, depending on the camera fps. The gop size determines the maximum distance between IDR/I-frames. Very high GOP size will result in slightly more efficient compression, especially on static scene. But it can result in more latency if IDR/I-frame packet are lost during streaming. Maximum allowed value is 256 (frames)

  • adaptative_bitrate (def. False): Enable/Disable adaptive bitrate.

    Bitrate will be adjusted regarding the number of packet loss during streaming. If activated, bitrate can vary between [bitrate/4, bitrate]. Currently, the adaptive bitrate only works when “sending” device is a NVIDIA® Jetson (X1, X2, Xavier, Nano)

Receive a remote stream

To acquire the streaming on a remote machine start a ZED node with the following command:

roslaunch zed_wrapper zed.launch stream:=<sender_IP>:<port>

For example:

roslaunch zed_wrapper zed.launch stream:=192.168.1.127:30000

The stream contains only visual information. When using a ZED Mini camera, the inertial topics are not available unless they are subscribed to using the standard ROS methods.

Spatial Mapping

The ZED node provides a basic mapping module publishing a 3D map of the environment as a 3D color point cloud (mapping/fused_cloud).

Spatial Mapping is disabled by default because it is computationally heavy. It can be enabled by setting to true the parameter mapping/mapping_enabled in the file params/common.yaml.

Spatial Mapping can be enabled manually at any time using the start_3d_mapping service.

To reduce the computational power requirements, use a value higher than 0.1 m for resolution and decrease the value of fused_pointcloud_freq to reduce the frequency of the point cloud topic publishing.

Mapping on RViz

It is possible to save the generated 3D map as a point cloud in the PLY, binary PLY or OBJ format, by calling the save_3d_map service.

Object Detection

The Object Detection module allows the detection and tracking of Objects.

Object detection is disabled by default because it is computationally heavy. It can be automatically enabled when the node starts by setting to true the parameter object_detection/od_enabled in the file params/common.yaml.

If Object Detection is disabled, it can be manually enabled at any time by calling the enable_object_detection service with true.

The list of the detected objects is published on the obj_det/objects topic as a custom message of type zed_interfaces/ObjectsStamped. For details about the message fields, please read the Object Detection tutorial and the Object Detection module documentation.

Object Tracking

Enabling Object Tracking allows getting information frame by frame about the status of each detected object. The same object is identified with the same ID in all the frames after its first detection and its position is estimated if an occlusion occurs.

Each detected object can get four different values about its Tracking Status:

  • OFF - The tracking is not yet initialized, and the object ID is not usable
  • OK - The object is tracked
  • SEARCHING - The object couldn’t be detected in the image and is potentially occluded, the trajectory is estimated
  • TERMINATE - This is the last searching state of the track, the track will be deleted in the next retrieveObjects
Object Detection

Diagnostic

The ZED node publishes diagnostic information that can be used by the robotics system using a diagnostic_aggregator node.

Using the Runtime monitor plugin of rqt it is possible to get all the diagnostic information and check that the node is working as expected:

RQT Diagnostic

A brief explanation of each field:

  • Component: name of the diagnostic component
  • Message: summary of the status of the ZED node
  • HardwareID: Model of the ZED camera and its serial number
  • Capture: grabbing frequency (if video or depth data are subscribed) and the percentage with respect to the camera frame rate
  • Processing time: time in seconds spent processing data and the time limit to achieve max frame rate
  • Playing SVO: (visible only if playing an SVO file) current frame position in the SVO file over the total frame count
  • Depth status: indicates if the depth processing is performed
  • Point Cloud: point cloud publishing frequency (if there is at least a subscriber) and the percentage with respect to the camera frame rate
  • Floor Detection: if the floor detection is enabled, indicates if the floor has been detected and the camera position correctly initialized
  • Tracking status: indicates the status of the positional tracking if enabled
  • Object data processing: if Object Detection is enabled indicates the time required to process the data relative to detected objects
  • IMU: the publishing frequency of the IMU topics, if the camera has an IMU and there is at least a subscriber
  • Left CMOS Temp.: (only ZED 2 and ZED 2i) the temperature of the CMOS of the left camera sensor [-273.15°C if not valid]
  • Right CMOS Temp.: (only ZED 2 and ZED 2i) the temperature of the CMOS of the right camera sensor [-273.15°C if not valid]
  • SVO Recording: indicates if the SVO recording is active
  • SVO Compression time: average time spent on frame compressing
  • SVO Compression ratio: average frame compression ratio

Using multiple ZEDs

It is possible to use multiple ZED cameras with ROS. Simply launch the nodes with the zed_multi_cam.launch file:

roslaunch zed_multicamera_example zed_multi_cam.launch

Assigning a GPU to a camera

To improve performance, you can specify the gpu_id of the graphic card that will be used for the depth computation in the launch file. The default value (-1) will select the GPU with the highest number of CUDA cores. When using multiple ZEDs, you can assign each camera to a GPU to increase performance.

Limitations

Performance

This wrapper lets you quickly prototype applications and interface the ZED with other sensors and packages available in ROS. However, the ROS layer introduces significant latency and a performance hit. If performance is a major concern for your application, please consider using the ZED SDK library.

Multiple ZEDs

The ZED camera uses the maximum bandwidth provided by USB 3.0 to output video. When using multiple ZEDs, you may need to reduce camera framerate and resolution to avoid corrupted frames (green or purple frames). You can also use multiple GPUs to load-balance computations and improve performance.