Skip to navigation

Running ZED SDK in a Docker Container

Open in ClaudeOpen in ChatGPT

Docker is the easiest way to set up ZED SDK on Linux and NVIDIA® Jetson™. Docker uses containers to create virtual environments that contain all the required dependencies and isolate an installation from the rest of the system.

StereoLabs provides two types of ZED SDK Docker images for each release:

  • runtime images include the minimum dependencies required to run applications using the ZED SDK. Use these images for production.

  • devel images are ideal for development. They contain all the tools needed to compile an application, including CUDA and the static libraries and headers of the ZED SDK.

Run a ZED SDK Container

Use the following command:

docker pull stereolabs/zed:[tag] # Download image with specified tag
docker run --gpus all -it --privileged stereolabs/zed:[tag] # Start container

The --gpus all flag adds all available GPUs to the container, and --privileged grants the container permission to access the camera connected via USB.

On NVIDIA® Jetson™, use --runtime nvidia instead of --gpus all. See Install on NVIDIA® Jetson™ for the complete setup, including GMSL2 cameras.

To choose between the image variants, manage your containers and images, and keep the AI models and calibration files across containers, see Manage Containers and Images.