Skip to navigation

Tutorial - Using Human Body Tracking

Open in ClaudeOpen in ChatGPT

This tutorial shows how to enable the Body Tracking module to detect and track 3D human body skeletons, with a confidence threshold you can tune for the scene (lower for outdoor/long-range use, higher for indoor/close-range use to avoid false positives). This module requires a stereo camera with an integrated IMU (ZED 2/2i, ZED Mini, ZED X or ZED X Mini); the original ZED and the ZED X Nano are not supported.

Getting Started

  • First, download the latest version of the ZED SDK.
  • Download the Body Tracking sample code in C, C++, Python or C#.

Code Overview

Open the camera

In this tutorial, we will use the Body Tracking AI module of the ZED SDK. As in previous tutorials, we create, configure and open the camera.

// Create ZED objects
Camera zed;
InitParameters initParameters;
initParameters.camera_resolution = RESOLUTION::HD720;
initParameters.depth_mode = DEPTH_MODE::NEURAL;
// Open the camera
ERROR_CODE zed_error = zed.open(initParameters);
if (zed_error != ERROR_CODE::SUCCESS) {
std::cout << "Error " << zed_error << ", exit program.\n";
return 1; // Quit if an error occurred
}

Enable Body Tracking

Before enabling body tracking, we specify the BodyTrackingParameters of the module.

Body tracking needs positional tracking to be able to track the bodies in the world reference frame.

// Define the Body Tracking module parameters
BodyTrackingParameters detection_parameters;
// Different models can be chosen, optimizing the runtime or the accuracy
detection_parameters.detection_model = BODY_TRACKING_MODEL::HUMAN_BODY_FAST;
// Enable tracking to detect bodies across time and space
detection_parameters.enable_tracking = true;
// Optimize the person joints position, requires more computations
detection_parameters.enable_body_fitting = true;
// If you want to track bodies you need to enable positional tracking first
if (detection_parameters.enable_tracking)
zed.enablePositionalTracking();

Then we can start the module, which loads the AI model. This operation can take a few seconds. The first time the module is used, the model will be optimized for the hardware and will take more time. This operation is done only once.

cout << "Body Tracking: Loading Module..." << endl;
zed_error = zed.enableBodyTracking(detection_parameters);
if (zed_error != ERROR_CODE::SUCCESS) {
cout << "Error " << zed_error << ", exit program.\n";
zed.close();
return EXIT_FAILURE;
}

Capture Data

The detection confidence threshold can be adjusted at runtime to select only the relevant skeletons depending on the scene complexity. For each grab call, the image is fed into the AI module, which outputs the bodies detected in that frame.

// Set runtime parameter confidence to 40
BodyTrackingRuntimeParameters body_parameters_rt;
body_parameters_rt.detection_confidence_threshold = 40;
Bodies bodies;
// Grab new frames and detect bodies
while (zed.grab() == ERROR_CODE::SUCCESS) {
zed.retrieveBodies(bodies, body_parameters_rt);
if (bodies.is_new) {
// Count the number of bodies detected
cout << bodies.body_list.size() << " Person(s) detected\n";
if (!bodies.body_list.empty()) {
auto first_body = bodies.body_list.front();
// Display the 3D keypoint coordinates of the first detected person
cout << " Keypoints 3D \n";
for (int i = 0; i < first_body.keypoint.size(); i++) {
auto &kp = first_body.keypoint[i];
cout << " " << kp.x << ", " << kp.y << ", " << kp.z << "\n";
}
}
}
}

Disable modules and exit

Once the program is over, the modules can be disabled and the camera closed. This step is optional since the zed.close() will take care of disabling all the modules. This function is also called automatically by the destructor if necessary.

// Disable body tracking and close the camera
zed.disableBodyTracking();
zed.close();

And this is it!