ROS 2 - ZED Stereo Node
The easiest way to start a ZED ROS 2 node for a stereo camera is by using the command line:
where <camera model> must be replaced with one in the list zed, zedm, zed2, zed2i, zedx, zedxm, zedxnano, and virtual.
Published Topics
Not all the topics are advertised by default. The version v5.1.0 of the ROS 2 Wrapper introduces new parameters to enable/disable the publishing of each topic. Please refer to the “Configuration parameters” section for more details.
The ZED node publishes data to the following topics:
-
Status
~/status/health: the general status of the node (custom message).~/status/heartbeat: heartbeat signal to monitor if the node is alive from other nodes (custom message).~/status/svo: the status of the SVO playback (custom message). Only advertised when an SVO file is used as input.
-
Image streams
The image topic names are created using the following naming convention:
~/<sensor_type>/<color_model>/<rect_type>/image
Starting from version 5.1.0 of the ROS 2 Wrapper the new convention replaces the previous formats such as ~/<sensor_type>/image_<rect_type>_<color_model> and ~/<sensor_type>_<rect_type>/image_<rect_type>_<color_model> (e.g., ~/left/image_rect_color, ~/rgb_raw/image_raw_gray). Please update your launch files and scripts to use the new topic names.
-
RGB channel
~/rgb/color/rect/image: Color rectified image.~/rgb/color/rect/camera_info: Color camera calibration data.~/rgb/gray/rect/image: Grayscale rectified image.~/rgb/gray/rect/camera_info: Grayscale camera calibration data.~/rgb/color/raw/image: Color unrectified image.~/rgb/color/raw/camera_info: Color raw calibration data.~/rgb/gray/raw/image: Grayscale unrectified image.~/rgb/gray/raw/camera_info: Grayscale raw calibration data.
-
Left channel
~/left/color/rect/image: Left sensor RGB rectified image.~/left/color/rect/camera_info: Left sensor RGB camera calibration data.~/left/gray/rect/image: Left sensor Grayscale rectified image.~/left/gray/rect/camera_info: Left sensor Grayscale camera calibration data.~/left/color/raw/image: Left sensor RGB unrectified image.~/left/color/raw/camera_info: Left sensor RGB raw calibration data.~/left/gray/raw/image: Left sensor Grayscale unrectified image.~/left/gray/raw/camera_info: Left sensor Grayscale raw calibration data.
-
Right channel
~/right/color/rect/image: Right sensor RGB rectified image.~/right/color/rect/camera_info: Right sensor RGB camera calibration data.~/right/gray/rect/image: Right sensor Grayscale rectified image.~/right/gray/rect/camera_info: Right sensor Grayscale camera calibration data.~/right/color/raw/image: Right sensor RGB unrectified image.~/right/color/raw/camera_info: Right sensor RGB raw calibration data.~/right/gray/raw/image: Right sensor Grayscale unrectified image.~/right/gray/raw/camera_info: Right sensor Grayscale raw calibration data.
Since v5.5.0 of the ROS 2 Wrapper the distortion_model and the distortion coefficients published in the camera_info topics are read from the ZED SDK (>= 5.4) instead of a hard-coded per-model table that the lens does not always follow: a fisheye ZED X One now reports equidistant instead of rational_polynomial. Rectified parameters are reported as plumb_bob with zero coefficients.
The rgb and left channels of stereo cameras are identical. We use both names to differentiate the usage: while left and right are used for stereo processing, rgb is associated with the synchronized depth map.
-
Stereo pair
~/stereo/color/rect/image: side-by-side left/right rectified stereo pair. Calibration data are available in the topics:~/left/color/rect/camera_infoand~/right/color/rect/camera_info.~/stereo/color/raw/image: side-by-side left/right unrectified stereo pair. Calibration data are available in the topics:~/left/color/raw/camera_infoand~/right/color/raw/camera_info.
-
Depth and point cloud
~/depth/camera_info: Depth camera calibration data.~/depth/depth_registered: Depth map image registered on left image.~/depth/depth_info: minimum and maximum depth information (custom message).~/point_cloud/cloud_registered: Registered color point cloud.~/confidence/confidence_map: Confidence image (floating point values).~/disparity/map: disparity map, of typestereo_msgs/msg/DisparityImage, to be used for depth processing.~/disparity/image: normalized disparity map, of typesensor_msgs/msg/Image, for visualization purposes. This is the topic to subscribe to in RViz 2.
The topic ~/disparity/disparity_image is obsolete since v5.4.0 of the ROS 2 Wrapper and is replaced by the two topics above. To visualize the disparity map, run ros2 run image_view disparity_view --ros-args -r image:=/zed/zed_node/disparity/map.
-
Region of Interest
~/roi_mask/image: the Region of Interest mask applied to the ZED SDK processing. See the Region of Interest page.
-
Sensors data
~/left_cam_imu_transform: Transform from the left camera sensor to the IMU sensor.~/imu/data: Accelerometer, gyroscope, and orientation data in Earth frame.~/imu/data_raw: Accelerometer and gyroscope data in Earth frame.~/imu/mag: Raw magnetometer data (only ZED 2 and ZED 2i).~/atm_press: atmospheric pressure (only ZED 2 and ZED 2i).~/temperature/imu: temperature measured by the IMU sensor.~/temperature/left: temperature measured near the left CMOS sensor (only ZED 2 and ZED 2i).~/temperature/right: temperature measured near the right CMOS sensor (only ZED 2 and ZED 2i).
-
Positional tracking
~/pose: Absolute 3D position and orientation relative to the Map frame (Sensor Fusion algorithm + SLAM).~/pose/status: the status of the positional tracking module (custom message).~/pose_with_covariance: Camera pose referred to Map frame with covariance.~/odom: Absolute 3D position and orientation relative to the Odometry frame (visual-inertial odometry on cameras equipped with an IMU, pure visual odometry on the original ZED).~/odom/status: the status of the odometry from the positional tracking module (custom message).~/path_map: Sequence of camera poses in Map frame.~/path_odom: Sequence of camera odometry poses in Map frame.~/pose/landmarks: the 3D landmarks used by the positional tracking algorithm, published as asensor_msgs/msg/PointCloud2message.
-
Geo Tracking
~/pose/filtered: the GNSS fused pose of the robot~/pose/filtered/status: the status of the GNSS fused pose (custom message).~/geo_pose: the Latitude/Longitude pose of the robot~/geo_pose/status: the status of the Latitude/Longitude pose (custom message).~/pose/fused_fix: the GNSS fused fix of the robot, published as asensor_msgs/msg/NavSatFixmessage.~/pose/origin_fix: the Latitude/Longitude of the origin of themapframe, published as asensor_msgs/msg/NavSatFixmessage.
-
3D Mapping
~/mapping/fused_cloud: Fused point cloud created when theenable_mappingservice is called.
-
Object Detection
~/obj_det/objects: detected objects (custom message).
-
Body Tracking
~/body_trk/skeletons: detected body skeletons (custom message).
-
Plane Detection
~/plane: Detected plane (custom message).~/plane_marker: Detected plane object to be displayed on RViz 2.
Each topic has a common prefix created by the launch file as ~ = /<namespace>/<node_name>/, where <namespace> is replaced with the value of the parameter camera_name and <node_name> is the name of the node, e.g. zed_node.
Image Transport
The ROS 2 wrapper supports the stack image_transport introduced with ROS 2 Crystal Clemmys.
Starting from version 5.3 of the ROS 2 Wrapper, image messages are published through rclcpp::TypeAdapter for more efficient handling:
- The base
rawtopic is handled by aTypeAdapterpublisher. Intra-process subscribers (e.g., other nodes running in the same component container) receive aStampedSlMatobject (a wrapper around the nativesl::Mat) directly, without any serialization overhead. Inter-process subscribers transparently receive a standardsensor_msgs/msg/Imagemessage thanks to the automaticTypeAdapterconversion. - The transport-specific variants are handled by an
image_transportpublisher. Itsrawtransport is disabled to avoid publishing duplicate messages, since therawstream is already provided by theTypeAdapterpublisher described above.
To prevent silent data corruption caused by incompatible plugin/encoding combinations (e.g., applying JPEG compression to floating-point depth data), the advertised image transports are filtered by topic type:
- Visual image topics (color and grayscale images) advertise only:
compressed: JPEG or PNG compressed imagetheora: Ogg Theora compressed imagezstd: lossless Zstandard-compressed image (available starting with ROS 2 Jazzy Jalisco)
- Measurement topics (e.g., depth) advertise only:
compressedDepth: depth image compressed with a lossless algorithmzstd: lossless Zstandard-compressed image (available starting with ROS 2 Jazzy Jalisco)
For proper association between images and their corresponding camera information, the ZED ROS 2 Wrapper also publishes camera_info topics for all compressed image streams:
~/rgb/color/rect/image/camera_info~/rgb/gray/rect/image/camera_info~/rgb/color/raw/image/camera_info~/rgb/gray/raw/image/camera_info
When the isaac_ros_nitros package is installed and NITROS is not disabled via the debug.disable_nitros parameter, NITROS publishers take priority and neither the TypeAdapter nor the image_transport publishers are created. Please refer to the dedicated section about NVIDIA® Isaac ROS Nitros for more details.
NVIDIA® Isaac ROS Nitros
The ZED ROS 2 Wrapper supports the NVIDIA® Isaac™ ROS Nitros package for zero-copy transport of ROS messages using NVIDIA® GPUDirect® RDMA.
NVIDIA® Isaac ROS Nitros integration is enabled and used only if the required packages are manually installed. They are not added as a dependency because this is an optional feature.
Starting from version 5.3 of the ROS 2 Wrapper, Intra-Process Communication (IPC) is handled automatically:
- If NITROS is not installed on the host machine, IPC is always enabled.
- If NITROS is installed, IPC is disabled and NITROS takes priority.
If you want to use IPC on a machine where NITROS is installed, set the debug.disable_nitros parameter to true to disable NITROS; IPC will then be enabled automatically. (This parameter has no effect when NITROS is not installed, since IPC is already active.)
IPC is also controlled by the enable_ipc launch argument of zed_camera.launch.py (default true). When NITROS is installed and debug.disable_nitros is false, IPC and NITROS conflict: with the default ipc_nitros_conflict_policy:=disable_ipc the launch file logs a warning and forces enable_ipc:=false for that launch. To use NITROS, you can also set enable_ipc:=false explicitly, as required by the Isaac ROS integration. Set enable_ipc:=false as well when no component shares the container with the ZED node and you do not need intra-process delivery.
For more information about the installation and usage of the NVIDIA® Isaac™ ROS packages, please refer to the dedicated section of the documentation: ZED Isaac™ ROS Integration Overview.
Point Cloud Transport
The ROS 2 wrapper supports the stack pointcloud_transport introduced with ROS 2 Humble Hawksbill.
The point cloud transport is enabled and used only if the required packages are manually installed, they are not added as a dependency because this is an optional feature:
Point cloud topics are published using the point_cloud_transport::Publisher object, which provides both standard raw and compressed point cloud streams for efficient data transmission.
QoS profiles
All the topics are configured by default to use the following ROS 2 QoS profile:
- Reliability: RELIABLE
- History (Depth): KEEP_LAST (10)
- Durability: VOLATILE
- Lifespan: Infinite
- Deadline: Infinite
- Liveliness: AUTOMATIC
- Liveliness lease duration: Infinite
Read the official ROS 2 documentation about the QoS and the related settings for details.
The QoS settings can be modified by changing the relative parameters in the YAML files, as described in this official ROS 2 design document.
When creating a subscriber, be sure to use a compatible QoS profile according to the following tables:
Compatibility of QoS durability profiles:
Compatibility of QoS reliability profiles:
In order for a connection to be made, all of the policies that affect compatibility must be compatible. For instance, if a publisher-subscriber pair has compatible reliability QoS profiles, but incompatible durability QoS profiles, the connection will not be made.
For a detailed list of all the compatibility settings, please refer to the official ROS 2 documentation.
Configuration parameters
Specify your launch parameters in the common_stereo.yaml, zed.yaml, zedm.yaml, zed2.yaml, zed2i.yaml, zedx.yaml, zedxm.yaml, zedxnano.yaml, and virtual.yaml files available in the folder zed_wrapper/config.
General parameters
Namespace: general
common_stereo.yaml
* Dynamic parameter
timestamp_reference: 'IMAGE_CENTER_OF_EXPOSURE' requires an input that carries a per-frame exposure, that is a ZED X or a ZED X Mini, live, from an SVO or from a stream. On the USB models the node warns once and falls back to IMAGE. It is not applied to the sensors data, to the SVO /clock topic, nor in simulation.
zed.yaml, zedm.yaml, zed2.yaml, zed2i.yaml, zedx.yaml, zedxm.yaml, zedxnano.yaml, and virtual.yaml
Valid grab_resolution values per camera model:
SVO input parameters
Namespace: svo
common_stereo.yaml
SVO encryption requires OpenSSL (libcrypto) at runtime. The value of svo.encryption_key is never written to the log, and the same value must be set as svo.decryption_key to play the recording back: if the key is lost the recorded data is unrecoverable.
Streaming input parameters
Namespace: stream
common_stereo.yaml
Simulation input parameters
Namespace: simulation
common_stereo.yaml
Streaming server parameters
Namespace: stream_server
common_stereo.yaml
Video parameters
Namespace: video
common_stereo.yaml
* Dynamic parameter
zed.yaml, zed2.yaml, and zed2i.yaml
* Dynamic parameter
zedx.yaml, zedxm.yaml, zedxnano.yaml, and virtual.yaml
* Dynamic parameter
Region of Interest parameters
Namespace: region_of_interest
common_stereo.yaml
Depth parameters
Namespace: depth
common_stereo.yaml
To disable depth calculation set depth_mode to NONE. All the other parameters relative to depth will be ignored and only the video streams and sensors data will be published.
* Dynamic parameter
zed.yaml, zedm.yaml, zed2.yaml, zed2i.yaml, zedx.yaml, zedxm.yaml, zedxnano.yaml, and virtual.yaml
* Dynamic parameter
Positional tracking parameters (Odometry and Localization)
Namespace: pos_tracking
common_stereo.yaml
Global Localization (GNSS Fusion)
Namespace: gnss_fusion
common_stereo.yaml
Mapping parameters
Namespace: mapping
common_stereo.yaml
Sensors parameters
Namespace: sensors
common_stereo.yaml
Starting from v5.5.0 of the ROS 2 Wrapper the sensors stream is read independently of grab(), so the IMU publishing delay no longer depends on general.grab_frame_rate nor on general.grab_compute_capping_fps. Measured on a ZED X on an AGX Orin, the median publish delay dropped from 411 ms to 10.5 ms and the output rate went from 92.6 Hz to the requested 100.0 Hz.
sensors.sensors_pub_rate is now decimated against the measured sample interval instead of the rate the ZED SDK advertises, so it is honored on cameras whose IMU does not run at the advertised rate (a ZED X One GS advertises 400 Hz but delivers 200 Hz), and cameras that report correctly produce exactly the requested rate.
Two consequences of the reduced CPU usage of the sensors thread: a new subscriber to a sensors topic can wait up to 250 ms for its first message, and a subscriber whose QoS is incompatible with the publisher no longer triggers publishing (it could never receive the data anyway).
Object detection parameters
Namespace: object_detection
common_stereo.yaml
object_detection.yaml
* Dynamic parameter
custom_object_detection.yaml
FOR EACH CLASS CREATE THE FOLLOWING PARAMETERS
* Dynamic parameter
Body Tracking parameters
Namespace: body_tracking
common_stereo.yaml
* Dynamic parameter
Starting from v5.5.0 of the ROS 2 Wrapper the default body_tracking.body_format is BODY_34 instead of BODY_38, and body_tracking.enable_body_fitting defaults to true. Only BODY_18 and BODY_34 have a GEN_2 network, so the previous default silently fell back to the older GEN_1. Skeletons published on ~/body_trk/skeletons now carry 34 keypoints instead of 38: set body_format back to BODY_38 to keep the previous topology, at the cost of running GEN_1.
Advanced parameters
Namespace: advanced
These are advanced threading parameters. Do not modify them unless you are confident of what you are doing. The SCHED_FIFO and SCHED_RR scheduling policies require running with sudo. Reference: sched(7).
common_stereo.yaml
Debug parameters
Namespace: debug
common_stereo.yaml
Dynamic parameters
The ZED node lets you reconfigure many parameters dynamically during the execution of the node. All the dynamic parameters are indicated with a * in the list above and with the tag [DYNAMIC] in the comments of the YAML files.
You can set the parameters using the CLI command ros2 param set, e.g.:
If the parameter is set successfully, you will get a confirmation message:
In the case you tried to set a parameter that’s not dynamically reconfigurable, or you specified an invalid value, you will get this type of error:
You can also use the Configuration -> Dynamic Reconfigure plugin of the rqt tool to dynamically set parameters by using a graphic interface.
Transform frames
The ZED ROS 2 wrapper broadcasts multiple coordinate frames that each provides information about the camera’s position and orientation. If needed, the reference frames can be changed in the launch file.
<camera_name>_camera_linkis the current position and orientation of the ZED base center. It corresponds to the bottom central fixing hole.<camera_name>_camera_centeris the current position and orientation of ZED middle baseline, determined by visual odometry and the tracking module.<camera_name>_right_camera_frameis the position and orientation of the ZED’s right camera.<camera_name>_right_camera_frame_opticalis the position and orientation of the ZED’s right camera optical frame.<camera_name>_left_camera_frameis the position and orientation of the ZED’s left camera.<camera_name>_left_camera_frame_opticalis the position and orientation of the ZED’s left camera optical frame.<camera_name>_imu_linkis the origin of the inertial data frame (not available with ZED).<camera_name>_mag_linkis the origin of the magnetometer frame (ZED2/ZED2i only).<camera_name>_baro_linkis the origin of the barometer frame (ZED2/ZED2i only).<camera_name>_temp_left_linkis the origin of the left temperature frame (ZED2/ZED2i only).<camera_name>_temp_right_linkis the origin of the right temperature frame (ZED2/ZED2i only).
For RViz 2 compatibility, the root frame map_frame is called map.
The TF tree generated by the zed_wrapper reflects the standard described in REP105.
The odometry frame is updated using only the “visual inertial odometry” information (loop closure is not applied).
The map frame is updated using the Positional Tracking algorithm provided by the StereoLabs SDK, fusing the inertial information from the IMU sensor, and applying loop closure information.
When the Geo Tracking module is enabled the ZED Node TF Tree reflects the following diagram:
Services
The ZED node provides the following services:
~/reset_odometry(std_srvs/srv/Trigger): Resets the odometry values eliminating the drift due to the Visual Odometry algorithm. The new odometry value is set to the latest camera pose received from the tracking algorithm. Only available if positional tracking is enabled.~/reset_pos_tracking(std_srvs/srv/Trigger): Restarts the Tracking algorithm setting the initial pose to the value available in the param server or to the latest pose set with the serviceset_pose. Only available if positional tracking is enabled.~/set_pose(zed_msgs/srv/SetPose): Restarts the Tracking algorithm setting the initial pose of the camera to the value passed as vector parameter -> [X, Y, Z, R, P, Y]. Only available if positional tracking is enabled.~/save_area_memory(zed_msgs/srv/SaveAreaMemory): Saves the Area Memory (.areafile) of the current session so that it can be reloaded later with thepos_tracking.area_file_pathparameter. The file path is passed in the request; if it is empty the value ofpos_tracking.area_file_pathis used. Only available if positional tracking is enabled.~/enable_depth(std_srvs/srv/SetBool): enable/disable the depth processing at runtime. Not available ifdepth.depth_modeisNONE.~/enable_obj_det(std_srvs/srv/SetBool): enable/disable object detection.~/enable_body_trk(std_srvs/srv/SetBool): enable/disable body tracking.~/enable_mapping(std_srvs/srv/SetBool): enable/disable spatial mapping.~/enable_streaming(std_srvs/srv/SetBool): enable/disable a local streaming server.~/start_svo_rec(zed_msgs/srv/StartSvoRec): Start recording an SVO file. If no filename is provided the defaultzed.svo2is used. A filename without a path is saved in the working directory of the node process.~/stop_svo_rec(std_srvs/srv/Trigger): Stop an active SVO recording.~/pause_svo_rec(std_srvs/srv/SetBool): Pause (data: true) and resume (data: false) an active SVO recording without closing the file. It returnssuccess: falsewhen no recording is active, and the diagnostic reportsSVO Recording: PAUSEDwhile paused.~/toggle_svo_pause(std_srvs/srv/Trigger): set/reset SVO playing pause. Only available ifsvo.svo_realtimeis false and if an SVO has been chosen as input source.~/set_svo_frame(zed_msgs/srv/SetSvoFrame): Set the SVO playback frame to the specified value. Only available if an SVO has been chosen as input source.~/set_roi(zed_msgs/srv/SetROI): Set the Region of Interest to the described polygon.~/reset_roi(std_srvs/srv/Trigger): Reset the Region of Interest to the full image frame.~/toLL(robot_localization/srv/ToLL): converts frommapcoordinate frame to Latitude/Longitude. Only available if GNSS fusion is enabled.~/fromLL(robot_localization/srv/FromLL): converts from Latitude/Longitude tomapcoordinate frame. Only available if GNSS fusion is enabled.
When positional tracking is disabled (pos_tracking.pos_tracking_enabled: false) the positional tracking and the spatial mapping services are not advertised at all.
Services can be called using the rqt graphical tool by enabling the plugin Plugins -> Services -> Service caller.
It is possible to call a service also by using the CLI command ros2 service call.
For example, to start Object Detection:
and the service server will reply:
Assigning a GPU to a camera
To improve performance, you can specify the gpu_id of the graphic card that will be used for the depth computation in the common_stereo.yaml configuration file. The default value (-1) will select the GPU with the highest number of CUDA cores. When using multiple ZEDs, you can assign each camera to a GPU to increase performance.
Node Diagnostic
The ZED ROS 2 node publishes useful diagnostic information aggregated into the /diagnostics topic using the diagnostic_updater package.
Diagnostic information can be analyzed and parsed by using ROS 2 tools, like for example the Runtime Monitor plugin of rqt.
Available information:
- Uptime
- Grab frequency and processing time
- Frame drop rate
- Input mode
- Video and Depth publishing rate and processing time
- Depth Mode
- Point Cloud publishing rate and processing time
- GNSS Fusion status
- Odometry and Localization status
- Pose confidence: the
[0,100]quality metric of the positional tracking. It requires ZED SDK >= 5.4 andPOSITIONAL_TRACKING_MODE::GEN_3, and is reported asN/Aotherwise - TF broadcasting rate
- Object Detection status and publishing rate
- Body Tracking status and publishing rate
- IMU TF broadcasting rate
- Sensor data publishing rate
- Camera Internal temperatures
- Scene Illuminance (ZED X family)
- Camera health status: image quality, lighting, depth reliability, motion sensors reliability and, with ZED SDK >= 5.5 and
zed_msgsv5.5, duplicated images - SVO playback status
- SVO recording status, including the
PAUSEDstate - Streaming server status
The diagnostic goes to WARN and names the issues while any camera health check is raised. It reports DISABLED when general.enable_image_validity_check is off.