Skip to navigation

Custom Object Detection and Tracking with ROS 2

Open in ClaudeOpen in ChatGPT

This guide explains how to use a custom YOLO-like or RF-DETR-like model for object detection with the ZED ROS 2 Wrapper. This is useful if you have trained your own model and want to integrate it with the ZED SDK.

The custom model must:

  • Be in ONNX format
  • Be compatible with the ZED SDK
  • Be exported correctly for integration

To enable your custom model:

  1. Generate the ONNX file from your trained model.
  2. Set the object_detection.custom_onnx_file parameter in your configuration.

Three detection models run a user-provided ONNX file inside the ZED SDK:

MODELDescription
CUSTOM_YOLOLIKE_BOX_OBJECTSThe ONNX file is a YOLO-like model
CUSTOM_RFDETRLIKE_BOX_OBJECTSThe ONNX file is an RF-DETR-like model. Requires ZED SDK >= 5.5
CUSTOM_BOX_OBJECTS_AUTODETECTThe ZED SDK picks between YOLO-like and RF-DETR-like from the model outputs. Requires ZED SDK >= 5.5

Export the YOLO-like ONNX Model

You can perform object detection inference using a custom YOLO-like ONNX model.

Refer to the YOLO ONNX model export documentation for detailed instructions.

Here’s a quick example using Ultralytics YOLOv8:

python -m pip install -U ultralytics
yolo export model=yolov8s.pt format=onnx simplify=True dynamic=False imgsz=512

Setup the Custom Model usage

To use your model:

  1. Set the following in your common_stereo.yaml:

    object_detection:
    detection_model: 'CUSTOM_YOLOLIKE_BOX_OBJECTS' # or 'CUSTOM_RFDETRLIKE_BOX_OBJECTS' / 'CUSTOM_BOX_OBJECTS_AUTODETECT'
    enable_tracking: true # Enable detected object tracking

    When enable_tracking is true, the ZED SDK’s advanced algorithms can track the detected objects over time, even if they are temporarily occluded or move out of the camera’s field of view.

    The field tracking_state in the zed_msgs/ObjectsStamped message will indicate the tracking state of each detected object. The possible values are:

    • 0 -> OFF: object is no longer valid
    • 1 -> OK: object is valid and tracked
    • 2 -> SEARCHING: occlusion occurred, trajectory is estimated
    • 3 -> TERMINATE: the track will be deleted in the next frame
  2. Create a custom ONNX configuration file using the custom_object_detection.yaml template.

Create a Custom Object Detection Model Configuration File

The header of your YAML config should look like this:

/**:
ros__parameters:
object_detection:
custom_onnx_file: '' # Path to your ONNX file
custom_onnx_input_size: 512 # Input resolution (e.g., 512 for 1x3x512x512 tensor)
custom_class_count: 80 # Number of classes in your model (e.g., 80 for COCO)
  • Set the custom_onnx_file parameter to the path of your ONNX file.
  • Set the custom_onnx_input_size parameter to the size of the square input tensor of the ONNX file, e.g. 512 for a 1x3x512x512 tensor. It must match the size used to optimize the model ahead of time with sl::optimizeCustomAIModel() or ZED_Diagnostic -onnx <path> [WxH], otherwise the cached engine is not reused and the model is optimized again on the first run.
  • Set the custom_class_count parameter to the number of classes your model was trained on (e.g., 80 for COCO dataset).

Class-Specific Configuration

For each class, add a class_XXX block (where XXX is the class index, from 0 to custom_class_count - 1):

class_XXX:
label: '' # Label of the object in the custom ONNX file
model_class_id: 0 # Class ID of the object in the custom ONNX file (it is not required that this value matches the value in the 'class_XXX' identifier)
enabled: true # Enable/disable the detection of this class
confidence_threshold: 50.0 # Minimum value of the detection confidence of an object [0,99]
is_grounded: true # Provide hypothesis about the object movements (degrees of freedom or DoF) to improve the object tracking
is_static: false # Provide hypothesis about the object staticity to improve the object tracking
tracking_timeout: -1.0 # Maximum tracking time threshold (in seconds) before dropping the tracked object when unseen for this amount of time
tracking_max_dist: -1.0 # Maximum tracking distance threshold (in meters) before dropping the tracked object when unseen for this amount of meters. Only valid for static object
max_box_width_normalized: -1.0 # Maximum allowed width normalized to the image size
min_box_width_normalized: -1.0 # Minimum allowed width normalized to the image size
max_box_height_normalized: -1.0 # Maximum allowed height normalized to the image size
min_box_height_normalized: -1.0 # Minimum allowed height normalized to the image size
max_box_width_meters: -1.0 # Maximum allowed 3D width
min_box_width_meters: -1.0 # Minimum allowed 3D width
max_box_height_meters: -1.0 # Maximum allowed 3D height
min_box_height_meters: -1.0 # Minimum allowed 3D height
object_acceleration_preset: 'DEFAULT' # Object acceleration preset. Possible values: 'DEFAULT', 'LOW', 'MEDIUM', 'HIGH'
max_allowed_acceleration: 100000.0 # If set with a different value from the default [100000], this value takes precedence over the selected preset, allowing for a custom maximum acceleration. Unit is m/s^2.
velocity_smoothing_factor: 0.50 # Control the smoothing of the velocity estimation. Values between 0.0 and 1.0. Default: 0.5
min_velocity_threshold: 0.20 # Threshold to force an object's velocity to zero. Default: 0.2 m/s
prediction_timeout_s: 0.50 # Duration to keep predicting a track's position after occlusion. Default: 0.5 seconds
min_confirmation_time_s: 0.05 # Minimum confirmation time required to validate a track. Default: 0.05 seconds
  • Set the label parameter to the label of the object in your custom ONNX file.
  • Set the model_class_id parameter to the class ID of the object in your custom ONNX file. It is required that this value matches the ID of the class used during the training of the model.
  • Set the enabled parameter to true to enable the detection of this class of objects. This is a dynamic parameter, so it can be changed at runtime.
  • Set the confidence_threshold parameter to the minimum value of the detection confidence of an object. The value must be in the range [0,99] and it can be changed at runtime.
  • Set the is_grounded parameter to provide hypothesis about the object movements (degrees of freedom or DoF) to improve the object tracking. This is a dynamic parameter, so it can be changed at runtime.
  • Set the is_static parameter to provide hypothesis about the object staticity to improve the object tracking. This is a dynamic parameter, so it can be changed at runtime.
  • Set the tracking_timeout parameter to the maximum tracking time threshold (in seconds) before dropping the tracked object when unseen for this amount of time. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the timeout.
  • Set the tracking_max_dist parameter to the maximum tracking distance threshold (in meters) before dropping the tracked object when unseen for this amount of meters. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the distance threshold.
  • Set the max_box_width_normalized parameter to the maximum allowed width normalized to the image size. The value must be in the range [0,1] and it can be changed at runtime. Use -1.0 to disable the width threshold.
  • Set the min_box_width_normalized parameter to the minimum allowed width normalized to the image size. The value must be in the range [0,1] and it can be changed at runtime. Use -1.0 to disable the width threshold.
  • Set the max_box_height_normalized parameter to the maximum allowed height normalized to the image size. The value must be in the range [0,1] and it can be changed at runtime. Use -1.0 to disable the height threshold.
  • Set the min_box_height_normalized parameter to the minimum allowed height normalized to the image size. The value must be in the range [0,1] and it can be changed at runtime. Use -1.0 to disable the height threshold.
  • Set the max_box_width_meters parameter to the maximum allowed 3D width. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the width threshold.
  • Set the min_box_width_meters parameter to the minimum allowed 3D width. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the width threshold.
  • Set the max_box_height_meters parameter to the maximum allowed 3D height. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the height threshold.
  • Set the min_box_height_meters parameter to the minimum allowed 3D height. The value must be in the range [0,500] and it can be changed at runtime. Use -1.0 to disable the height threshold.
  • Set the object_acceleration_preset parameter to the object acceleration preset. The possible values are: DEFAULT, LOW, MEDIUM, HIGH.
  • Set the max_allowed_acceleration parameter to the maximum acceleration of the object. The value must be in the range [0,100000] and it can be changed at runtime. When the value is different from the default [100000.0], this value takes precedence over the selected object_acceleration_preset, allowing for a custom maximum acceleration. The unit is m/s^2. Using a good value for this parameter is important to avoid false positives in the object tracking process.
  • Set the velocity_smoothing_factor parameter to control the smoothing of the velocity estimation. The value must be in the range [0.0, 1.0]; the default is 0.5. Use a high value for static and slow objects so that they do not jitter, and a low value for fast movers so that their velocity stays responsive.
  • Set the min_velocity_threshold parameter to the threshold below which the velocity of an object is forced to zero. The default is 0.2 m/s.
  • Set the prediction_timeout_s parameter to the duration for which the position of a track keeps being predicted after an occlusion. The default is 0.5 s.
  • Set the min_confirmation_time_s parameter to the minimum confirmation time required to validate a track. The default is 0.05 s. Use a higher value for small objects, which produce more false positives.

object_acceleration_preset and max_allowed_acceleration are deprecated since ZED SDK 5.5 and are left at their default value for every class in the template file.

Template File

Use the provided custom_object_detection.yaml template as a reference example. It is preconfigured for models trained on the 80 classes COCO dataset, in the COCO 2017 order (class 0 person to class 79 toothbrush), which is the order used by the YOLO and RF-DETR models trained on COCO.

Starting from v5.5.0 of the ROS 2 Wrapper the per-class defaults of the template are set per object type instead of being identical for all 80 classes: is_grounded is set only for objects that really lie on the floor, is_static only for objects fixed in the world, and the tracking timeout, the 3D box bounds, the velocity settings and the confirmation and prediction times follow the object type.

Launch the ZED Node with Custom Object Detection and Tracking configuration

To launch the ZED node with the custom object detection configuration, use the launch command and set the value of the custom_object_detection_config_path launch argument:

ros2 launch zed_wrapper zed_camera.launch.py camera_model:=<camera_model> custom_object_detection_config_path:='<path_to_custom_object_detection.yaml>'

Replace <camera_model> with the desired camera model (e.g., zedx, zedxm, zedxnano, zed2i, zed2, zedm, zed, or virtual) and <path_to_custom_object_detection.yaml> with the path to your custom object detection configuration file created in the previous step.

The custom_object_detection_config_path launch parameter is optional. If not provided, the ZED node will use the default configuration file custom_object_detection.yaml located in the config folder of the ZED ROS 2 Wrapper package.

Enable the Object Detection processing

You can automatically start the object detection module by setting the object_detection.od_enabled parameter to true in the common_stereo.yaml file. This will enable the object detection when the ZED node starts.

You can also start the object detection manually by calling the service ~/enable_obj_det with the parameter True.

In both cases, you can stop the object detection by calling the service ~/enable_obj_det with the parameter False.

See the services documentation for more info.

The first time you run the ZED node with the custom object detection configuration, the SDK will optimize the model for the GPU used on the host device.

This process may take a long time, depending on the model size and the power of the GPU used. The optimized model will be saved in the /usr/local/zed/resources folder and reused in subsequent runs, which will no longer require the optimization process.

[ZED][INFO] Please wait while the AI model is being optimized for your graphics card
This operation will be run only once and may take a few minutes

Object Detection and Tracking results

The results of the Object Detection and Tracking processing are published using a custom message of type zed_msgs/ObjectsStamped defined in the package zed_msgs.

To visualize the results of the Object Detection processing in RViz 2, the ZedOdDisplay plugin is required. The plugin is available in the zed-ros2-examples GitHub repository and can be installed following the online instructions.

The source code of the plugin is a valid example of how to process the data of the topics of type zed_msgs/ObjectsStamped.

image

Parameters:

  • Topic: Selects the object detection topic to visualize from the list of available topics in the combo box.
  • Depth: The depth of the incoming message queue.
  • History policy: Set the QoS history policy. Keep Last is suggested for performance and compatibility.
  • Reliability Policy: Set the QoS reliability policy. Best Effort is suggested for performance and compatibility.
  • Durability Policy: Set the QoS durability policy. Volatile is suggested for compatibility.
  • Transparency: the transparency level of the structures composing the detected objects.
  • Show skeleton: Not used.
  • Show Labels: enable/disable the visualization of the object label.
  • Show Bounding Boxes: enable/disable the visualization of the bounding boxes of the detected objects.
  • Link Size: the size of the bounding boxes’ corner lines.
  • Joint Radius: the radius of the spheres placed on the corners of the bounding boxes.
  • Label Scale: the scale of the label of the object.

The format of the label of the detected objects is:

<tracking_id>-<label> [<label_id>]

Where:

  • tracking_id is the tracking ID of the detected object, associated by the ZED SDK to the detected object. The tracking ID is unique for each detected object and it is used to identify the object in the tracking process.
  • label is the label of the detected object, corresponding to the value of the parameter label in the configuration file.
  • label_id is the ID of the label of the detected object, corresponding to the value of the parameter model_class_id in the configuration file.
image