Skip to navigation

Recommended Specifications for ZED SDK

Open in ClaudeOpen in ChatGPT

We recommend the following system specifications for developing software with the latest version of the ZED SDK:

PC MinimumPC RecommendedEmbedded Systems
RAM8 GB16 GB4 GB minimum
Graphics CardNVIDIA® RTX GPU *NVIDIA® RTX model with >6 GB VRAMNVIDIA® Jetson™ Orin™ or Jetson™ Thor™
ConnectivityUSB 2.0 **USB 3.0USB 2.0 ** / USB 3.0 / GMSL2
Operating SystemWindows, UbuntuWindows, UbuntuJetson™ Linux (L4T)

* An NVIDIA® GPU with Compute Capabilities >= 7.5 based on Turing or more recent micro-architecture is required.

** With USB 2.0, the maximum supported resolution is VGA at 30 FPS.

Please refer to the ZED SDK release page for the list of supported operating system versions for Windows, Ubuntu, and Jetson™ Linux. The release page also offers installers for NVIDIA® IGX OS (IGX Thor) and, experimentally, for DGX OS on NVIDIA® DGX systems such as the DGX Spark.

On the NVIDIA® Jetson™ Orin™ Nano 4GB, optimizing the NEURAL and NEURAL_PLUS depth models can take a long time and requires large swap files and memory optimizations to complete.

Supported embedded platforms

The ZED SDK is fully supported on both NVIDIA® Jetson™ Orin™ and Jetson™ Thor™ platforms, including:

PlatformNVIDIA® Jetson™ module
ZED Box MiniOrin™
ZED BoxOrin™
ZED Box 2Orin™
ZED Box 2 Max - T4000Thor™
ZED Box 2 Max - T5000Thor™
Partners’ carrier boards and ECUsOrin™, Thor™

When using a partner’s carrier board or ECU, make sure the GMSL2 driver provided by the manufacturer matches your Jetson™ Linux (L4T) version and the ZED SDK release you install.

Minimum ZED SDK version per camera

Each camera model was introduced in a specific version of the ZED SDK. Using a camera requires that version or a newer one:

Camera modelMinimum ZED SDK version
ZED Miniv2.3
ZED 2iv3.5
ZED Xv4.0
ZED X Miniv4.0
ZED X One GSv4.2
ZED X One 4Kv4.2
ZED X One Sv4.2
ZED X Nanov5.3
ZED X One Corev5.5

We always recommend installing the latest ZED SDK release, which supports every camera listed above.

NVIDIA® Driver Requirements

We recommend using the latest NVIDIA® drivers available for your desktop/laptop GPU.

We recommend you follow the official NVIDIA® Driver Download page instructions to get the latest drivers for your GPU.

This is not required for NVIDIA® Jetson™ embedded systems as the NVIDIA® drivers are already included in the Jetson™ Linux distribution.

To install the open kernel module flavor:

sudo apt-get install -y nvidia-open

To install the proprietary kernel module flavor:

sudo apt-get install -y cuda-drivers

We recommend you follow the official NVIDIA® Driver Installation Guide for Ubuntu for more details.