Skip to navigation

Using Geo Tracking with ROS 2

Open in ClaudeOpen in ChatGPT

In this tutorial, you will learn how to leverage georeferential information from a GNSS sensor to improve the overall outdoor performance of the Positional Tracking module.

The ZED ROS 2 Wrapper is compatible with any GNSS sensor provided with a ROS 2 driver that publishes Latitude and Longitude data with a message of type sensor_msgs::msg::NavSatFix on the topic defined by the parameter gnss_fusion.gnss_fix_topic (/fix in the default common_stereo.yaml). This can be the driver provided by your receiver vendor, a generic NMEA driver such as nmea_navsat_driver, or a gpsd client node such as the one of the gps_umd package.

If you are new to GNSS, see the GNSS Overview to learn about GNSS and RTK and how to choose and install a receiver, and Setting up GNSS / RTK on Linux to configure it.

Enable GNSS Fusion

GNSS Fusion can be started automatically when the ZED Wrapper node starts by setting the parameter gnss_fusion.gnss_fusion_enabled to true in the file common_stereo.yaml.

GNSS Fusion cannot be combined with loop closure: when it is enabled, the node disables the Area Memory (pos_tracking.area_memory) and ignores the area file.

With ZED SDK >= 5.6 and pos_tracking.pos_tracking_mode: 'GEN_3', GNSS Fusion also runs without depth (depth.depth_mode: 'NONE'), which saves the GPU time of the depth computation. With older ZED SDK versions, GNSS Fusion requires a depth mode and the node disables it, with a warning, when depth.depth_mode is NONE.

When the Geo Tracking module is active, the ZED ROS 2 Wrapper nodes wait for the first valid GNSS Datum on the subscribed topic before starting the processing:

[INFO] [1681308875.997297634] [zed2i.zed_node]: *** Positional Tracking with GNSS fusion ***
[INFO] [1681308875.997340244] [zed2i.zed_node]: * Waiting for the first valid GNSS fix...

GNSS Fusion results

When the Geo Tracking module is enabled, the GNSS datum is automatically fused with the Positional Tracking information to provide a precise camera pose in the map frame on the topic ~/pose. The messages on the topic ~/pose/filtered contain the GNSS-fused odometry information, to be used with external Kalman Filters.

The ZED ROS 2 Wrapper also publishes the pose of the robot in Earth coordinates on the topic ~/geo_pose of type geographic_msgs::msg::GeoPoseStamped.