Skip to navigation

Troubleshooting

Open in ClaudeOpen in ChatGPT

This troubleshooting guide provides solutions to common issues that may arise when using the ZED X One camera. If you encounter any problems, please refer to the sections below for potential fixes.

This page covers the GMSL2 ZED X One models (ZED X One GS, ZED X One 4K and ZED X One S). If you are using a ZED X One Core with a ZED Link MIPI capture card, the hardware-configuration advice below does not apply: see the MIPI Troubleshooting page instead.

The camera is not detected

GMSL2 cameras have lower flexibility compared to USB cameras. Any modification in the hardware configuration, such as plugging or unplugging a camera, or changing the camera order, requires either rebooting the Jetson, or restarting the installed daemon with the following command:

sudo systemctl restart zed_x_daemon

If you are using a custom carrier board, or a partner’s ECU, please make sure that the custom driver provides the zed_x_daemon service. If not, every hardware modification will require a reboot of the Jetson device.


Blurry images after system update

After a system update, if you experience blurry images from the GMSL2 camera, it may be caused by the overwriting of a patched library used by the ZED Link driver.

This issue is fixed in ZED X Driver 1.4.1: first update the driver to the latest version. The manual procedure below is only needed with older drivers.

To fix this issue, please follow this procedure to manually restore the patched library:

  1. Download the latest ZED Link driver package for your device from the ZED X Drivers download page.

  2. Extract the downloaded .deb package and copy the patched library to the correct location:

    ar x stereolabs-zed<model>_<version>-<deser>-<l4t_version>_arm64.deb
    tar xvf data.tar.xz
    sudo cp ./tmp/R<l4t_version>/libnvisppg.so /usr/lib/aarch64-linux-gnu/tegra/libnvisppg.so

    Replace stereolabs-zed<model>_<version>-<deser>-<l4t_version>_arm64.deb with the actual filename of the downloaded package.

    Replace <l4t_version> with your current L4T version (for example, 36.4.3, which gives the ./tmp/R36.4.3/ folder).

  3. Reboot the Jetson device:

    sudo reboot

After following these steps, the GMSL2 camera should function correctly with clear images.


Contact Support

If you are unable to resolve your issue, ask for help on the StereoLabs community forum or contact support@stereolabs.com.

If the device is defective, see Returns and RMA to request a replacement under warranty.