Building ZED Live Link
Deprecation Information
From the 4.1 version on, the Live Link senders (sender-mono and sender-multi-camera in the ZED Live Link repository) can be built with CMake like any other ZED SDK sample, without the Unreal Engine source files. Refer to the samples documentation if you need guidance to build them. The instructions below only apply to versions before 4.1.
Before 4.1
In the Live Link for UE5 page, we explained how to animate an avatar on Unreal using the pre-compiled ZED Live Link sample executable.
A pre-built ZEDLiveLink sender for the current SDK version is located in zed-livelink-fusion (or mono)/Releases/your system/.
However, you might prefer to directly manipulate the ZED Live Link sample code and make some modifications to it. To do so, you must compile the ZED Live Link sample from source.
- First, download the latest version of the ZED SDK on stereolabs.com
- For more information, read the ZED Documentation and API documentation
To compile the tool from source, you will require a source build of Unreal Engine.
Download the Engine
To gain access to the UE engine code, please follow the steps below:
- Create an account at GitHub: Sign up
- Create an account at Epic Games: Sign up
- Log in to your Epic Games account and associate your GitHub account in the settings by entering your username into the GitHub account field.
- Log in to your GitHub account and accept the Epic team invitation* (can take a few seconds to appear).
- Download or clone the UE5 engine code.
The link above will result in a 404 error if your GitHub account is not linked to an Epic Games one. Make sure to follow all the instructions above.
*If the invitation isn’t sent, clicking on the following link seems to trigger it: Unreal Group.
Build for Windows
- Inside the Engine root directory, run Setup.bat. This will check all the project dependencies and update them as needed.
- Clone the ZED Live Link repository inside
<Engine Install Folder>\Engine\Source\Programs\. - Run GenerateProjectFiles.bat in the Unreal Engine root directory to create project files for the Engine.
- Load the project into Visual Studio by double-clicking on the
UE5.slnfile, in the Unreal Engine root directory, then right click on the ZEDLiveLink target and select Build.
- You will find the
ZEDLiveLinktarget (and its counterpartZEDLiveLinkFusion) underSolution UE5/Programs/LiveLink/in the Solution Explorer.
- The binaries will be placed in
<Engine Install Folder>\Engine\Binaries\Win64\ZEDLiveLink\and<Engine Install Folder>\Engine\Binaries\Win64\ZEDLiveLinkFusion\.
Build for Linux
-
Go inside the Engine root directory and run Setup.sh from the terminal. This will check all the project dependencies and update them as needed.
-
Clone the ZED Live Link repository inside
<Engine Install Folder>/Engine/Source/Programs. -
In the Engine root directory, run GenerateProjectFiles.sh.
-
Run make to build the Engine.
-
Go to
<Engine Install Folder>/Engine/Build/BatchFilesand open a terminal. -
Build the sample with the following command.
- For the mono camera sample:
- For the fusion sample:
-
The binaries will be placed in
<Engine Install Folder>/Engine/Binaries/Linux/ZEDLiveLink/for the mono camera sample and in<Engine Install Folder>/Engine/Binaries/Linux/ZEDLiveLinkFusion/for the fusion/multi-cameras sample.