Skip to navigation

Flash your ZED Box Mini

Open in ClaudeOpen in ChatGPT

Should I flash my ZED Box Mini?

The ZED Box Mini is shipped with a pre-configured operating system and drivers optimized for its hardware.

Flashing (resetting or upgrading the device firmware) is only recommended if you need to:

  • Install a different OS or JetPack version,
  • Recover from a corrupted system,
  • Resolve issues preventing the device from booting or functioning properly.

Flashing will erase all data and custom configurations on your ZED Box Mini. Proceed only if you are familiar with the process or have been instructed by support. For most users, flashing should be a last resort.

Flashing Procedure

The NVIDIA® SDK Manager does not support automatic flashing of the Jetson modules installed in the ZED Box. Therefore, you must manually flash the board using NVIDIA’s BSP for the desired JetPack version.

Force the ZED Box Mini in Recovery mode

It is not required to open the ZED Box Mini to force it into Recovery mode. Opening the box will void the warranty

  • First method:

    This is applicable only if your device can normally boot.

    Open a terminal console (Ctrl+Alt+t) and enter the command

    sudo reboot --force forced-recovery
  • Second method:

    1. Connect the power
    2. Use a pin to push the RCV button
    3. While keeping the RCV button pushed, use a pin to push the RST button

When the ZED Box Mini boots in Force Recovery mode, the power LED stays OFF.

Check that the ZED Box Mini restarted in Force Recovery mode

Connect a Type-A/MicroUSB cable to an Ubuntu host PC and to the OTG port of the ZED Box Mini.

Open a terminal console (Ctrl+Alt+t).

You can verify that the ZED Box Mini correctly started in “Recovery Mode” by entering this command:

lsusb -d '0955:'
  • NVIDIA® Jetson™ Orin Nano 4 GB: an NVIDIA® device with VID:PID 0955:7623 should be listed. e.g. Bus xxx Device yyy: ID 0955:7623 NVIDIA Corp. APX
  • NVIDIA® Jetson™ Orin Nano 8 GB: an NVIDIA® device with VID:PID 0955:7523 should be listed. e.g. Bus xxx Device yyy: ID 0955:7523 NVIDIA Corp. APX
  • NVIDIA® Jetson™ Orin NX 8 GB: an NVIDIA® device with VID:PID 0955:7423 should be listed. e.g. Bus xxx Device yyy: ID 0955:7423 NVIDIA Corp. APX
  • NVIDIA® Jetson™ Orin NX 16 GB: an NVIDIA® device with VID:PID 0955:7323 should be listed. e.g. Bus xxx Device yyy: ID 0955:7323 NVIDIA Corp. APX

If an NVIDIA® device with VID:PID 0955:7020 and type NVIDIA Corp. L4T (Linux for Tegra) running on Tegra is listed, then your ZED Box Mini has not rebooted in Force Recovery mode. You must retry the procedure.

Flash the ZED Box Mini

Requirements:

  • use a host PC running Ubuntu 20.04 or Ubuntu 22.04.

Do not use virtual machines or WSL2 to run Ubuntu when flashing the ZED Box Mini. If you do not have a PC running Ubuntu ready, please consider using a Live USB Key instead:

On the host PC:

  1. Open a terminal console from an empty folder of your choice.

    For example:

    mkdir -p ~/zedbox_flash
    cd ~/zedbox_flash
  2. Install QEMU to build the image:

    sudo apt install qemu-user-static
  3. Ensure that you previously booted the ZED Box Mini in “Recovery mode”.

  4. Download the flash script for the NVIDIA® JetPack version you want to install:

  5. Flash the ZED Box Mini:

    • Ensure you have at least 80GB of free space on your working hard drive.

    • Use the following commands to flash the ZED Box Mini:

      chmod +x <script_name>.sh
      BSP_ROOT=./stereolabs_bsp/ ./<script_name>.sh

      Replace <script_name> with the name of the downloaded script, e.g., zedbox_mini_usb_flash_6.2_gpio.

    • All necessary files will be downloaded in the folder $BSP_ROOT. The script will create this folder if it does not exist and will ask you to log in as root.

  6. Wait for the operation to complete. You will see the following output if the flash is successful:

    [...]
    Flash is successful
    Reboot device
    Cleaning up...
    Log is saved to Linux_for_Tegra/initrdlog/flash_<date_time>.log
    FLASH SUCCESS

If you encounter any problems during this procedure, please consult the troubleshooting guide.

Post-Flash operations

After flashing your device, follow these steps to install the necessary NVIDIA® and StereoLabs packages to ensure your ZED camera works correctly.

  1. Boot and Login:

    Power on the device and log in with your credentials.

    The new default credentials of your ZED Box are:

    • username: user
    • password: admin
  2. Check the OS Version:

    Follow this support guide to determine the version of the operating system installed on your device.

  3. Connect to the Internet:

    Connect your device to the internet using an Ethernet cable (WiFi may not yet be available, depending on the script you used to flash the device).

  4. Open a Terminal:

    Press Ctrl+Alt+T to open a terminal window.

  5. Update the APT cache:

    Run the following commands to update the APT cache:

    sudo apt update

    Do not run the command sudo apt upgrade before performing the next steps!

  6. Install NVIDIA® JetPack Packages:

    Run the following command to install the NVIDIA® JetPack packages, which include the required Jetson™ drivers, CUDA, and all necessary NVIDIA® libraries:

    sudo apt install nvidia-jetpack
  7. Install the ZED Box Mini GMSL2 driver (for ZED X and ZED X One cameras):

    Download and install the appropriate drivers from the driver web page:

    cd ~/Downloads
    sudo dpkg -i stereolabs-zedbox-mini_<ver_info>_arm64.deb
  8. Hold the kernel packages to not upgrade them and invalidate the setup:

    • Create a hold-zedbox-kernel.sh script file with the following content:

      • nano hold-zedbox-kernel.sh

        Fill the file with this script:

        #!/bin/bash
        #
        # hold-zedbox-kernel.sh
        #
        # Prevents `apt upgrade` from installing nvidia-l4t-kernel versions
        # that are incompatible with the stereolabs-zedbox-mini package.
        #
        # The stereolabs-zedbox-mini package requires an nvidia-l4t-kernel version within the
        # range supported by the L4T release it was built for. For example, the
        # L4T 36.4 (JetPack 6.2) driver requires:
        # >= 5.15.148-tegra-36.4.0-20240912212859
        # <= 5.15.148-tegra-36.4.4-20250616085344
        # The range differs for other JetPack versions. Check your driver with:
        # dpkg-query -W -f='${Package}: ${Depends}\n' stereolabs-zedbox-mini
        #
        # This script holds all NVIDIA L4T kernel-related packages at their
        # currently installed versions so they won't be upgraded past the
        # compatible range.
        #
        # The package list is discovered dynamically from dpkg rather than
        # hardcoded. L4T/JetPack images ship these packages
        # under names that vary between releases (sometimes version-suffixed, e.g.
        # nvidia-l4t-kernel-5.15.148, sometimes via a different meta-package), so a
        # fixed list often matches nothing and every entry is skipped.
        #
        # Usage:
        # sudo ./hold-zedbox-kernel.sh hold # Hold the packages (default)
        # sudo ./hold-zedbox-kernel.sh unhold # Release the hold
        # sudo ./hold-zedbox-kernel.sh status # Show current hold status
        set -euo pipefail
        # Regex matching the L4T kernel package family we want to hold. This is
        # anchored at the start and allows arbitrary suffixes (e.g. -headers,
        # version suffixes) so it catches naming variants across L4T releases.
        PKG_REGEX='^nvidia-l4t-(kernel|rt-kernel|display-kernel|bootloader|xusb-firmware|init)'
        # --- helpers ---------------------------------------------------------------
        require_root() {
        if [[ $EUID -ne 0 ]]; then
        echo "Error: this script must be run with sudo or as root." >&2
        exit 1
        fi
        }
        is_installed() {
        # Returns 0 if the package is installed (status "ii" or "hi"), 1 otherwise.
        dpkg-query -W -f='${db:Status-Abbrev}\n' "$1" 2>/dev/null | grep -qE '^.i'
        }
        # Discover installed L4T kernel-related packages by pattern. Populates the
        # global PACKAGES array. Exits with an error if nothing matches, since that
        # means the regex (or the image) needs to be inspected manually.
        discover_packages() {
        mapfile -t PACKAGES < <(
        dpkg-query -W -f='${Package} ${db:Status-Abbrev}\n' 2>/dev/null \
        | awk '$2 ~ /^.i/ {print $1}' \
        | grep -E "$PKG_REGEX" \
        | sort -u
        )
        if [[ ${#PACKAGES[@]} -eq 0 ]]; then
        echo "Error: no installed nvidia-l4t kernel packages matched." >&2
        echo "Inspect manually with:" >&2
        echo " dpkg -l | grep -i nvidia-l4t-kernel" >&2
        echo " dpkg -l | grep -i nvidia-l4t | grep -iE 'kernel|boot|init|firmware'" >&2
        echo "Then adjust PKG_REGEX in this script if the names differ." >&2
        exit 1
        fi
        }
        hold_packages() {
        require_root
        discover_packages
        echo "Holding NVIDIA L4T kernel packages at their current versions..."
        echo
        local held=0
        for pkg in "${PACKAGES[@]}"; do
        local ver
        ver=$(dpkg-query -W -f='${Version}' "$pkg" 2>/dev/null || echo "unknown")
        apt-mark hold "$pkg" >/dev/null
        printf " [HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        held=$((held + 1))
        done
        echo
        echo "Done. Held: $held"
        echo
        echo "These packages will now be ignored by 'apt upgrade'."
        echo "Use 'apt-mark showhold' to verify, or run this script with 'status'."
        }
        unhold_packages() {
        require_root
        discover_packages
        echo "Releasing hold on NVIDIA L4T kernel packages..."
        echo
        local released=0
        local all_holds
        all_holds=$(apt-mark showhold)
        for pkg in "${PACKAGES[@]}"; do
        if echo "$all_holds" | grep -qxF "$pkg"; then
        apt-mark unhold "$pkg" >/dev/null
        printf " [UNHELD] %s\n" "$pkg"
        released=$((released + 1))
        else
        printf " [SKIPPED] %s (was not held)\n" "$pkg"
        fi
        done
        echo
        echo "Done. Released: $released"
        echo
        echo "WARNING: these packages may now be upgraded by 'apt upgrade',"
        echo "which can break stereolabs-zedbox-mini if an incompatible kernel"
        echo "version is installed."
        }
        show_status() {
        discover_packages
        echo "Current hold status for NVIDIA L4T kernel packages:"
        echo
        local all_holds
        all_holds=$(apt-mark showhold)
        for pkg in "${PACKAGES[@]}"; do
        local ver
        ver=$(dpkg-query -W -f='${Version}' "$pkg" 2>/dev/null)
        if echo "$all_holds" | grep -qxF "$pkg"; then
        printf " [HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        else
        printf " [NOT HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        fi
        done
        echo
        echo "stereolabs-zedbox-mini status:"
        if is_installed "stereolabs-zedbox-mini"; then
        local zedver
        zedver=$(dpkg-query -W -f='${Version}' "stereolabs-zedbox-mini" 2>/dev/null)
        echo " Installed (version: $zedver)"
        else
        echo " Not installed"
        fi
        }
        usage() {
        cat <<EOF
        Usage: sudo $0 [hold|unhold|status]
        hold Hold NVIDIA L4T kernel packages at their current versions (default)
        unhold Release the hold so packages can be upgraded again
        status Show whether each package is currently held
        Why this is needed:
        stereolabs-zedbox-mini depends on nvidia-l4t-kernel within a specific
        version range. Newer kernels from NVIDIA's apt repo fall outside this
        range and break the package. Holding the kernel keeps 'apt upgrade'
        from touching it.
        Note:
        The package list is discovered dynamically from dpkg using PKG_REGEX,
        so version-suffixed or renamed kernel packages are matched automatically.
        Holding only prevents FUTURE upgrades; it cannot roll back a kernel that
        has already been installed outside the compatible range.
        EOF
        }
        # --- main ------------------------------------------------------------------
        cmd="${1:-hold}"
        case "$cmd" in
        hold) hold_packages ;;
        unhold) unhold_packages ;;
        status) show_status ;;
        -h|--help|help) usage ;;
        *)
        echo "Error: unknown command '$cmd'" >&2
        echo
        usage
        exit 1
        ;;
        esac
    • Make the script executable:

      chmod +x hold-zedbox-kernel.sh

    • Run the script:

      sudo ./hold-zedbox-kernel.sh

    • Verify the result:

      sudo ./hold-zedbox-kernel.sh status

      All the listed nvidia-l4t-* kernel packages should be reported as [HELD] nvidia-l4t-* (version: xx.y.z-dddddddddddddd).

  9. Download and install the ZED SDK:

    • Visit the StereoLabs website and download the ZED SDK for Jetson that matches your installed JetPack/L4T version.

    • Navigate to your Downloads directory and run the installer:

      cd ~/Downloads
      chmod +x ZED_SDK_Tegra_L4T<l4t_version>_v<x.y.z>.zstd.run
      ./ZED_SDK_Tegra_L4T<l4t_version>_v<x.y.z>.zstd.run
  10. Reboot:

    Restart your device to apply all changes:

    sudo reboot
  11. Enjoy Your Device:

    Your device is now ready for use with the ZED cameras.