Skip to navigation

Tutorial - Global Localization

Open in ClaudeOpen in ChatGPT

This tutorial shows how to use the Global Localization (GNSS Fusion) API to fuse GNSS coordinates with the camera’s visual-inertial odometry, in order to compute the camera’s global position (latitude, longitude, altitude) using the Fusion API. To keep this tutorial self-contained and easy to run without any external hardware, the GNSS data is randomly generated rather than read from a real GNSS receiver. We assume that you have followed the Positional Tracking tutorial before.

This module requires a stereo camera equipped with an inertial sensor (IMU), such as the ZED 2/2i, ZED Mini, ZED X, ZED X Mini, ZED X Nano. The original ZED (no built-in IMU) is not supported.

Getting Started

Code Overview

Open the camera and enable positional tracking

As in the previous tutorials, we create, configure and open the ZED. Two positional tracking parameters are mandatory here: enable_imu_fusion (to get the gravity direction from the IMU) and set_gravity_as_origin (to align the camera and GNSS reference frames).

// Open camera
sl::InitParameters init_params;
init_params.depth_mode = sl::DEPTH_MODE::NEURAL;
init_params.coordinate_system = sl::COORDINATE_SYSTEM::IMAGE;
init_params.coordinate_units = sl::UNIT::METER;
init_params.camera_resolution = sl::RESOLUTION::AUTO;
init_params.camera_fps = 60;
sl::Camera zed;
sl::ERROR_CODE camera_open_error = zed.open(init_params);
if (camera_open_error > sl::ERROR_CODE::SUCCESS) {
std::cerr << "[ZED][ERROR] Can't open ZED camera" << std::endl;
return EXIT_FAILURE;
}
// Enable positional tracking
sl::PositionalTrackingParameters ptp;
ptp.initial_world_transform = sl::Transform::identity();
ptp.enable_imu_fusion = true; // Enable IMU (for having the gravity direction)
ptp.set_gravity_as_origin = true; // Set gravity as origin for allowing GNSS to Camera initialization
auto positional_init = zed.enablePositionalTracking(ptp);
if (positional_init > sl::ERROR_CODE::SUCCESS) {
std::cerr << "[ZED][ERROR] Can't start tracking of camera" << std::endl;
return EXIT_FAILURE;
}

Publish the camera for Fusion

The Fusion module works on a Publish/Subscribe pattern: the camera publishes its data, and a Fusion object subscribes to it. Here, camera and Fusion run in the same process, communicating over shared memory.

// Enable camera publishing for fusion
sl::CommunicationParameters communication_parameters;
communication_parameters.setForSharedMemory();
zed.startPublishing(communication_parameters);
// Run a first grab to start sending data
while (zed.grab() > sl::ERROR_CODE::SUCCESS)
;

Set up Fusion and subscribe the camera

We create the Fusion object, initialize it, enable its own positional tracking (with GNSS fusion), and subscribe our camera to it using its serial number as an identifier.

// Create fusion object
sl::InitFusionParameters init_multi_cam_parameters;
init_multi_cam_parameters.coordinate_units = sl::UNIT::METER;
init_multi_cam_parameters.coordinate_system = sl::COORDINATE_SYSTEM::IMAGE;
init_multi_cam_parameters.output_performance_metrics = true;
init_multi_cam_parameters.verbose = true;
sl::Fusion fusion;
sl::FUSION_ERROR_CODE fusion_init_code = fusion.init(init_multi_cam_parameters);
if (fusion_init_code != sl::FUSION_ERROR_CODE::SUCCESS) {
std::cerr << "[Fusion][ERROR] Failed to initialize fusion, error: " << fusion_init_code << std::endl;
return EXIT_FAILURE;
}
// Subscribe to camera
sl::CameraIdentifier uuid(zed.getCameraInformation().serial_number);
fusion.subscribe(uuid, communication_parameters, sl::Transform::identity());
// Enable positional tracking, with GNSS fusion
sl::PositionalTrackingFusionParameters ptfp;
ptfp.enable_GNSS_fusion = true;
fusion.enablePositionalTracking(ptfp);

The python snippet above calls enable_positionnal_tracking (with the extra “n”): this is the actual name exposed by the Fusion Python bindings.

Ingest GNSS data and retrieve the fused position

At each grab(), we get the camera-only pose, generate a fake GNSS position and ingest it into fusion, then call fusion.process() to retrieve both the fused camera pose and the geographic position (latitude, longitude, altitude) once the GNSS-to-camera alignment has converged.

unsigned number_detection = 0;
while (number_detection < 200) {
// Grab camera
if (zed.grab() <= sl::ERROR_CODE::SUCCESS) {
sl::Pose zed_pose;
zed.getPosition(zed_pose, sl::REFERENCE_FRAME::WORLD);
}
// Ingest (fake) GNSS data, timestamped with the current camera timestamp
sl::GNSSData input_gnss = getGNSSData();
input_gnss.ts = zed.getTimestamp(sl::TIME_REFERENCE::IMAGE);
if (input_gnss.ts != sl::Timestamp(0))
fusion.ingestGNSSData(input_gnss);
// Process fusion
if (fusion.process() == sl::FUSION_ERROR_CODE::SUCCESS) {
// Fused camera pose
sl::Pose fused_position;
sl::POSITIONAL_TRACKING_STATE current_state = fusion.getPosition(fused_position);
// Global position (GNSS coordinate system)
sl::GeoPose current_geopose;
sl::GNSS_FUSION_STATUS current_geopose_status = fusion.getGeoPose(current_geopose);
if (current_geopose_status == sl::GNSS_FUSION_STATUS::OK) {
number_detection++;
double latitude, longitude, altitude;
current_geopose.latlng_coordinates.getCoordinates(latitude, longitude, altitude, false);
std::cout << "latitude = " << latitude << ", longitude = " << longitude << ", altitude = " << altitude << std::endl;
}
// Otherwise, the GNSS-to-ZED coordinate system alignment hasn't converged yet:
// it is an optimization problem that fits the ZED computed path to the GNSS computed path,
// so keep moving the camera until it converges.
}
}

Because this tutorial uses synthetic GNSS data, only the fusion mechanics are demonstrated. With a real GNSS receiver, you must provide the full GNSSData (coordinates, timestamp, position covariance, latitude/longitude/altitude standard deviation) for accurate results. See Using GNSS Data in Your Application.

Close Fusion and the camera

fusion.close();
zed.close();

For more information on the Fusion workflow, coordinate frames and calibration, read the Global Localization module documentation.