Skip to navigation

GStreamer - ZED X One Camera Source

Open in ClaudeOpen in ChatGPT

The GStreamer element ZED X One Camera Source, zedxonesrc, injects the monocular color stream of a ZED X One camera into a GStreamer pipeline.

Properties

zedxonesrc is built and installed only on NVIDIA® Jetson™ platforms (L4T 35.3/35.4 or L4T 36.3 and newer), because the ZED X One cameras are connected through a GMSL2 capture card.

The following listing is the output of gst-inspect-1.0 zedxonesrc:

async-grab-camera-recovery: Async Grab Camera Recovery
flags: readable, writable
Boolean. Default: false
blocksize : Size in bytes to read per buffer (-1 = default)
flags: readable, writable
Unsigned Integer. Range: 0 - 4294967295 Default: 4096
camera-flip : Mirror image vertically if camera is flipped
flags: readable, writable
Boolean. Default: false
camera-fps : Camera frame rate
flags: readable, writable
Enum "GstZedXOneSrcFPS" Default: 30, "30 FPS"
(120): 120 FPS - Only with SVGA. Not with ZED X One 4K
(60): 60 FPS - Not available with 4K mode
(30): 30 FPS - Available with all the resolutions
(15): 15 FPS - Available with all the resolutions
camera-id : Select camera from cameraID
flags: readable, writable
Integer. Range: -1 - 255 Default: -1
camera-resolution : Camera Resolution
flags: readable, writable
Enum "GstZedXOneSrcResol" Default: 2, "HD1200"
(4): 4K - 3840x2160 (only ZED X One 4K)
(3): QHDPLUS - 3200x1800 (only ZED X One 4K)
(2): HD1200 - 1920x1200
(1): HD1080 - 1920x1080
(0): SVGA - 960x600 (only ZED X One GS)
camera-sn : Select camera from the serial number
flags: readable, writable
Integer64. Range: 0 - 999999999 Default: 0
camera-timeout : Connection opening timeout in seconds
flags: readable, writable
Float. Range: 0.5 - 86400 Default: 5
coordinate-system : SDK Coordinate System
flags: readable, writable
Enum "GstZedXOneSrcCoordSys" Default: 0, "IMAGE"
(0): IMAGE - Standard image (0,0) at top left corner
(1): LEFT_HANDED_Y_UP - Left handed, Y up and Z forward
(2): RIGHT_HANDED_Y_UP - Right handed, Y up and Z backward
(3): RIGHT_HANDED_Z_UP - Right handed, Z up and Y forward
(4): LEFT_HANDED_Z_UP - Left handed, Z up and Y forward
(5): RIGHT_HANDED_Z_UP_X_FWD - Right handed, Z up and X forward
coordinate-units : SDK Coordinate Units
flags: readable, writable
Enum "GstZedXOneSrcUnit" Default: 0, "MILLIMETER"
(0): MILLIMETER - Millimeter
(1): CENTIMETER - Centimeter
(2): METER - Meter
(3): INCH - Inch
(4): FOOT - Foot
ctrl-analog-gain : Camera control: Analog Gain value
flags: readable, writable
Integer. Range: 1000 - 30000 Default: 30000
ctrl-auto-analog-gain: Enable Automatic Analog Gain
flags: readable, writable
Boolean. Default: true
ctrl-auto-analog-gain-range-max: Maximum Analog Gain for the automatic analog gain setting
flags: readable, writable
Integer. Range: 1000 - 30000 Default: 30000
ctrl-auto-analog-gain-range-min: Minimum Analog Gain for the automatic analog gain setting
flags: readable, writable
Integer. Range: 1000 - 30000 Default: 1000
ctrl-auto-digital-gain: Enable Automatic Digital Gain
flags: readable, writable
Boolean. Default: true
ctrl-auto-digital-gain-range-max: Maximum Digital Gain for the automatic digital gain setting
flags: readable, writable
Integer. Range: 1 - 256 Default: 256
ctrl-auto-digital-gain-range-min: Minimum Digital Gain for the automatic digital gain setting
flags: readable, writable
Integer. Range: 1 - 256 Default: 1
ctrl-auto-exposure : Enable Automatic Exposure
flags: readable, writable
Boolean. Default: true
ctrl-auto-exposure-range-max: Maximum exposure time in microseconds for the automatic exposure setting
flags: readable, writable
Integer. Range: 28 - 66666 Default: 66666
ctrl-auto-exposure-range-min: Minimum exposure time in microseconds for the automatic exposure setting
flags: readable, writable
Integer. Range: 28 - 66666 Default: 1024
ctrl-denoising : Denoising factor
flags: readable, writable
Integer. Range: 0 - 100 Default: 50
ctrl-digital-gain : Digital Gain value
flags: readable, writable
Integer. Range: 1 - 256 Default: 3
ctrl-exposure-compensation: Exposure Compensation
flags: readable, writable
Integer. Range: 0 - 100 Default: 50
ctrl-exposure-time : Exposure time in microseconds
flags: readable, writable
Integer. Range: 28 - 66666 Default: 10000
ctrl-gamma : Image gamma
flags: readable, writable
Integer. Range: 1 - 9 Default: 2
ctrl-saturation : Image saturation
flags: readable, writable
Integer. Range: 0 - 8 Default: 4
ctrl-sharpness : Image sharpness
flags: readable, writable
Integer. Range: 0 - 8 Default: 1
ctrl-whitebalance-auto: Image automatic white balance
flags: readable, writable
Boolean. Default: true
ctrl-whitebalance-temperature: Image white balance temperature
flags: readable, writable
Integer. Range: 2800 - 6500 Default: 4200
do-timestamp : Apply current stream time to buffers
flags: readable, writable
Boolean. Default: false
enable-hdr : Enable HDR if supported by resolution and frame rate.
flags: readable, writable
Boolean. Default: false
input-stream-ip : Specify IP address when using streaming input
flags: readable, writable
String. Default: ""
input-stream-port : Specify port when using streaming input
flags: readable, writable
Integer. Range: 1 - 65535 Default: 30000
name : The name of the object
flags: readable, writable, 0x2000
String. Default: "zedxonesrc0"
num-buffers : Number of buffers to output before sending EOS (-1 = unlimited)
flags: readable, writable
Integer. Range: -1 - 2147483647 Default: -1
opencv-calibration-file: Optional OpenCV Calibration File
flags: readable, writable
String. Default: ""
optional-settings-path: Optional Settings Path
flags: readable, writable
String. Default: ""
output-rectified-image: Enable image rectification (disable for custom optics without calibration)
flags: readable, writable
Boolean. Default: true
parent : The parent of the object
flags: readable, writable, 0x2000
Object of type "GstObject"
sdk-verbose-log-file: SDK Verbose Log File
flags: readable, writable
String. Default: ""
stream-type : Image stream type
flags: readable, writable
Enum "GstZedXOneSrcStreamType" Default: -1, "Auto [prefer NV12 zero-copy]"
(-1): Auto [prefer NV12 zero-copy] - Auto-negotiate format based on downstream (prefer NV12 zero-copy)
(0): Image [BGRA] - 8 bits- 4 channels image
svo-file-path : Input from SVO file
flags: readable, writable
String. Default: ""
svo-real-time-mode : SVO Real Time Mode
flags: readable, writable
Boolean. Default: false
svo-recording-compression: Compression mode for SVO recording
flags: readable, writable
Enum "GstZedXOneSrcSvoCompression" Default: 2, "H265"
(0): LOSSLESS - Lossless (PNG/ZSTD, CPU)
(1): H264 - H264 (GPU)
(2): H265 - H265/HEVC (GPU)
(3): H264_LOSSLESS - H264 Lossless (GPU)
(4): H265_LOSSLESS - H265 Lossless (GPU)
svo-recording-enable: Start/stop SVO recording at runtime (requires svo-recording-filename to be set)
flags: readable, writable
Boolean. Default: false
svo-recording-filename: Output filename for SVO recording (.svo2 extension recommended)
flags: readable, writable
String. Default: ""
typefind : Run typefind before negotiating (deprecated, non-functional)
flags: readable, writable, deprecated
Boolean. Default: false
verbose-level : ZED SDK Verbose level
flags: readable, writable
Integer. Range: 0 - 999 Default: 1

Zero-copy NV12 stream type

When the plugin is built against ZED SDK v5.2 or newer, stream-type exposes an additional value (1), Raw NV12 zero-copy [NV12], that pushes NV12 buffers in memory:NVMM without any CPU copy, for direct consumption by the Jetson hardware encoders.

The default value (-1), Auto [prefer NV12 zero-copy], negotiates the format with the downstream element and selects the zero-copy NV12 path when it is available, falling back to Image [BGRA] otherwise.

Example pipelines

Display the color stream on the screen with FPS information

This simple pipeline starts the ZED X One grabbing using the default parameters of the zedxonesrc element and automatically converts (autovideoconvert) the frames to the correct format for the fpsdisplaysink element in order to be displayed on the screen with FPS information.

gst-launch-1.0 zedxonesrc ! queue ! autovideoconvert ! queue ! fpsdisplaysink

The queue element is used to decouple frames in a different queue thread, useful for data synchronization for more complex pipelines.

When using the ZED X One 4K model, you can leverage the full 4K resolution (3840x2160) by selecting camera-resolution=4:

gst-launch-1.0 zedxonesrc camera-resolution=4 camera-fps=15 ! queue ! autovideoconvert ! queue ! fpsdisplaysink

The intermediate QHD+ resolution (3200x1800), also exclusive to the ZED X One 4K, is selected with camera-resolution=3:

gst-launch-1.0 zedxonesrc camera-resolution=3 camera-fps=30 ! queue ! autovideoconvert ! queue ! fpsdisplaysink

When using the ZED X One GS model, you can stream frames at 1200p resolution (camera-resolution=2, the default) with 60 Hz frequency:

gst-launch-1.0 zedxonesrc camera-resolution=2 camera-fps=60 ! queue ! autovideoconvert ! queue ! fpsdisplaysink