Skip to navigation

Flash your ZED Box

Open in ClaudeOpen in ChatGPT

Should I flash my ZED Box?

The ZED Box is shipped with a pre-configured operating system and drivers optimized for its hardware.

Flashing (resetting or upgrading the device firmware) is only recommended if you need to:

  • Install a different OS or JetPack version,
  • Recover from a corrupted system,
  • Resolve issues preventing the device from booting or functioning properly.

Flashing will erase all data and custom configurations on your ZED Box. Proceed only if you are familiar with the process or have been instructed by support. For most users, flashing should be a last resort.

Flashing Procedure

The NVIDIA® SDK Manager does not support automatic flashing of the Jetson modules installed in the ZED Box. Therefore, you must manually flash the board using NVIDIA’s BSP for the desired JetPack version.

Force the ZED Box in Recovery mode

It is not required to open the ZED Box to force it into Recovery mode. Opening the box will void the warranty

  • First method:

    To automatically start the ZED Box in Force Recovery mode:

    1. Power off the device by removing both the barrel jack and any connected PoE+ Ethernet cable.
    2. Connect a Type-A to micro USB cable from the Ubuntu host PC to the micro USB port labeled OTG on the device.
    3. Power on the device by plugging in the barrel jack.

    If the above procedure does not work and your ZED Box is in working status, you can force the “Recovery Mode” with the command line below.

  • Second method:

    This is applicable only if your device can normally boot.

    Open a terminal console (Ctrl+Alt+t) and enter the command

    sudo reboot --force forced-recovery

    This command will reboot the ZED Box in Recovery Mode.

When the ZED Box boots in Force Recovery mode, the power LED stays OFF

You can verify that the ZED Box correctly started in “Recovery Mode” by entering this command in a command line console of the host PC:

lsusb -d '0955:'
  • ZED Box with Orin Nano 8 GB: an NVIDIA® device with VID:PID 0955:7523 should be listed. e.g. Bus xxx Device yyy: ID 0955:7523 NVIDIA Corp. APX
  • ZED Box with Orin NX 16 GB: an NVIDIA® device with VID:PID 0955:7323 should be listed. e.g. Bus xxx Device yyy: ID 0955:7323 NVIDIA Corp. APX
  • ZED Box with Orin NX 8 GB: an NVIDIA® device with VID:PID 0955:7423 should be listed. e.g. Bus xxx Device yyy: ID 0955:7423 NVIDIA Corp. APX

If an NVIDIA® device with VID:PID 0955:7020 and type NVIDIA Corp. L4T (Linux for Tegra) running on Tegra is listed, then your ZED Box has not rebooted in Force Recovery mode. You must retry the procedure to boot it in Force Recovery mode.

When the ZED Box is in Recovery Mode, the power LED will not turn on and the device will not boot into the operating system. Instead, it will wait for a host PC to connect to it via USB and flash the OS. The ZED Box will not be accessible via SSH or any other means until the flashing process is completed.

There is a known issue with the first generation of ZED Box with serial numbers starting with GTW-ONX- that prevents them from booting into Force Recovery Mode using the methods described above. Please use the method described in the section “Entering recovery mode with a live USB flashdrive” below to be able to flash the device.

Flashing the ZED Box model

Requirements:

  • JetPack version <= 5.1.2, use a host PC running Ubuntu 18.04 or Ubuntu 20.04.
  • JetPack version >= 6.0, use a host PC running Ubuntu 20.04 or Ubuntu 22.04.

Do not use virtual machines or WSL2 to run Ubuntu when flashing the ZED Box. If you do not have a PC running Ubuntu ready, please consider using a Live USB Key instead:

On the host PC:

  1. Open a terminal console from an empty folder of your choice.

    • For example:

      mkdir -p ~/zedbox_flash
      cd ~/zedbox_flash
  2. Install QEMU to build the image:

    sudo apt install qemu-user-static
  3. Ensure that you previously forced the ZED Box in “Recovery mode”.

  4. Download the Flash Script:

  5. Flash the ZED Box:

    • Ensure you have at least 80GB of free space on your working hard drive.

    • Use the following commands to flash the ZED Box:

      chmod +x <script_name>.sh
      BSP_ROOT=./stereolabs_bsp/ ./<script_name>.sh
      • Replace <script_name> with the name of the downloaded script, e.g., zedbox_all_usb_flash_6.2.
      • All necessary files will be downloaded in the folder $BSP_ROOT. The script will create this folder if it does not exist and will ask you to log in as root.
  6. Wait for the operation to complete. You will see the following output if the flash is successful:

    image

If you encounter any problems during this procedure, please consult the troubleshooting guide.

Post-Flash operations

After flashing your device, follow these steps to install the necessary NVIDIA® and StereoLabs packages to ensure your ZED camera works correctly.

  1. Boot and Login:

    Power on the device and log in with your credentials.

    The new default credentials of your ZED Box are:

    • username: user
    • password: admin
  2. Check the OS Version:

    Follow this support guide to determine the version of the operating system installed on your device.

  3. Connect to the Internet:

    Connect your device to the internet using an Ethernet cable (WiFi may not yet be available, depending on the script you used to flash the device).

    If WiFi is not detected or not connecting, please follow this troubleshooting guide.

  4. Open a Terminal:

    Press Ctrl+Alt+T to open a terminal window.

  5. Update the APT cache:

    Run the following commands to update the APT cache:

    sudo apt update

    Do not run the command sudo apt upgrade before performing the next steps!

  6. Install NVIDIA® JetPack Packages:

    Run the following command to install the NVIDIA® JetPack packages, which include the required Jetson™ drivers, CUDA, and all necessary NVIDIA® libraries:

    sudo apt install nvidia-jetpack
  7. Install the ZED Box GMSL2 driver (for ZED X and ZED X One cameras):

    Download and install the appropriate drivers from the driver web page:

    cd ~/Downloads
    sudo dpkg -i stereolabs-zedbox-<ver_info>_arm64.deb
  8. Hold the kernel packages to not upgrade them and invalidate the setup:

    • Create a hold-zedbox-kernel.sh script file with the following content:

      • nano hold-zedbox-kernel.sh

        Fill the file with this script:

        #!/bin/bash
        #
        # hold-zedbox-kernel.sh
        #
        # Prevents `apt upgrade` from installing nvidia-l4t-kernel versions
        # that are incompatible with the stereolabs-zedbox-* driver package.
        #
        # The stereolabs-zedbox-* driver package requires an nvidia-l4t-kernel version within the
        # range supported by the L4T release it was built for. For example, the
        # L4T 36.4 (JetPack 6.2) driver requires:
        # >= 5.15.148-tegra-36.4.0-20240912212859
        # <= 5.15.148-tegra-36.4.4-20250616085344
        # The range differs for other JetPack versions. Check your driver with:
        # dpkg-query -W -f='${Package}: ${Depends}\n' 'stereolabs-zedbox*'
        #
        # This script holds all NVIDIA L4T kernel-related packages at their
        # currently installed versions so they won't be upgraded past the
        # compatible range.
        #
        # The package list is discovered dynamically from dpkg rather than
        # hardcoded. L4T/JetPack images ship these packages
        # under names that vary between releases (sometimes version-suffixed, e.g.
        # nvidia-l4t-kernel-5.15.148, sometimes via a different meta-package), so a
        # fixed list often matches nothing and every entry is skipped.
        #
        # Usage:
        # sudo ./hold-zedbox-kernel.sh hold # Hold the packages (default)
        # sudo ./hold-zedbox-kernel.sh unhold # Release the hold
        # sudo ./hold-zedbox-kernel.sh status # Show current hold status
        set -euo pipefail
        # Regex matching the L4T kernel package family we want to hold. This is
        # anchored at the start and allows arbitrary suffixes (e.g. -headers,
        # version suffixes) so it catches naming variants across L4T releases.
        PKG_REGEX='^nvidia-l4t-(kernel|rt-kernel|display-kernel|bootloader|xusb-firmware|init)'
        # --- helpers ---------------------------------------------------------------
        require_root() {
        if [[ $EUID -ne 0 ]]; then
        echo "Error: this script must be run with sudo or as root." >&2
        exit 1
        fi
        }
        # Discover installed L4T kernel-related packages by pattern. Populates the
        # global PACKAGES array. Exits with an error if nothing matches, since that
        # means the regex (or the image) needs to be inspected manually.
        discover_packages() {
        mapfile -t PACKAGES < <(
        dpkg-query -W -f='${Package} ${db:Status-Abbrev}\n' 2>/dev/null \
        | awk '$2 ~ /^.i/ {print $1}' \
        | grep -E "$PKG_REGEX" \
        | sort -u
        )
        if [[ ${#PACKAGES[@]} -eq 0 ]]; then
        echo "Error: no installed nvidia-l4t kernel packages matched." >&2
        echo "Inspect manually with:" >&2
        echo " dpkg -l | grep -i nvidia-l4t-kernel" >&2
        echo " dpkg -l | grep -i nvidia-l4t | grep -iE 'kernel|boot|init|firmware'" >&2
        echo "Then adjust PKG_REGEX in this script if the names differ." >&2
        exit 1
        fi
        }
        hold_packages() {
        require_root
        discover_packages
        echo "Holding NVIDIA L4T kernel packages at their current versions..."
        echo
        local held=0
        for pkg in "${PACKAGES[@]}"; do
        local ver
        ver=$(dpkg-query -W -f='${Version}' "$pkg" 2>/dev/null || echo "unknown")
        apt-mark hold "$pkg" >/dev/null
        printf " [HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        held=$((held + 1))
        done
        echo
        echo "Done. Held: $held"
        echo
        echo "These packages will now be ignored by 'apt upgrade'."
        echo "Use 'apt-mark showhold' to verify, or run this script with 'status'."
        }
        unhold_packages() {
        require_root
        discover_packages
        echo "Releasing hold on NVIDIA L4T kernel packages..."
        echo
        local released=0
        local all_holds
        all_holds=$(apt-mark showhold)
        for pkg in "${PACKAGES[@]}"; do
        if echo "$all_holds" | grep -qxF "$pkg"; then
        apt-mark unhold "$pkg" >/dev/null
        printf " [UNHELD] %s\n" "$pkg"
        released=$((released + 1))
        else
        printf " [SKIPPED] %s (was not held)\n" "$pkg"
        fi
        done
        echo
        echo "Done. Released: $released"
        echo
        echo "WARNING: these packages may now be upgraded by 'apt upgrade',"
        echo "which can break the stereolabs-zedbox-* driver if an incompatible kernel"
        echo "version is installed."
        }
        show_status() {
        discover_packages
        echo "Current hold status for NVIDIA L4T kernel packages:"
        echo
        local all_holds
        all_holds=$(apt-mark showhold)
        for pkg in "${PACKAGES[@]}"; do
        local ver
        ver=$(dpkg-query -W -f='${Version}' "$pkg" 2>/dev/null)
        if echo "$all_holds" | grep -qxF "$pkg"; then
        printf " [HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        else
        printf " [NOT HELD] %-45s (version: %s)\n" "$pkg" "$ver"
        fi
        done
        echo
        echo "stereolabs-zedbox-* driver status:"
        local zedpkgs
        zedpkgs=$(dpkg-query -W -f='${Package} ${db:Status-Abbrev} ${Version}\n' 'stereolabs-zedbox*' 2>/dev/null \
        | awk '$2 ~ /^.i/ {print $1 " (version: " $3 ")"}' || true)
        if [[ -n "$zedpkgs" ]]; then
        echo "$zedpkgs" | sed 's/^/ Installed: /'
        else
        echo " Not installed"
        fi
        }
        usage() {
        cat <<EOF
        Usage: sudo $0 [hold|unhold|status]
        hold Hold NVIDIA L4T kernel packages at their current versions (default)
        unhold Release the hold so packages can be upgraded again
        status Show whether each package is currently held
        Why this is needed:
        the stereolabs-zedbox-* driver depends on nvidia-l4t-kernel within a specific
        version range. Newer kernels from NVIDIA's apt repo fall outside this
        range and break the package. Holding the kernel keeps 'apt upgrade'
        from touching it.
        Note:
        The package list is discovered dynamically from dpkg using PKG_REGEX,
        so version-suffixed or renamed kernel packages are matched automatically.
        Holding only prevents FUTURE upgrades; it cannot roll back a kernel that
        has already been installed outside the compatible range.
        EOF
        }
        # --- main ------------------------------------------------------------------
        cmd="${1:-hold}"
        case "$cmd" in
        hold) hold_packages ;;
        unhold) unhold_packages ;;
        status) show_status ;;
        -h|--help|help) usage ;;
        *)
        echo "Error: unknown command '$cmd'" >&2
        echo
        usage
        exit 1
        ;;
        esac
    • Make the script executable:

      chmod +x hold-zedbox-kernel.sh

    • Run the script:

      sudo ./hold-zedbox-kernel.sh

    • Verify the result:

      sudo ./hold-zedbox-kernel.sh status

      All the listed nvidia-l4t-* kernel packages should be reported as [HELD] nvidia-l4t-* (version: xx.y.z-dddddddddddddd).

  9. Download and install the ZED SDK:

    • Visit the StereoLabs website and download the ZED SDK for Jetson that matches your installed JetPack/L4T version.

    • Navigate to your Downloads directory and run the installer:

      cd ~/Downloads
      chmod +x ZED_SDK_Tegra_L4T<l4t_version>_v<x.y.z>.zstd.run
      ./ZED_SDK_Tegra_L4T<l4t_version>_v<x.y.z>.zstd.run
  10. Reboot:

    Restart your device to apply all changes:

    sudo reboot
  11. Enjoy Your Device:

    Your device is now ready for use with the ZED cameras.

Entering recovery mode with a live USB flashdrive

If the bootloader of the ZED Box is “broken”, or you own a first-gen ZED Box (serial number not beginning with GTW-ONX1- or GTW-ONX2-), you will not be able to enter recovery mode automatically by using the standard methods described above.

This tutorial will help you recover from such a situation.

If the serial number of your ZED Box begins with GTW-ONX1- or GTW-ONX2-, you should follow this guide only if you experienced problems while booting the ZED Box to Recovery mode using the standard methods

Requirements:

  • for JetPack version <= 5.1.2, use a host PC running Ubuntu 18.04 or Ubuntu 20.04.
  • for JetPack version >= 6.0, use a host PC running Ubuntu 20.04 or Ubuntu 22.04.
  • a 32 GB or larger USB 3.0 key.

ALL THE INFORMATION STORED IN THE USB KEY WILL BE WIPED DURING THE PROCEDURE

Setting up the USB Key

  • Plug the USB Key to the Ubuntu host machine

  • Download the flash script for the NVIDIA® JetPack version you want to install:

  • Install the necessary dependencies:

    sudo apt install qemu-user-static abootimg libxml2-utils sshpass nfs-kernel-server
  • Use lsblk to identify the USB disk you want to flash. In the caption below, we can identify that the USB disk ID is sda:

    image

    Please be careful and use the name of the drive and not the name of a partition. For instance, use sda instead of sda1.

  • Make the script executable:

    chmod +x <script_name>.sh

    Replace <script_name> with the name of the downloaded script, e.g. zedbox_onx_usb_flash_5.1.2 or zedbox_all_usb_flash_6.2.

  • Launch the script to flash your disk. The operation requires 80GB of free space. You need to specify the USB disk you want to install it on (e.g. sda) and the working directory you want to create (e.g. ./stereolabs_bsp). It will ask you to log in as root several times. Replace the BSP_ROOT and SDX variables with yours in this command:

    BSP_ROOT=./stereolabs_bsp SDX=<sdX> ./<script_name>.sh

    Replace <script_name> with the name of the downloaded script, as in the previous step.

  • Upon success, you will read the following message:

    image
  • The USB drive is now flashed. You will have to run almost the same command to flash the ZED Box later.

You can use the same BSP_ROOT directory to flash your ZED Box once it is in recovery mode. This allows you to skip the download and unpack sections of the script.

Booting from the USB disk

  • Shut down your ZED Box.

  • Plug your USB disk into the single vertical USB type A port of the ZED Box.

  • Power the ZED Box and wait for it to boot from USB, it will take some time.

  • You can now open a terminal console (Ctrl+Alt+t) and enter the following command to reboot into force recovery mode:

    sudo reboot --force forced-recovery

    If you do not have a connected display, you can use a Serial Console. Read the guide on Remote access via Serial Console.

When the ZED Box boots in Force Recovery mode, the power LED stays OFF

You can verify that the ZED Box correctly started in “Recovery Mode” by entering this command in a command line console of the host PC:

lsusb -d '0955:'
  • ZED Box with Orin Nano 8 GB: an NVIDIA® device with VID:PID 0955:7523 should be listed. e.g. Bus xxx Device yyy: ID 0955:7523 NVIDIA Corp. APX

  • ZED Box with Orin NX 16 GB: an NVIDIA® device with VID:PID 0955:7323 should be listed. e.g. Bus xxx Device yyy: ID 0955:7323 NVIDIA Corp. APX

  • ZED Box with Orin NX 8 GB: an NVIDIA® device with VID:PID 0955:7423 should be listed. e.g. Bus xxx Device yyy: ID 0955:7423 NVIDIA Corp. APX

  • Remove the USB drive from the ZED Box.

  • You can now follow the instructions in Flashing the ZED Box model.

If you encounter any problems during this procedure, you can contact the support team by sending an email to support@stereolabs.com.