Flash your ZED Box Orin with Real-Time Kernel
This guide is only for Advanced users who want to flash the ZED Box Orin with a Real-Time Kernel. If you are not familiar with flashing devices, you do not require real-time capabilities, or you do not know what we are talking about, it is recommended to not follow this guide.
The ZED Box Orin can run a Real-Time Kernel (RT Kernel) for applications that require low-latency processing and high determinism. This is particularly useful for robotics, industrial automation, and other time-sensitive applications.
Prerequisites
- Ubuntu 22.04 or 20.04 Linux host machine
- At least 30GB free disk space on the host machine
- A ZED Box Orin device (Orin NX or Orin Nano series)
Download the flashing script
We provide ready scripts to flash the ZED Box Orin with a Real-Time Kernel:
What the Script Does
The script will perform the following actions:
- Downloads required NVIDIA and StereoLabs files automatically
- Extracts and sets up build environment
- Builds RT kernel with ZED Box optimizations
- Flashes the device or creates a bootable USB Key
Flash the ZED Box Orin with Real-Time Kernel
-
Set the workspace directory:
-
Make the script executable:
Replace
XYZwith the version you downloaded, e.g.,364for L4T 36.4. -
[Optional] Set a custom hostname for the ZED Box:
If not set, the default hostname will be used.
-
Put your ZED Box in recovery mode. You can follow the instructions in the ZED Box Orin Flashing Guide.
-
Connect the ZED Box to your host machine via USB.
-
Run the script:
Replace
XYZwith the version you downloaded, e.g.,364for L4T 36.4.The process will take a long time to complete; please be patient.
-
Boot the ZED Box Orin
-
Hold the dependencies before running any
sudo apt updateorsudo apt upgradecommands:This will prevent the system from updating the kernel and overwriting the real-time patches. For detailed information please read here.
Script Process
The script will ask you to confirm the following steps:
- Flash with RT kernel? (y/n) - Answer
yto flash your device; Answernto build the kernel without flashing
Create a bootable USB Key
If you do not want to flash the ZED Box Orin, you can create a bootable USB key with the Real-Time Kernel. This allows you to boot the ZED Box Orin from the USB key without flashing the internal storage. This is useful for testing or development purposes.
-
Insert USB drive (16GB+ recommended)
-
Set USB device:
Replace
sdawith the name of your USB device (e.g.,sdbfor/dev/sdb). -
Set the workspace directory:
-
Make the script executable:
Replace
XYZwith the version you downloaded, e.g.,364for L4T 36.4. -
Run the script:
Replace
XYZwith the version you downloaded, e.g.,364for L4T 36.4.The process will take a long time to complete, depending on your USB drive speed.
Troubleshooting
If you encounter issues during the flashing process:
- Review the
logsdirectory for detailed error messages and troubleshooting information. - Ensure that you have sufficient disk space on your host machine.
- Double-check that your ZED Box Orin is properly in recovery mode.
- Check the USB cable and, if necessary, replace it with a shorter one to avoid connection issues.
- If problems persist, collect the relevant log files and contact StereoLabs support at support@stereolabs.com for further assistance.