Using ZED with ROS 2 from a Docker Container
This tutorial shows how to run the ZED SDK with ROS 2 inside a Docker container: pulling and running a ready-made image, then launching the ZED node.
Download and Run the Docker Image
Pull and run a Docker image that includes the ZED SDK and ROS 2. To build your own, see Create and use Docker images for ZED and ROS 2.
If you want to use RViz2 in Docker, make sure the image includes OpenGL support. Desktop images built with the ZED ROS 2 Wrapper Docker files include the OpenGL runtime libraries.
For a breakdown of these docker run flags, and for the extra volumes required by GMSL2 cameras and recommended for AI models and calibration files, see the Run the Docker image section of the ROS 2 Docker image guide.
Launch the ZED Node
If your image was built with the ZED ROS 2 Wrapper Docker files, the zed-ros2-wrapper is already installed and compiled, and its environment is sourced automatically by the container entry point. You can launch the ZED node right away, setting camera_model to your camera (for example zed2i, zed2, zedm, zedx, or zedxm):
If you are using a plain ROS 2 image that does not already include the wrapper, install it in a colcon workspace first:
To go further, explore the zed-ros2-examples package: it provides tutorials and sample packages to display ZED images, depth, point clouds, and more. Full documentation is available in the ROS 2 section.