Record and Replay Camera Data with ROS 2
This guide provides step-by-step instructions for recording and replaying data with the ZED ROS 2 wrapper. You’ll learn how to capture camera sensor data into SVO or ROS 2 bag files, and how to replay these recordings for debugging, analysis, or development.
The guide also highlights best practices for data synchronization, playback configuration, and optimizing your workflow for efficient data handling.
In order to use the recording and replay tools efficiently, make sure to tune your DDS settings properly by following the dedicated tutorial.
Recording and replaying SVO files
Record SVO files with the ZED ROS 2 Wrapper
An SVO file is a proprietary video format used by the ZED stereo camera to record:
- Synchronized stereo video (left and right images)
- Inertial Measurement Unit (IMU) and other sensor data (temperature, magnetometer, barometer if available)
✅ Main advantages of the SVO
- Low system load during recording: Only essential sensor data is saved, resulting in smaller file sizes and minimal CPU usage. Heavy data types such as point clouds and stereo images can be generated later from the SVO during replay, reducing the need for high-performance hardware during data capture.
- Flexible SDK parameter tuning during replay: SVO files allow you to replay the same recorded sequence multiple times while adjusting ZED SDK parameters (e.g., depth mode, resolution, tracking settings). This enables efficient experimentation and optimization without the need to re-record data, streamlining the development and debugging process.
🚫 SVO Limitations
- Records and replays only ZED SDK sensor data: SVO files capture data directly from the camera (images, IMU, etc.) but do not include topics from other ROS nodes or external navigation modules. If you need to record and replay the full ROS ecosystem, including additional sensors or navigation data, use ROS bag files instead.
Single camera recording
1️⃣ Launch the ZED ROS 2 Wrapper:
2️⃣ Start recording an SVO file: (in a new terminal)
SVO videos can be recorded using various compression modes. We provide both lossless and compressed modes to preserve image quality or reduce file size. Choose your preferred compression mode when recording an SVO with the ZED wrapper:
By default, the SVO file is saved as zed.svo2 (zed_one.svo2 for monocular cameras) in the working directory of the node process. To change this, use the svo_filename field of the request.
Compression mode by default will be 0 if not assigned, which is the H265 LOSSY compression mode, similar to the default SVO recording tool in ZED_Explorer.
On NVIDIA® Jetson™ with ZED SDK >= 5.6, the H.264 LOSSLESS and H.265 LOSSLESS modes are now near lossless, with the sizes given in the table above. With older ZED SDK versions on JetPack 6, they produced lossy files of only 1 to 2% of the raw size. The files are therefore much larger than before: about 12 times larger with H.265 LOSSLESS and 30 times larger with H.264 LOSSLESS (about 75 MB/s with H.265 LOSSLESS for a ZED X Mini at HD1200 and 30 FPS). Check the free space and the write speed of the storage before recording. For images identical to the live ones, use LOSSLESS (mode 5).
3️⃣ Pause and resume the SVO recording (optional):
Starting from v5.5.0 of the ROS 2 Wrapper you can pause an active recording without closing the file, and resume it later:
The service returns success: false when no recording is active, and the node diagnostic reports SVO Recording: PAUSED while the recording is paused.
4️⃣ Stop the SVO recording:
The node and the camera keep running after the recording stops, and a new recording can be started with start_svo_rec. To convert the SVO file to another compression mode, or to export it to a video file or an image sequence, see Converting and Exporting SVO Files.
Encoder preset and encryption
Two parameters of the svo namespace apply to every recording started with start_svo_rec:
svo.svo_encoding_preset[ZED SDK >= 5.3] selects the encoder speed/quality tradeoff:DEFAULT,ULTRAFAST,FAST,MEDIUMorSLOW. See Encoding Presets for what each preset maps to.svo.encryption_key[ZED SDK >= 5.3] encrypts the recorded file with AES-256-CTR. It accepts a path to a 32-byte key file, a 64-character hex key, or a passphrase, and it is never written to the log. Set the same value assvo.decryption_keyto play the recording back.
SVO encryption requires OpenSSL (libcrypto) at runtime. If the encryption key is lost the recorded data is unrecoverable.
Recording Instructions (multi camera setup)
To record SVO files from several cameras at the same time, run each camera node in its own container, that is, in its own process.
Do not use the multi-camera tutorial launch file for SVO recording: it loads all the cameras in the same container. On NVIDIA® Jetson™, recording several cameras from the same process can make the hardware encoder fail after a few minutes. All the cameras then stop, and the SVO files being recorded can be corrupted. We observed this on a Jetson AGX Orin recording four GMSL2 cameras at HD1200 and 30 fps with ZED SDK 5.6, while the same four recordings made from four separate containers completed without errors.
The simplest way is to start the ZED wrapper once per camera, each in its own terminal. When the container_name launch argument is empty (default), each launch creates its own container, /<camera_name>/zed_container:
Only one camera should broadcast the map -> odom -> camera_link TF, so set publish_tf:=false and publish_map_tf:=false on all the other cameras.
You can also start all the cameras from a single launch file. The following example includes zed_camera.launch.py once per camera without setting container_name, so each camera still runs in its own container:
Each camera node provides its own SVO recording service, so you can start and stop the recordings independently. Call the service of each camera, with a different file name for each one:
Stop the SVO recording with the following command for each camera:
Zero-copy Intra-Process Communication (IPC) only works within a container. With one container per camera, a node loaded in a camera’s container gets that camera’s data without copies, but data from the other cameras goes through the regular ROS 2 transport.
Recording Performances
To evaluate recording performance, the following metrics are based on tests performed with all optional SDK modules disabled (depth, positional tracking, and object detection) when launching the ZED wrapper. Up to four ZED X cameras were connected to a single Jetson board. For each camera configuration, the results represent the maximum achievable performance using the latest ZED SDK. All values are reported per camera for consistency and easy comparison.
Orin AGX
Orin NX 16
Test Metrics
- The Maximum SVO FPS metric indicates the mean recording frame rate achieved for each individual SVO file.
- The SVO file size metric indicates the mean file size of an SVO recorded over a recording period of 1 minute.
Replaying SVO files with the ZED ROS 2 Wrapper
Once you have recorded an SVO file, you can use the ZED ROS 2 wrapper to replay it, simulating a live camera stream. During SVO playback, you can enable or disable SDK modules (such as depth sensing, point cloud generation, and tracking) to extract additional data or test different processing pipelines. This flexibility allows you to experiment with various parameter settings and replay the same sequence multiple times, making it easier to debug, optimize, and validate your robotics applications without needing to re-record data.
To replay an SVO file, first set your desired parameters in the ZED wrapper’s configuration YAML file. Then, launch the wrapper with the following command:
At the moment, this feature is limited to single SVO replay.
To support debugging workflows involving SVO files within a robotics architecture, we provide several tools and tutorials:
-
svo_control_node: a utility for precise control over SVO playback using the ZED ROS 2 wrapper. Features include pause/resume, step forward/backward, and playback speed adjustment. -
sync_node: enables synchronized playback of SVO files alongside external navigation data from a ROS 2 bag. Supports pause/resume and step-wise playback, while maintaining time alignment. -
SVO to ROS Bag Conversion Workflow: a tutorial-based method to convert .svo files into standard ROS 2 bag files and merge them with navigation data from another bag, allowing unified playback and analysis.
👉 Follow the dedicated tutorial to learn how to use these tools effectively in your workflow.
Recording and replaying rosbag files
Record rosbag files with the ZED ROS 2 Wrapper
Rosbag files provide a standard way to record and replay data within the ROS ecosystem. With the ZED ROS 2 Wrapper, you can capture not only camera sensor data but also any additional topics published by other nodes in your robotics stack. This makes rosbags ideal for debugging, analysis, and sharing complete system datasets. Recorded topics can be replayed and visualized using tools like RViz or Foxglove, enabling thorough inspection and troubleshooting of complex robotics applications.
✅ Main advantages of the rosbag
- Record and replay the entire robotics stack, including all ROS topics published by any node in your system.
- Capture data from navigation modules, additional sensors, and both standard and custom (proprietary) ROS messages for complete dataset coverage.
- Easily share, analyze, and visualize recorded data using standard ROS tools and third-party applications.
🚫 Rosbag limitations
- Recording large or high-frequency topics, such as images and point clouds, can quickly consume significant storage and system resources, potentially impacting performance.
- ZED parameters and processing options are set at recording time and cannot be changed during playback, limiting flexibility for post-recording optimization or experimentation.
Recording Best Practices
To achieve optimal performance when working with ROS bags, we recommend following a set of best practices.
Use mcap storage
The mcap format allows rosbags optimization and the capability to be immediately replayed through visualization tools like Foxglove.
Use image_transport compression and ffmpeg codecs
If you plan to record image topics, using FFmpeg with the NVENC (for desktop GPUs) or NvMpi (for Jetson boards) codecs in ROS 2 enables hardware-accelerated video encoding on NVIDIA GPUs. This offloads the computationally intensive encoding process from the CPU to the GPU, resulting in lower CPU usage and more stable system performance during recording. Leveraging GPU-based encoding helps maintain higher frame rates, reduces the risk of dropped frames, and allows for reliable rosbag recording even with multiple high-resolution video streams.
Follow the instructions here to build a version of ffmpeg that supports NVMPI:
Once installed, ensure the codecs h264_nvmpi/hevc_nvmpi (for Jetson boards) or hevc_nvenc (for desktop GPU) are properly listed within the available ffmpeg codecs:
We recommend installing the image_transport plugins from source in your ROS workspace (remove any previously installed binary versions to avoid conflicts):
You should now be able to use the ffmpeg installed codecs with the ROS wrapper with the foxglove_compressed_video_transport package. To do so, modify slightly the zed camera launcher to add the chosen codec parameters for the desired type of images. For example, if you want to enable Foxglove image transport with the ffmpeg h264_nvmpi compression codec on the cameras rectified images topics, add these lines to the ZED wrapper node parameters:
Use the following command to explore available codec parameters and options:
You can then adjust the launcher configuration to match your desired recording setup. The parameters will be used at the next launch of the cameras, after recompiling your ros workspace containing the ZED wrapper.
Use rosbag recording as a component node available with IPC [Optional]
Starting with ROS 2 Jazzy, the ros2 bag tool natively supports node composition. This allows you to launch the rosbag recorder as a composable node within a container, enabling efficient intra-process communication (IPC) and reducing data copying overhead.
For earlier ROS 2 distributions, you can achieve similar functionality using the rosbag2_composable_recorder community package. This package provides a component node for rosbag recording with IPC support, improving performance when recording high-bandwidth topics such as images or point clouds.
Using rosbag as a composable node with IPC is especially beneficial in multi-camera or high-throughput scenarios, as it minimizes CPU and memory usage during recording.
Recording Instructions
1️⃣ Launch the ZED ROS 2 Wrapper:
Single camera setup:
Multi camera setup (up to 4 cameras):
2️⃣ Record node topics as a Rosbag mcap file
In the example described above (recording each of the stereo camera images topics with foxglove_compressed_video_transport), the command would be:
Recording Performances of the ZED Cameras images with the ZED Wrapper
To evaluate recording performance, the metrics below are based on tests conducted with no additional SDK modules enabled (depth, positional tracking, object detection modules disabled), using up to four ZED X cameras connected to a single Jetson board. For each camera configuration, the results reflect the maximum achievable performance using the latest version of the ZED SDK. One Rosbag file is recorded with all the cameras left and right images topics. The test is launched with the h264_nvmpi codec added on each stereo camera rectified images topics with a bitrate of 4194304 and medium preset.
Performance Tables
Orin AGX
Orin NX 16
Test Metrics
- The Maximum Rosbag FPS metric indicates the mean recording frame rate achieved for the rosbag file.
- The rosbag file size metric indicates the mean file size of a rosbag recorded over a period of 1 minute.
💡 Tips for recording rosbags efficiently and reducing overall recording load
- Record only the topics you need.
- On Jetson, run
sudo jetson_clocksto maximize the clock frequencies.- On Jetson, get the highest power mode possible (MAXN recommended)
- Split large bags with the
--max-bag-sizeor--max-bag-durationparameters.- Reduce the frame rate for the images and point clouds (e.g from 30 fps to 10 fps) to reduce rosbag loads.
- Reduce publishing rates of other topics when a fast publishing rate (>10 Hz) is not necessary.
- Images and point cloud sizes can be further reduced from the chosen resolution using the
pub_downscale_factorparameter (e.g setting the parameter to 2.0 on a HD1200 resolution publishing images with a resolution of 960x600 pixels).- The
pub_frame_rateparameter clamps the publishing rate to the chosen limit.
Replaying the recorded rosbag
You can replay your recorded mcap rosbag file using standard ROS 2 tools or visualize it directly in Foxglove. Foxglove natively supports the mcap format and compressed video topics via the foxglove_compressed_video_transport plugin, enabling efficient playback and inspection of high-bandwidth data. With Foxglove, you can pause, seek, and resume playback at any point, making it easy to analyze specific events or time ranges within your dataset.
To replay a rosbag in ROS 2, use:
For advanced playback options (such as rate control or topic remapping), refer to the ros2 bag play documentation.