Skip to navigation

Tutorial - Using Depth Perception

Open in ClaudeOpen in ChatGPT

This tutorial shows how to enable depth sensing on the ZED camera and retrieve the depth map and colored point cloud, printing the distance to the pixel at the center of the image in the terminal. The program loops until 50 frames are grabbed. We assume that you have followed the previous tutorials: Hello ZED and Image Capture.

Getting Started

  • First, download the latest version of the ZED SDK.
  • Download the Depth Sensing sample code in C, C++, Python or C#.

Code Overview

Open the camera

As in previous tutorials, we create, configure and open the ZED. We enable depth in NEURAL_LIGHT mode, the fastest depth mode, and express measurements in millimeters. For more information on this parameter, see Depth Modes.

// Create a ZED camera
Camera zed;
// Create configuration parameters
InitParameters init_params;
init_params.sdk_verbose = true; // Enable verbose logging
init_params.depth_mode = DEPTH_MODE::NEURAL_LIGHT; // Set the depth mode to NEURAL_LIGHT (fastest)
init_params.coordinate_units = UNIT::MILLIMETER; // Use millimeter units
// Open the camera
ERROR_CODE err = zed.open(init_params);
if (err != ERROR_CODE::SUCCESS) {
cout << "Error " << err << ", exit program.\n"; // Display the error
return -1;
}

By default, depth perception uses the NEURAL mode (NEURAL_LIGHT on NVIDIA® Jetson™). If you use the default mode, it is not necessary to set the depth mode in InitParameters.

Capture Image and Depth

Now that the ZED is opened, we can capture images and depth. Here we loop until we have successfully captured 50 images. Retrieving the depth map is as simple as retrieving an image:

  • We create a Mat to store the depth map.
  • We call retrieveMeasure() to get the depth map.
// Capture 50 images and depth, then stop
int i = 0;
sl::Mat image, depth, point_cloud;
RuntimeParameters runtime_parameters;
while (i < 50) {
// Grab an image
if (zed.grab(runtime_parameters) == ERROR_CODE::SUCCESS) {
// A new image is available if grab() returns ERROR_CODE::SUCCESS
zed.retrieveImage(image, VIEW::LEFT); // Get the left image
zed.retrieveMeasure(depth, MEASURE::DEPTH); // Retrieve depth matrix. Depth is aligned on the left RGB image.
zed.retrieveMeasure(point_cloud, MEASURE::XYZRGBA); // Retrieve colored point cloud
i++;
}
}

For more information on depth and point cloud parameters, read Using the Depth API.

Measure Distance in Point Cloud

Now that we have retrieved the point cloud, we can extract the depth at a specific pixel. In the example, we extract the distance of the point at the center of the image (width/2, height/2).

// Get and print distance value in mm at the center of the image
// We measure the distance camera - object using Euclidean distance
int x = image.getWidth() / 2;
int y = image.getHeight() / 2;
sl::float4 point_cloud_value;
point_cloud.getValue(x, y, &point_cloud_value);
float distance = sqrt(point_cloud_value.x*point_cloud_value.x + point_cloud_value.y*point_cloud_value.y + point_cloud_value.z*point_cloud_value.z);
printf("Distance to Camera at (%d, %d): %f mm\n", x, y, distance);

We can also directly use the depth map instead of the point cloud to extract the depth value at a specific pixel.

int x = image.getWidth() / 2;
int y = image.getHeight() / 2;
float depth_value;
depth.getValue(x, y, &depth_value);
printf("Depth to Camera at (%d, %d): %f mm\n", x, y, depth_value);

Close the camera

Once 50 frames have been grabbed, we close the camera.

// Close the camera
zed.close();

Advanced Example

To learn how to retrieve and display the live point cloud from the camera and adjust depth confidence filters, check the Point Cloud Viewer sample code.