GStreamer - ZED Data mux
The ZED Data Mux, zeddatamux GStreamer element, allows adding ZED Metadata to a ZED video stream. This is useful if the metadata is removed by a transform filter element that does not automatically propagate it.
The zeddatamux element has the following pads:
sink_video: sink pad receiving a video stream compatible with the ZED capssink_data: sink pad receiving theapplication/datametadata stream generated by thesrc_datapad of azeddemuxelementsrc: source pad pushing the video stream with the metadata attached
Properties
The element defines no specific property. gst-inspect-1.0 zeddatamux only reports the name and parent properties inherited from GstObject:
Example pipelines
Inject ZED metadata information in a stream
Example pipeline that resizes the 2K RGB and depth streams to VGA resolution for display purposes, remuxing the Object Detection metadata as input for the zedodoverlay element:
- Line 1: a
zeddatamuxelement is defined with the namemux. - Line 2: the
zedsrcelement is configured to acquire Left and Depth data with HD2K resolution at 15 FPS, enabling Object Detection with the MULTI-CLASS FAST model. - Line 3: a
zeddemuxelement is defined to split the pipeline into 3 separate branches: one to process the Left Color stream, one to process the Depth stream, and one with binary data created from the Sensors and Detected Objects metadata, which is injected into themuxelement. - Line 4: the depth stream is processed by a
videoscaletransform filter element to reduce the size of the image and is finally displayed on the screen with FPS info. - Line 5: the metadata stream from the
src_datapad ofdemuxis injected into thesink_datapad of themuxelement. - Line 6: the left stream is processed by a
videoscaletransform filter element to reduce the size of the image and is injected into thesink_videopad of themuxelement. - Line 7: the muxed stream from the
muxelement is processed by thezedodoverlaytransform filter element to draw object detection data. - Line 8: the object detection result is converted and displayed on screen with FPS info.
The zeddatamux element is important to ensure that the stream filtered by zedodoverlay contains the Object Detection metadata, which could be removed from the original ZED stream by the videoscale transform filter if it does not handle this kind of metadata.
The ZED metadata is designed to handle scaling transformations of the image stream; in this particular case, the object bounding boxes are rendered correctly even if the filtered images have a size different from the grabbed frames.