Skip to navigation

ZED Link MIPI Quad on AGX Thor with Holoscan Sensor Bridge

Open in ClaudeOpen in ChatGPT

This tutorial will help you assemble the ZED Link MIPI Quad capture card on an NVIDIA® Holoscan Sensor Bridge (HSB), connect it to an NVIDIA® Jetson AGX Thor™ Developer Kit, and stream up to two ZED X One Core cameras.

Support for the NVIDIA® Holoscan Sensor Bridge with the Jetson AGX Thor™ Developer Kit is currently in beta and may have limitations. The driver package required by this configuration is delivered by StereoLabs on request: please contact support@stereolabs.com.

The ZED Link MIPI Quad is designed for the ZED X One Core camera only. It is not compatible with the GMSL2 cameras, and the GMSL2 ZED Link Mono, Duo, and Quad cards are not compatible with the ZED X One Core.

How it works

On the AGX Orin Developer Kit, the ZED Link MIPI Quad plugs directly into the CSI connector of the carrier board. The Jetson AGX Thor™ Developer Kit does not expose a MIPI CSI-2 connector, so the capture card is instead mounted on an NVIDIA® Holoscan Sensor Bridge, which converts the MIPI streams into Camera-over-Ethernet (CoE) and sends them to the Thor over a 10 Gb Ethernet link. On the host, the frames are processed by NVIDIA’s SIPL hardware imaging engine and delivered to your application by the ZED SDK.

The full chain is:

CAMERA SIDEZED X One CoreAR0234 image sensor1 or 2 camerasZED Link MIPI Quadchannels J1 / J2 onlyFPGA sync, 15 µsHoloscan Sensor BridgeLattice CPNX100FPGA IP 0x2510 or newerMIPI CSI-2I-PEX cableMIPI CSI-2J10 connectorCamera-over-Ethernet (CoE)10 GbE · QSFP+ to 4× SFP+ breakout cablehost interface mgbe* · camera subnet 192.168.0.xHOST · NVIDIA JETSON AGX THOR DEVELOPER KITJetPack 7.2 / NVIDIA SIPLhardware imaging pipeline, already flashed on the Developer KitpreinstalledZED Link MIPI driver for HSBAR0234 sensor driver · CoE transport · camera configuration · ISP tuningStep 4ZED SDK v5.5opens the camera and delivers fully processed framesStep 5ZED Studio / your applicationsl::CameraOne APIStep 6provided by StereoLabsprovided by NVIDIA

Frames travel downward through this diagram, and this guide follows the same order: after the host network is set up, it checks the FPGA firmware of the bridge board, then installs the driver, then the ZED SDK.

Because the camera data travels over Ethernet, the Jetson needs a network route to the camera before anything can stream. This is the main difference from the AGX Orin setup, and the most common cause of a camera that is not detected.

Prerequisites

Hardware

Make sure that you have the following items before starting this guide:

  • 1x NVIDIA® Jetson AGX Thor™ Developer Kit, with a QSFP+ port
  • 1x NVIDIA® Holoscan Sensor Bridge, Lattice CPNX100-ETH-SENSOR-BRIDGE board (also referred to as HSB Lite by the NVIDIA® firmware tools)
  • 1x ZED Link MIPI Quad capture card
  • 1x or 2x ZED X One Core cameras
  • 1x MIPI I-PEX cable per camera (one cable is included with each ZED X One Core)
  • 1x QSFP+ to 4x SFP+ breakout cable
  • 1x USB-C power supply for the Holoscan Sensor Bridge, or a free USB-C port on the Developer Kit (see Power up)
  • 1x NVIDIA® power supply to power the Developer Kit (included with the Developer Kit)
NVIDIA Jetson AGX Thor Developer Kit, ZED Link MIPI Quad capture card and NVIDIA Holoscan Sensor Bridge

A standard RJ45 Ethernet cable will not work. The Jetson AGX Thor™ exposes a QSFP+ cage and the Holoscan Sensor Bridge exposes SFP+ cages, so a QSFP+ to 4x SFP+ breakout cable is mandatory.

Software

RequirementWhere it comes fromHow to check it
JetPack 7.2 (Jetson Linux R39.2.0) or newer, with the NVIDIA® Camera packageAlready flashed on the Developer Kitcat /etc/nv_tegra_release returns R39 ... REVISION: 2.0
dpkg -l nvidia-l4t-camera
ZED Link MIPI driver for Holoscan Sensor BridgeStereoLabs delivery archive, contact support@stereolabs.comInstall the driver
ZED SDK v5.5 or newer, for L4T 39.2StereoLabs developer pageInstall the ZED SDK
HSB FPGA firmware 0x2510 or newerPreloaded on the bridge board, upgradableCheck the FPGA firmware version

The driver package is tied to your Jetson Linux release. The R392 suffix in its filename means L4T R39.2 / JetPack 7.2. If /etc/nv_tegra_release reports a different release, ask StereoLabs for the matching package instead of installing this one: a mismatch shows up as a camera that is never detected.

You do not need the ZED SDK sources, the CUDA development packages, or the Holoscan SDK to complete this guide. The only software built from source is a set of small NVIDIA® firmware tools, in Step 3.

If you encounter any issues during the installation process, please refer to the MIPI Troubleshooting page, which has a section dedicated to the Holoscan Sensor Bridge, or contact support@stereolabs.com.

Step 1: Assemble the hardware

Please make sure the Developer Kit and the Holoscan Sensor Bridge are switched off and disconnected from any power source before beginning the installation process.

The Holoscan Sensor Bridge at a glance

Three interfaces of the bridge board are used in this guide: the Camera Connector, where the ZED Link MIPI Quad is mounted; the top SFP+ cage, which carries the video to the Jetson; and the USB-C power input.

Holoscan Sensor Bridge, front view with the camera connector, the SFP+ cages and the USB-C power input
InterfaceSilkscreenUsed in this guide
Camera connector, board-to-boardJ9✔️ mates with the J10 connector of the ZED Link MIPI Quad
SFP+ cage, topJ2 / J3✔️ 10 GbE link to the Jetson AGX Thor
SFP+ cage, bottomJ4 / J5❌ not used
USB-C power inputJ23✔️ powers the bridge board and the capture card
GPIO headerG0 to G15❌ not used

The designators of the SFP+ cages belong to the bridge board. Do not confuse them with the J1 and J2 camera connectors of the ZED Link MIPI Quad, described further down.

Mount the capture card on the Holoscan Sensor Bridge

Align the 120-pin J10 Samtec connector on the bottom of the ZED Link MIPI Quad with the Camera Connector (J9) of the Holoscan Sensor Bridge, then press the card down firmly until the two connectors are fully mated. This is the only connector the capture card mates with, and it also powers the card.

ZED Link MIPI Quad capture card mounted on the Holoscan Sensor Bridge

The capture card sits over the right half of the bridge board, with its four camera connectors facing up.

Connect the cameras

Each camera channel of the ZED Link MIPI Quad uses a 30-pin, 0.4 mm pitch Micro I-PEX receptacle. Insert the plug of the MIPI I-PEX cable into the receptacle and press it down gently until it is fully seated.

With the Holoscan Sensor Bridge, only the J1 (4-Lane CH1) and J2 (4-Lane CH2) channels are wired through. A camera plugged into J3 or J4 is never detected, which limits this configuration to two cameras.

The four channels are silkscreened 4-Lane CH1 to 4-Lane CH4 on the front side of the card:

ZED Link MIPI Quad, front view with the four camera connectors
ConnectorSilkscreen labelPosition on the cardUsable with the Holoscan Sensor Bridge
J14-Lane CH1top right✔️
J24-Lane CH2bottom right✔️
J34-Lane CH3bottom left❌
J44-Lane CH4top left❌

Connect the first camera to J1, and the second one, if any, to J2.

Two MIPI I-PEX cables connected to the J1 and J2 channels of the ZED Link MIPI Quad

Then connect the free end of each cable to the connector on the back of the ZED X One Core:

Two ZED X One Core cameras connected to the ZED Link MIPI Quad mounted on the Holoscan Sensor Bridge

Micro I-PEX connectors are fragile. Never force the plug, never insert it at an angle, and never pull on the wires to disconnect it: always handle the plug body. Damaged connectors are not covered by the warranty.

Cable the bridge to the Jetson AGX Thor

The link between the bridge and the Jetson uses the top SFP+ cage of the bridge. The silkscreen labels of the two cages are printed on the board, just to the right of each of them.

On the Developer Kit, the QSFP+ cage is the wide port on the connection panel, between the power connector and the two USB-C ports:

Connection panel of the NVIDIA Jetson AGX Thor Developer Kit, with the QSFP+ cage
  1. Plug the QSFP+ end of the breakout cable into the QSFP+ port of the Jetson AGX Thor™ Developer Kit.
QSFP+ end of the breakout cable connected to the Jetson AGX Thor Developer Kit
  1. Plug one SFP+ leg of the breakout cable, preferably the first one, into the top SFP+ port of the bridge, labeled J2/J3, shown in the board photo above.

Each leg of the breakout cable appears as a separate mgbe* network interface on the Jetson. You do not need to know which one in advance: Step 2 detects the interface the bridge is plugged into, and Step 4 writes it into the camera configuration files.

Power up

Connect the USB-C power supply to the Holoscan Sensor Bridge, plug in the NVIDIA® power supply of the Developer Kit, connect the optional HDMI, keyboard, and mouse, then power up both boards. The cameras are powered through the MIPI I-PEX cables, so they need no additional power supply.

Once cabled, the bridge board carries the SFP+ leg on its top cage and the USB-C power cable on the opposite side:

Holoscan Sensor Bridge cabled, with the SFP+ leg in the top cage and the USB-C power cable

The bridge board can also be powered from one of the USB-C ports of the Developer Kit, as shown below, which avoids a second power supply on the bench.

QSFP+ data cable and USB-C power cable connected to the Jetson AGX Thor Developer Kit

The ZED X One Core does not support hot-plugging. Cameras must be connected and disconnected only when the host is powered off, and any change to the hardware configuration requires a full reboot of the host to take effect.

Step 2: Configure the host network

The bridge board has a fixed IP address of 192.168.0.2. The Jetson interface it is plugged into must be on the same subnet.

Which mgbe* interface that is depends on the breakout leg you used and on how your board enumerates the interfaces. Rather than guessing, the first block below detects the bridge: the board broadcasts a 1 Hz enumeration beacon on UDP port 12267, which can be heard before any IP address is configured. Paste the three blocks in order, in the same shell, since $EN0 is reused:

# 1. Detect the interface the sensor bridge is on.
# The HSB broadcasts a 1 Hz enumeration beacon on UDP 12267, which we can
# hear before any IP is configured, so this works on a fresh board and does
# not care whether the port is called mgbe0, mgbe0_0, mgbe3, ...
EN0=$(sudo python3 - <<'PY'
import glob, os, socket, struct, time
def carrier(i):
try: return open(f"/sys/class/net/{i}/carrier").read().strip() == "1"
except OSError: return False
cands = [os.path.basename(p) for p in sorted(glob.glob("/sys/class/net/mgbe*"))]
for i in cands:
os.system(f"ip link set {i} up 2>/dev/null")
time.sleep(2)
up = [i for i in cands if carrier(i)]
hit = None
for i in up:
try:
s = socket.socket(socket.AF_PACKET, socket.SOCK_RAW, socket.ntohs(3))
s.bind((i, 0)); s.settimeout(2.5)
except OSError:
continue
t0 = time.time()
while time.time() - t0 < 2.5:
try: d = s.recv(2048)
except Exception: break
if (len(d) >= 42 and struct.unpack("!H", d[12:14])[0] == 0x0800
and d[23] == 17 and struct.unpack("!H", d[36:38])[0] == 12267):
hit = i; break
s.close()
if hit: break
print(hit or (up[0] if len(up) == 1 else ""))
PY
)
if [ -n "$EN0" ]; then echo "Sensor bridge is on $EN0"
else echo "No sensor bridge found. Is it powered and cabled?"; fi
# 2. Create the network profile on the detected interface
sudo nmcli con add con-name hololink-$EN0 ifname $EN0 type ethernet ip4 192.168.0.101/24
sudo nmcli connection modify hololink-$EN0 +ipv4.routes 192.168.0.2/32
sudo nmcli connection up hololink-$EN0
# 3. Check that the board answers
ping -c 3 192.168.0.2

If ping succeeds, the link is good.

If block 1 prints No sensor bridge found, the bridge is not transmitting on any mgbe* port: check that it is powered, that the SFP+ leg is in the top cage (J2/J3), and that ip -br link shows the port as UP, then run the block again.

The rest of this guide spells the interface as mgbe0_0 in its example commands. If the detection picked a different port, substitute yours, or keep using $EN0.

Step 3: Check the FPGA firmware version

The Holoscan Sensor Bridge runs its own FPGA firmware, called the HSB IP, which is completely independent of the software installed on the Jetson. It must be recent enough before anything can stream.

The ZED X One Core requires HSB IP version 0x2510 or newer. Older firmware versions are not supported. The version is encoded as 0xYYMM, so 0x2510 corresponds to the NVIDIA® 25.10 release.

Build the Holoscan Sensor Bridge tools

hololink-enumerate, hololink-read, and hsb_flasher are NVIDIA® tools from the Holoscan Sensor Bridge project. They are not part of the StereoLabs driver package, so they must be built once on the Jetson. Only the small native C++ tools are needed, not the Holoscan SDK, so the build takes only a couple of minutes.

Install the build dependencies:

sudo apt update
sudo apt install -y build-essential git cmake \
libfmt-dev libssl-dev libcurl4-openssl-dev libyaml-cpp-dev python3-dev

Clone the release this guide is written against:

git clone --branch 2.7.0 --depth 1 \
https://github.com/nvidia-holoscan/holoscan-sensor-bridge.git
cd holoscan-sensor-bridge

Configure a tools-only build and build the three tools:

cmake -B build \
-DHOLOLINK_BUILD_ONLY_NATIVE=ON \
-DHOLOLINK_BUILD_EXAMPLES=OFF \
-DHOLOLINK_BUILD_TESTS=OFF \
-DHOLOLINK_BUILD_PYTHON=OFF \
-DHOLOLINK_BUILD_ROCE=OFF \
-DHOLOLINK_BUILD_EMULATOR=OFF
cmake --build build -j$(nproc) \
--target hololink-enumerate hololink-read hsb_flasher

HOLOLINK_BUILD_ONLY_NATIVE=ON is the option that keeps the Holoscan SDK and CUDA compilation out of the build. Without it, CMake requires Holoscan 4.x. The configure step downloads pybind11, so the Jetson needs internet access at this point. CMake 3.24 or newer is required; the version shipped with Ubuntu 24.04 is recent enough.

The binaries are produced in the build tree, relative to the holoscan-sensor-bridge folder:

ToolPath
hololink-enumeratebuild/tools/enumerate/hololink-enumerate
hololink-readbuild/tools/read/hololink-read
hsb_flasherbuild/tools/hsb_flasher/hsb_flasher

The two read-only tools are self-contained and can be installed system-wide:

sudo install -m 755 build/tools/enumerate/hololink-enumerate \
build/tools/read/hololink-read /usr/local/bin/

Leave hsb_flasher in its build folder and run it in place. It locates its firmware manifests and flash strategies next to its own executable, so copying the binary elsewhere breaks it.

Read the current version

The bridge board broadcasts its identity once per second, so hololink-enumerate only needs to listen: no control connection is required and nothing has to be streaming.

hololink-enumerate -i mgbe0_0 -t 10
mac_id=48:B0:2D:EE:84:DA hsb_ip_version=0x2510 fpga_crc=0xffff ip_address=192.168.0.2
fpga_uuid=889b7ce3-65a5-4247-8b05-4ff1904c3359 serial_number=1003003282811 interface=mgbe0_0 board=hololink-lite

hsb_ip_version is the value to check. The board=hololink-lite field confirms that the board is the Lattice CPNX100-ETH-SENSOR-BRIDGE.

On a board that already answers ping, the version register can also be read directly:

hololink-read -H 192.168.0.2 0x80 # HSB_IP_VERSION
hololink-read -H 192.168.0.2 0x84 # FPGA datecode

If hololink-enumerate prints nothing at all, no board is broadcasting: check that the bridge is powered, that ip -br link shows mgbe0_0 as UP, then redo Step 2.

Upgrade the firmware

hsb_flasher recognizes the board from its FPGA UUID and selects the right flash routine and images automatically, so no board-specific option is needed:

# 1. Confirm that the board is reachable
ping -c 3 192.168.0.2
# 2. Flash, from the holoscan-sensor-bridge folder. Omit -t to take the newest
# firmware available, or pin the version validated by StereoLabs (hex, no 0x prefix)
./build/tools/hsb_flasher/hsb_flasher -H 192.168.0.2 -t 2510
# 3. POWER CYCLE the bridge board: the new image only takes effect after a full power-off
# 4. Confirm the new version
hololink-enumerate -i mgbe0_0 -t 10

The power cycle in the commands above is mandatory. A reboot of the Jetson is not enough: the bridge board itself has to be fully powered off and on again.

Points to keep in mind before flashing:

  • No other client may be connected to the board. The control plane accepts exactly one client, so close ZED Studio and any other tool first.
  • The Jetson needs internet access. hsb_flasher downloads the CLNX and CPNX images from the NVIDIA® server and verifies their MD5 checksum. If the Jetson is offline, fetch the two .bit files on another machine and pass them explicitly:
    ./build/tools/hsb_flasher/hsb_flasher -H 192.168.0.2 \
    --clnx fpga_clnx_v2510.bit --bitfile fpga_cpnx_v2510.bit
  • If the board already runs the target version, the tool exits without doing anything. Add --reapply to force a reflash.
  • Firmware older than 0x2407 is not handled by this flasher. Follow the NVIDIA® HSB 2.0 update procedure first, then come back to this step.

The complete upstream procedure is available in the NVIDIA® Holoscan Sensor Bridge documentation.

A blank board cannot be flashed this way. Depending on the vendor, the bridge may ship with no FPGA image at all, in which case it answers neither ping nor hololink-enumerate, because flashing over Ethernet requires working firmware to begin with. Such a board has to be programmed over JTAG with the Lattice Radiant Programmer first: please check with your board vendor.

This package contains everything the Jetson needs to see the camera: the AR0234 sensor driver, the Camera-over-Ethernet transport driver, the camera configuration, and the ISP tuning. There is nothing to build and nothing to copy by hand: once the package is installed, only the host interface name has to be set.

The driver package for the Holoscan Sensor Bridge configuration is different from the ZED Link MIPI driver used on the AGX Orin Developer Kit. It is delivered by StereoLabs on request: please contact support@stereolabs.com.

Unpack the archive sent by StereoLabs and install the Debian package:

sudo dpkg -i sipl-uddf-drivers_<version>-R392_arm64.deb

Check that the five files are correctly installed:

dpkg -L sipl-uddf-drivers | grep -E '\.so$|\.json$|\.nito$'
/usr/lib/nvsipl_drv/libar0234_library.so
/usr/lib/nvsipl_drv/libhsb_transport_library.so
/var/nvidia/nvcam/settings/sipl/nova0_camera.json
/var/nvidia/nvcam/settings/sipl/nova1_camera.json
/var/nvidia/nvcam/settings/sipl/ZED_AR0234CS_HAWK.nito

If any of them is missing, the installation failed: run dpkg -i again and read its output.

Point the camera configuration to the host interface

The camera configuration files name the Jetson interface the bridge is plugged into. Set it to the interface detected in Step 2:

# Recover the interface from the network profile created in Step 2,
# in case this is a new shell
[ -n "$EN0" ] || EN0=$(nmcli -t -f NAME con show | sed -n 's/^hololink-//p' | head -n 1)
echo "Using $EN0"
sudo python3 - "$EN0" <<'PY'
import glob, re, sys
ifname = sys.argv[1]
for p in sorted(glob.glob("/var/nvidia/nvcam/settings/sipl/nova*_camera.json")):
src = open(p).read()
new, n = re.subn(r'("if_name"\s*:\s*")[^"]*(")',
lambda m: m.group(1) + ifname + m.group(2), src)
if new != src:
open(p, "w").write(new)
print("%s: %d if_name field(s) -> %s" % (p, n, ifname))
PY

Each file should report at least one if_name field set to your interface. If Using prints an empty name, no network profile was found: redo Step 2 and run this block again in the same shell. If a file reports 0 if_name field(s), it was not installed correctly: reinstall the driver package.

The IP address (192.168.0.2) and the subnet also come from /var/nvidia/nvcam/settings/sipl/nova0_camera.json, and must match the network profile created in Step 2.

Reinstalling or upgrading the driver package can restore the default interface name: run this block again after every dpkg -i.

To remove or upgrade the package later:

sudo dpkg -r sipl-uddf-drivers # remove
sudo dpkg -i sipl-uddf-drivers_<new-version>-R392_arm64.deb # upgrade in place

Step 5: Install the ZED SDK

The ZED SDK turns the SIPL pipeline into a regular ZED camera, accessible through the sl::CameraOne API, and includes ZED Studio. Camera-over-Ethernet support is built into the v5.5 release.

Download the installer matching your Jetson Linux version from the StereoLabs developer page, then run it:

chmod +x ZED_SDK_Tegra_L4T39.2_v5.5.0.zstd.run
./ZED_SDK_Tegra_L4T39.2_v5.5.0.zstd.run

The L4T39.2 part of the filename must match the release reported by /etc/nv_tegra_release. Answer the prompts of the installer and accept the license; the optional AI models and the Python API are not required for this guide. The SDK is installed in /usr/local/zed/.

More details are available in the Install the ZED SDK on NVIDIA® Jetson guide.

Install the ZED SDK after the driver package. Both orders work, but this way the first detection test you run is already meaningful.

Step 6: Verify the installation

Check that the cameras are detected:

ZED_Studio --list

Each connected ZED X One Core is listed with its serial number and an Input type: HOLOLINK field. ZED_Explorer --all lists them as well. If nothing is listed, see the MIPI Troubleshooting page.

Open ZED Studio to get a live view and select the camera in the device list:

ZED_Studio

The ISP tuning shipped in the driver package is applied automatically, so the image arrives fully processed, with auto exposure and auto white balance already running.

A camera can also be opened directly at a given resolution and frame rate, using the serial number printed by --list:

ZED_Studio --camera <serial_number> HD1200 30
ZED_Studio --camera <serial_number> HD1080 60

In this configuration, the ZED X One Core supports the following video modes, each at 15, 30, or 60 fps:

ValueResolutionNotes
HD12001920x1200native AR0234
HD10801920x1080center-cropped
SVGA960x600binned and cropped

Any other value falls back to the closest supported mode.

The 960x600 @120 fps binning mode listed in the ZED X One Core specifications is not available in this configuration: over Camera-over-Ethernet, every resolution is capped at 60 fps. The full set of modes is available on an NVIDIA® Jetson AGX Orin™ Developer Kit.

The -r option of ZED Studio is --recording, not the resolution. The resolution is the second positional argument of --camera, as shown above. Run ZED_Studio --help for the complete list of options.

Multi-camera configuration

Only the J1 and J2 channels of the ZED Link MIPI Quad are wired through the Holoscan Sensor Bridge, so this configuration supports a maximum of two cameras.

Camera typeCamera modelMax number of camerasMax resolution/FPS
per channel
MonocularZED X One Core2 camerasHD1200@60fps
HD1080@60fps
SVGA@60fps

The two cameras are hardware-synchronized by the FPGA of the capture card, with a precision of 15 µs, so no jumper or external wiring is required. They can be used as a virtual stereo camera in the ZED SDK, after calibration: see Setting up the ZED X One Stereo.

Although frames are hardware-synchronized with 15 µs precision, software timestamps are assigned when the driver receives the frames, and may show a slight millisecond-level jitter. Frames are considered synchronized if the timestamp difference is less than one frame period (1000/FPS ms).

Quick reference

ItemValue
Bridge board IP address192.168.0.2
Host interfacemgbe* port detected in Step 2 (mgbe0_0 in the examples)
Minimum FPGA firmware0x2510
Minimum Jetson Linux releaseR39.2.0 (JetPack 7.2)
Minimum ZED SDK versionv5.5
Usable camera channelsJ1 and J2 only, two cameras maximum

End-to-end command summary:

# 1. Host network (EN0 = interface detected in Step 2)
EN0=mgbe0_0
sudo nmcli con add con-name hololink-$EN0 ifname $EN0 type ethernet ip4 192.168.0.101/24
sudo nmcli connection modify hololink-$EN0 +ipv4.routes 192.168.0.2/32
sudo nmcli connection up hololink-$EN0
ping -c 3 192.168.0.2
# 2. FPGA firmware, must be 0x2510 or newer
hololink-enumerate -i $EN0 -t 10
# only if too old: flash, then POWER CYCLE the bridge board
./build/tools/hsb_flasher/hsb_flasher -H 192.168.0.2 -t 2510
# 3. Camera driver package, then set if_name in the camera config (Step 4)
sudo dpkg -i sipl-uddf-drivers_<version>-R392_arm64.deb
sudo sed -i -E "s/(\"if_name\"[[:space:]]*:[[:space:]]*\")[^\"]*/\1$EN0/" \
/var/nvidia/nvcam/settings/sipl/nova*_camera.json
# 4. ZED SDK
chmod +x ZED_SDK_Tegra_L4T39.2_v5.5.0.zstd.run
./ZED_SDK_Tegra_L4T39.2_v5.5.0.zstd.run
# 5. Run
ZED_Studio --list # confirm the detection
ZED_Studio # live view

Troubleshooting

The troubleshooting checks for this configuration are gathered on the MIPI Troubleshooting page, alongside the ones shared with the AGX Orin Developer Kit:

  • Common checks and commands, to list the cameras seen by the ZED SDK and inspect the capture pipeline.
  • Holoscan Sensor Bridge on Jetson AGX Thor, for the symptoms specific to this setup: no device listed, a single camera detected, firmware too old, black live view, recovering the Ethernet connection, and cleaning up the SIPL log output.

🎉 Congratulations! You have successfully assembled your StereoLabs ZED Link MIPI Quad capture card on an NVIDIA® Holoscan Sensor Bridge and connected it to your NVIDIA® Jetson AGX Thor™ Developer Kit. Now that the cameras are up and running, it is time to start experimenting and building your projects. Happy coding!