Setting Up Multiple 3D Cameras
There are two ways to build a multi-camera setup:
- Connecting multiple cameras on a single machine, such as a desktop PC, server or NVIDIA® Jetson™ board.
- Turning ZEDs into IP cameras that share and exchange synchronized data on the local network.
StereoLabs cameras come in two connectivity families, and several of the recommendations below depend on which one you use:
- USB cameras (ZED, ZED Mini, ZED 2, ZED 2i): connect over USB 3.0 to any Windows or Linux host.
- GMSL2 cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One S/GS, ZED X One 4K): connect through a ZED Link GMSL2 capture card and are only compatible with NVIDIA® Jetson™ platforms.
ZED and ZED 2 camera models are out of production.
Each section below indicates whether it applies to USB, GMSL2, or both. Both families can be combined on a single host and can be used as IP cameras on a local network.
Setting up Multiple Cameras on One Host
It is possible to connect multiple ZED cameras to a single host. Check out the Multi-Camera sample on GitHub to see an example of implementation.
The way cameras are connected and the limits you have to consider depend on whether they are USB or GMSL2 cameras.
Hardware Recommendations for USB cameras
Applies to USB cameras (ZED, ZED Mini, ZED 2, ZED 2i).
-
Watch the USB bandwidth: The ZED in 1080p30 mode generates around 250MB/s of image data. The maximum USB 3.0 bandwidth is around 620MB/s, so the number of cameras, resolutions, and frame rates you can use on a single machine will be limited by the USB 3.0 controller on the motherboard. When the bandwidth limit is exceeded, corrupted frames (green or purple frames, tearing) can appear, and cameras may even disconnect.
-
Use PCIe expansion cards: To use multiple USB ZED cameras at full speed on a single computer, we recommend distributing them across several USB controllers by adding USB 3.0 multi-channel expansion cards.
Hardware Recommendations for GMSL2 cameras
Applies to GMSL2 cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One S/GS, ZED X One 4K).
GMSL2 cameras do not connect over USB. They are linked to an NVIDIA® Jetson™ device through a ZED Link GMSL2 capture card, which provides dedicated, low-latency serial links instead of a shared USB bus. This removes the USB-controller bottleneck and makes GMSL2 the recommended option for dense multi-camera rigs.
-
Choose the right capture card: each GMSL2 link drives one camera. Pick the capture card according to the number of cameras you need to connect to a single Jetson™:
- ZED Link Mono: 1 camera.
- ZED Link Duo: up to 2 stereo cameras, or up to 4 monocular ZED X One cameras.
- ZED Link Quad: up to 4 stereo cameras, or up to 8 monocular ZED X One cameras.
-
Mind the power budget: connecting several GMSL2 cameras (especially when powering accessories over the GMSL2 link) increases the current draw on the capture card. Check the GMSL2 Power Requirements before scaling up a rig.
-
Install the ZED Link driver: GMSL2 cameras require the ZED Link driver to be installed on the Jetson™ before they can be opened by the ZED SDK. See Install and Upgrade the Drivers.
Increase GPU memory
Applies to both USB and GMSL2 cameras.
The ZED SDK needs up to 750MB of GPU memory when retrieving depth information in NEURAL LIGHT mode. To make sure you don’t run out of GPU memory when using the SDK with multiple cameras, we recommend using an NVIDIA® GPU with at least 6GB of memory. On NVIDIA® Jetson™ platforms, where memory is shared between CPU and GPU, make sure the device has enough total RAM for the number of cameras and depth modes you plan to run.
Frame synchronization
GMSL2 cameras can be synchronized at the hardware level for accurate, frame-level alignment, while USB cameras rely on timestamp-based software alignment.
-
GMSL2 (hardware triggering): cameras connected to the same ZED Link Duo or Quad capture card are automatically frame-synchronized. The capture card can also act as a trigger master to drive external sensors, or as a slave to be driven by an external trigger source, and multiple capture cards can be chained together so all their cameras share the same trigger. See the GPIO triggering guides for the ZED Link Mono, ZED Link Duo, and ZED Link Quad cards.
-
USB: USB cameras do not expose a hardware trigger. To align frames across USB cameras, rely on the image timestamps provided by the ZED SDK, or use the local network setup with PTP synchronization described below.
How to list connected cameras
Applies to both USB and GMSL2 cameras.
The ZED SDK can list the connected cameras using getDeviceList(), and provide their serial number and model for identification. Once you know which ZED should be opened, you can request a specific serial number with InitParameters.input.setFromSerialNumber(1010). See Identifying the Camera Model for code examples, including how to get the model from a serial number alone.
Setting up Multiple Cameras on a Local Network
Applies to both USB and GMSL2 cameras.
Both USB and GMSL2 cameras can be turned into IP cameras and stream synchronized data over the local network. Because synchronization here relies on the system clock of each host rather than on a physical trigger line, the Precision Time Protocol (PTP) is used to align the clocks of all the devices on the network.
When GMSL2 cameras are connected to the same Jetson™ (or to chained capture cards), prefer the hardware triggering described above for the most accurate frame alignment. PTP is the method to use when cameras are distributed across different hosts on the network.
Configure the PTP service to synchronize the devices
Precision Time Protocol (PTP or IEEE1588), an IEEE standard, is a method to synchronize the clock of multiple devices on an Ethernet network. This is achieved by setting one device as the master clock and having all other devices synchronize and periodically adjust to the master clock. Synchronization is handled automatically by the devices once the master and slave devices are set.
PTP is essential to ensure that all the cameras on the local network publish frames with timestamps referenced to the same time source, since each timestamp uses the system clock for reference.
To configure the local network rig, you must select one device to act as the master. It will be the only one (if connected to the internet) that keeps the NTP service active to adjust the system clock according to world time.
Advantages of PTP
A major advantage of PTP is the hardware support found in various Network Interface Controllers (NICs) and network switches. This specialized hardware allows PTP to account for delays in message transfer and greatly improves the accuracy of time synchronization. Although it is possible to use non-PTP-enabled hardware components within the network, doing so often causes increased jitter or introduces delay asymmetry, resulting in synchronization inaccuracies that grow with the number of PTP-incompatible components in the communication path. To achieve the best possible accuracy, it is recommended that all network components between PTP clocks support PTP hardware.
With hardware PTP support, the NIC has its own built-in clock, which is used to time stamp received and transmitted PTP messages. It is this onboard clock that is synchronized with the PTP master, and the computer system clock is synchronized with the PTP hardware clock on the NIC. With PTP software support, the system clock is used to time stamp PTP messages and is synchronized directly with the PTP master. Hardware PTP support provides greater accuracy as the NIC can stamp PTP packets as they are sent and received, while software PTP support requires additional processing of PTP packets by the operating system.
Install PTP and tools
To enable each device on the local network to receive PTP messages, you must install the linuxptp and ethtool packages:
The linuxptp package includes the ptp4l and phc2sys programs for clock synchronization. The ptp4l program implements the PTP boundary clock and the ordinary clock. With hardware timestamping, it synchronizes the PTP hardware clock with the master clock; with software timestamping, it synchronizes the system clock with the master clock. The phc2sys program is only needed with hardware timestamps, to synchronize the system clock with the PTP hardware clock on the network interface card.
ethtool is used to verify the clock capabilities of the NIC installed on the devices.
Check PTP hardware support
To verify the capabilities of the NIC installed on the device, use the following command:
The network interface name can be retrieved using the command:
The DEVICE column shows the name of all the network interfaces currently connected.
For software time stamping support, the parameters list should include:
SOF_TIMESTAMPING_SOFTWARESOF_TIMESTAMPING_TX_SOFTWARESOF_TIMESTAMPING_RX_SOFTWARE
For hardware time stamping support, the parameters list should include:
SOF_TIMESTAMPING_RAW_HARDWARESOF_TIMESTAMPING_TX_HARDWARESOF_TIMESTAMPING_RX_HARDWARE
For example, the following Ethernet adapter of an NVIDIA® Jetson™ device supports hardware and software timestamping:
The WiFi adapter, on the other hand, cannot be used for PTP synchronization: it does not support hardware timestamping and does not provide full software timestamping support, because the SOF_TIMESTAMPING_TX_SOFTWARE capability is missing:
Set up the master device
If the master device is connected to the internet and you want to be sure that the time of all the devices in the local network is synchronized with the world time, enable the NTP sync service:
Open a console and start the PTP service in hardware mode:
Replace <interface_name> with the name of the network interface that you are using for communication (e.g. eth0, eno1).
You can get the list of available network devices using the command
The DEVICE column shows the name of all the network interfaces currently connected.
If the ptp4l command reports an error message similar to the following
then the selected network interface does not support hardware timestamping and the PTP service must be started in “software mode”:
Remove the -m option to stop console logging messages.
Set up all the slave devices
Please replicate the following procedure for all the slave devices to be synchronized on the local network.
Open a console and enter the following command to start the PTP service in slave mode:
Replace <interface_name> with the name of the network interface that you are using for communication (e.g. eth0, eno1).
As with the master, if the ptp4l command reports an error message similar to the following
then the network interface does not support hardware timestamping and the PTP service must be started in “software mode”:
Remove the -m option to stop console logging messages.
If the slave has been started in hardware timestamping mode, it is necessary to synchronize the system clock to the PTP hardware clock on the NIC. Open a new console and enter the command:
The -s option sets the clock source, in this case the /dev/ptp0 clock created above with the ptp4l command.
The -c option sets the destination clock to be synchronized, in this case the real-time clock of the operating system.
It is important to explicitly set the “clock offset” to zero with the option -O 0, otherwise a default offset of ~37 seconds will be applied (see the TIME SCALE USAGE section of the phc2sys man page with man phc2sys).
Remove the -m option to stop console logging messages.
Test the configuration
To test the correctness of the configuration, you must also disable the NTP service on the master so that you can manually change the system time:
Compile the following simple ZED application:
The application compares the timestamps from the CURRENT reference and the IMAGE reference.
Under normal conditions, the value printed while the application runs should stay fairly constant; the value depends on the frame rate:
However, if a clock change occurs due to PTP sync:
- The
CURRENTtimestamp will change according to the clock configuration change (smooth or jump). - The
IMAGEtimestamp will be smoothly adapted to the current system clock. There will be no large jumps because it needs to stay consistent with the camera FPS. Therefore, you should see an initial large difference that decreases over time and finally returns to the original constant difference.
To generate a visible PTP sync, you can manually modify the system time of the master device:
The greater the difference between the new time and the previous one, the greater the time jump highlighted by the test application, and the greater the time taken to stabilize.
Do not forget to re-enable the NTP service on the master device after the test to ensure that the system clocks are synchronized with world time: